You are viewing documentation for version:3.3.0Public Attributes#uint8_tdev_addrremote device address uint16_tlengthlength of attribute value uint8_tatt_valueThis contains the attribute value. Public Attribute Documentation#dev_addr#uint8_t rsi_ble_event_att_value_s::dev_addr[RSI_DEV_ADDR_LEN]remote device address length#uint16_t rsi_ble_event_att_value_s::lengthlength of attribute value att_value#uint8_t rsi_ble_event_att_value_s::att_value[RSI_DEV_ATT_LEN]This contains the attribute value. The maximum value is 240, please refer RSI_DEV_ATT_LEN Macro