Public Attributes#
uint8_t
BD Address of the remote device.
uint8_t
16 byte irk of the local device
uint8_t
16 byte irk of the remote device
uint16_t
remote device ediv value
uint8_t
remote device rand value
uint8_t
remote device ltk value
uint8_t
Identity address type - public/random
0x00 --> Public Identity Address
0x01 --> Random (static) Identity Address
All other values Reserved for future use.
uint8_t
Identity address which is resolved after security keys exchange.
uint8_t
Device address type.
Public Attribute Documentation#
dev_addr#
uint8_t rsi_bt_event_le_security_keys_s::dev_addr[RSI_DEV_ADDR_LEN]
BD Address of the remote device.
Identity_addr_type#
uint8_t rsi_bt_event_le_security_keys_s::Identity_addr_type
Identity address type - public/random
0x00 --> Public Identity Address
0x01 --> Random (static) Identity Address
All other values Reserved for future use.
Identity_addr#
uint8_t rsi_bt_event_le_security_keys_s::Identity_addr[6]
Identity address which is resolved after security keys exchange.