MQTT Client broker information structure.
Public Attributes#
sl_ip_address_t
IP address of broker.
uint16_t
Port number of broker.
bool
Whether to use MQTT or MQTTS.
uint16_t
MQTT Connection timeout.
uint16_t
Keep alive timeout of MQTT connection.
uint16_t
MQTT ping retries.
Public Attribute Documentation#
ip#
sl_ip_address_t sl_mqtt_broker_t::ip
IP address of broker.
Definition at line
132
of file components/service/mqtt/inc/sl_mqtt_client_types.h
port#
uint16_t sl_mqtt_broker_t::port
Port number of broker.
Definition at line
133
of file components/service/mqtt/inc/sl_mqtt_client_types.h
is_connection_encrypted#
bool sl_mqtt_broker_t::is_connection_encrypted
Whether to use MQTT or MQTTS.
Definition at line
134
of file components/service/mqtt/inc/sl_mqtt_client_types.h
connect_timeout#
uint16_t sl_mqtt_broker_t::connect_timeout
MQTT Connection timeout.
Definition at line
135
of file components/service/mqtt/inc/sl_mqtt_client_types.h
keep_alive_interval#
uint16_t sl_mqtt_broker_t::keep_alive_interval
Keep alive timeout of MQTT connection.
Definition at line
136
of file components/service/mqtt/inc/sl_mqtt_client_types.h
keep_alive_retries#
uint16_t sl_mqtt_broker_t::keep_alive_retries
MQTT ping retries.
Definition at line
137
of file components/service/mqtt/inc/sl_mqtt_client_types.h