Public Attributes#
uint8_t
Device address of the remote device.
uint16_t
Maximum TX Octets to be transmitted.
uint16_t
Maximum TX time to transmit the MaxTxOctets.
uint16_t
Maximum Rx Octets to be received.
uint16_t
Maximum Rx time to receive the MaxRxOctets.
Public Attribute Documentation#
dev_addr#
uint8_t rsi_ble_event_data_length_update_s::dev_addr[RSI_DEV_ADDR_LEN]
Device address of the remote device.
Definition at line
384
of file components/device/silabs/si91x/wireless/ble/inc/rsi_ble_apis.h
MaxTxOctets#
uint16_t rsi_ble_event_data_length_update_s::MaxTxOctets
Maximum TX Octets to be transmitted.
Definition at line
386
of file components/device/silabs/si91x/wireless/ble/inc/rsi_ble_apis.h
MaxTxTime#
uint16_t rsi_ble_event_data_length_update_s::MaxTxTime
Maximum TX time to transmit the MaxTxOctets.
Definition at line
388
of file components/device/silabs/si91x/wireless/ble/inc/rsi_ble_apis.h
MaxRxOctets#
uint16_t rsi_ble_event_data_length_update_s::MaxRxOctets
Maximum Rx Octets to be received.
Definition at line
390
of file components/device/silabs/si91x/wireless/ble/inc/rsi_ble_apis.h
MaxRxTime#
uint16_t rsi_ble_event_data_length_update_s::MaxRxTime
Maximum Rx time to receive the MaxRxOctets.
Definition at line
392
of file components/device/silabs/si91x/wireless/ble/inc/rsi_ble_apis.h