Public Attributes#
Remote device Address.
Status of the Encryption
ENCRYPT_ENABLED BIT(0) --> To indicate or set encryption is enabled AUTH_LTK_OR_STK_ENC
BIT(1) --> To indicate or set Authenticated Pairing and Encryption UN_AUTH_LTK_OR_STK_ENC
BIT(2) --> To indicate or set UnAuthenticated pairing and Encryption AUTH_LTK_WITH_LE_SC_ENC
BIT(3) --> To indicate or set Authenticated Pairing and Enc with LE SC.
BLE Secure Connections Enable/disable indication
0 --> Disable
1 --> Enable.
Local device EDIV.
Local RAND.
Local Long term Key.
Remote Device Address type.
Public Attribute Documentation#
dev_addr#
uint8_t rsi_bt_event_encryption_enabled_s::dev_addr[RSI_DEV_ADDR_LEN]
Remote device Address.
180
of file components/device/silabs/si91x/wireless/ble/inc/rsi_ble_apis.h
enabled#
uint8_t rsi_bt_event_encryption_enabled_s::enabled
Status of the Encryption
ENCRYPT_ENABLED BIT(0) --> To indicate or set encryption is enabled AUTH_LTK_OR_STK_ENC
BIT(1) --> To indicate or set Authenticated Pairing and Encryption UN_AUTH_LTK_OR_STK_ENC
BIT(2) --> To indicate or set UnAuthenticated pairing and Encryption AUTH_LTK_WITH_LE_SC_ENC
BIT(3) --> To indicate or set Authenticated Pairing and Enc with LE SC.
190
of file components/device/silabs/si91x/wireless/ble/inc/rsi_ble_apis.h
sc_enable#
uint8_t rsi_bt_event_encryption_enabled_s::sc_enable
BLE Secure Connections Enable/disable indication
0 --> Disable
1 --> Enable.
196
of file components/device/silabs/si91x/wireless/ble/inc/rsi_ble_apis.h
localediv#
uint16_t rsi_bt_event_encryption_enabled_s::localediv
Local device EDIV.
198
of file components/device/silabs/si91x/wireless/ble/inc/rsi_ble_apis.h
localrand#
uint8_t rsi_bt_event_encryption_enabled_s::localrand[8]
Local RAND.
200
of file components/device/silabs/si91x/wireless/ble/inc/rsi_ble_apis.h
localltk#
uint8_t rsi_bt_event_encryption_enabled_s::localltk[16]
Local Long term Key.
202
of file components/device/silabs/si91x/wireless/ble/inc/rsi_ble_apis.h
dev_addr_type#
uint8_t rsi_bt_event_encryption_enabled_s::dev_addr_type
Remote Device Address type.
204
of file components/device/silabs/si91x/wireless/ble/inc/rsi_ble_apis.h