Public Attribute Documentation#
maxtxoctets#
uint16_t rsi_ble_resp_read_max_data_length_s::maxtxoctets
maxtxoctets
Preferred maximum number of payload octets that the local Controller should include in a single Link Layer packet on this connection.
Definition at line
984
of file components/device/silabs/si91x/wireless/ble/inc/rsi_ble_apis.h
maxtxtime#
uint16_t rsi_ble_resp_read_max_data_length_s::maxtxtime
maxtxtime
Preferred maximum number of microseconds that the local Controller should use to transmit a single Link Layer packet on this connection
Definition at line
989
of file components/device/silabs/si91x/wireless/ble/inc/rsi_ble_apis.h
maxrxoctets#
uint16_t rsi_ble_resp_read_max_data_length_s::maxrxoctets
maxrxoctets
Maximum number of payload octets that the local Controller supports for reception of a single Link Layer packet on a data connection
Definition at line
994
of file components/device/silabs/si91x/wireless/ble/inc/rsi_ble_apis.h
maxrxtime#
uint16_t rsi_ble_resp_read_max_data_length_s::maxrxtime
maxrxtime
Maximum time, in microseconds, that the local Controller supports for reception of a single Link Layer packet on a data connection.
Definition at line
999
of file components/device/silabs/si91x/wireless/ble/inc/rsi_ble_apis.h