HTTP Server#
This module contains the HTTP Server API data types.
Modules#
sl_http_server_uri_query_parameter_t
Typedefs#
typedef sl_status_t(*
sl_http_request_handler_t)(sl_http_server_t *handle, sl_http_server_request_t *request)
Callback invoked when an HTTP request is received.
typedef struct sl_http_server_request_s
HTTP server request parameters.
typedef struct sl_http_server_s
HTTP server handle used to manage all HTTP server functions.
Typedef Documentation#
sl_http_request_handler_t#
sl_http_request_handler_t )(sl_http_server_t *handle, sl_http_server_request_t *request)
Callback invoked when an HTTP request is received.
Parameters
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| [out] | handle | HTTP server handle of type sl_http_server_t | |
| [out] | request | HTTP request which has been received of type sl_http_server_request_t |
Returns
sl_status_t. See https://docs.silabs.com/gecko-platform/4.1/common/api/group-status for details.
sl_http_server_request_t#
typedef struct sl_http_server_request_s sl_http_server_request_t
HTTP server request parameters.
sl_http_server_t#
typedef struct sl_http_server_s sl_http_server_t
HTTP server handle used to manage all HTTP server functions.