HTTP server request parameters.

Public Attributes#

HTTP protocol version.

uint16_t

Number of request headers received.

Type of the request (GET, POST, etc.)

uint32_t

Length of the request data.

Public Attribute Documentation#

uri#

sl_http_server_request_uri_t sl_http_server_request_s::uri

URI of the request.


Definition at line 175 of file components/service/sl_http_server/inc/sl_http_server_types.h

version#

sl_http_request_version_t sl_http_server_request_s::version

HTTP protocol version.


Definition at line 176 of file components/service/sl_http_server/inc/sl_http_server_types.h

request_header_count#

uint16_t sl_http_server_request_s::request_header_count

Number of request headers received.


Definition at line 177 of file components/service/sl_http_server/inc/sl_http_server_types.h

type#

sl_http_server_request_type_t sl_http_server_request_s::type

Type of the request (GET, POST, etc.)


Definition at line 178 of file components/service/sl_http_server/inc/sl_http_server_types.h

request_data_length#

uint32_t sl_http_server_request_s::request_data_length

Length of the request data.


Definition at line 179 of file components/service/sl_http_server/inc/sl_http_server_types.h