Wi-Fi advanced scan configuration options.

Indicates the configuration parameters for an advanced Wi-Fi scan operation.

Public Attributes#

int32_t

RSSI level to trigger advanced scan.

uint32_t

RSSI level change to trigger advanced scan.

uint16_t

Time spent on each channel during active scan (milliseconds)

uint16_t

Time spent on each channel during passive scan (milliseconds)

uint8_t

Flag to start advanced scan immediately.

uint8_t

Flag to send multiple probes to AP. If the value is set to 1, a probe request would be sent to all access points in addition to the connected SSID.

Public Attribute Documentation#

trigger_level#

int32_t sl_wifi_advanced_scan_configuration_t::trigger_level

RSSI level to trigger advanced scan.


Definition at line 244 of file components/protocol/wifi/inc/sl_wifi_types.h

trigger_level_change#

uint32_t sl_wifi_advanced_scan_configuration_t::trigger_level_change

RSSI level change to trigger advanced scan.


Definition at line 245 of file components/protocol/wifi/inc/sl_wifi_types.h

active_channel_time#

uint16_t sl_wifi_advanced_scan_configuration_t::active_channel_time

Time spent on each channel during active scan (milliseconds)


Definition at line 246 of file components/protocol/wifi/inc/sl_wifi_types.h

passive_channel_time#

uint16_t sl_wifi_advanced_scan_configuration_t::passive_channel_time

Time spent on each channel during passive scan (milliseconds)


Definition at line 247 of file components/protocol/wifi/inc/sl_wifi_types.h

enable_instant_scan#

uint8_t sl_wifi_advanced_scan_configuration_t::enable_instant_scan

Flag to start advanced scan immediately.


Definition at line 248 of file components/protocol/wifi/inc/sl_wifi_types.h

enable_multi_probe#

uint8_t sl_wifi_advanced_scan_configuration_t::enable_multi_probe

Flag to send multiple probes to AP. If the value is set to 1, a probe request would be sent to all access points in addition to the connected SSID.


Definition at line 250 of file components/protocol/wifi/inc/sl_wifi_types.h