You are viewing documentation for version:
3.3.3
Wi-Fi device status structure.
Indicates the status of various Wi-Fi functionalities on the device. It uses bit fields to indicate the status of different Wi-Fi modes and operations.
Public Attributes# uint8_t
WiFi Access point active.
uint8_t
WiFi promiscuous mode active.
Public Attribute Documentation# client_active# uint8_t sl_wifi_status_t::client_active WiFi Client active.
ap_active# uint8_t sl_wifi_status_t::ap_active WiFi Access point active.
monitor_mode_active# uint8_t sl_wifi_status_t::monitor_mode_active WiFi promiscuous mode active.
wfd_go_active# uint8_t sl_wifi_status_t::wfd_go_active Reserved Status bit.
wfd_client_active# uint8_t sl_wifi_status_t::wfd_client_active Reserved Status bit.
scan_active# uint8_t sl_wifi_status_t::scan_active Scan in Progress.
_reserved# uint8_t sl_wifi_status_t::_reserved Reserved Status bit.
_reserved2# uint8_t sl_wifi_status_t::_reserved2 Reserved Status bit.