Functions#
This section provides a reference to the ECDSA Crypto API functions.
Functions#
sl_status_t
sl_si91x_ecdsa(sl_si91x_ecdsa_config_t *config, uint8_t *output)
To sign or verify the message according to the given configuration.
Function Documentation#
sl_si91x_ecdsa#
sl_status_t sl_si91x_ecdsa (sl_si91x_ecdsa_config_t * config, uint8_t * output)
To sign or verify the message according to the given configuration.
Parameters
[in] | config | Configuration object of type sl_si91x_ecdsa_config_t |
[out] | output | Buffer to store the output. |
This is a blocking API. Returns
sl_status_t. For more information on status codes, refer to SL STATUS DOCUMENTATION.
Definition at line
183
of file components/device/silabs/si91x/wireless/crypto/ecdsa/inc/sl_si91x_ecdsa.h