PSRAM Driver#


Introduction#

PSRAM (Pseudo Static Random Access Memory) is a random-access memory whose internal structure is based on dynamic memory with refresh control signals generated internally, in the standby mode, so that it can mimic the functionality of a static memory. It combines the high density of DRAM with the ease-of-use of true SRAM. The M4 core communicates with the PSRAM via Quad SPI interface.

Memory Architecture DiagramMemory Architecture Diagram

To enhance performance, PSRAM access is optimized through a cache memory system. This "Modified Harvard Architecture" allows the core to access instructions and data through separate caches (Data cache and Instruction cache), which then access the common PSRAM. When data is already in the cache ("Cache Hit"), it’s quickly provided to the core. If not ("Cache Miss"), the cache retrieves the data from PSRAM, improving overall performance.

The architecture is designed to ensure efficient memory access, with the data path supported by a 16KB, 4-way set associative cache with a 32-byte cache line. The instruction path leverages the existing instruction cache shared between flash and PSRAM.

PSRAM AccessibilityPSRAM Accessibility


Configuration#

PSRAM Device Configuration#

The PSRAM Driver offers configuring the following:

  • Read-Write type

    • Normal: This is supported only in SPI interface mode. Supports a maximum frequency of 33MHz. Uses normal read and normal write commands.

    • Fast: Supported in SPI and QPI mode. Uses fast read and normal write.

    • Quad IO: Supported in SPI and QPI mode. Uses fast quad read and write.

  • Interface mode

    • SPI Mode (Serial IO)

    • QPI Mode (Quad IO)

Linker configurations#

The text segment, data segment, bss, heap, and stack can be placed in PSRAM by installing the respective components present under "PSRAM Linker Configurations" from the "SOFTWARE COMPONENTS" GUI. Since PSRAM is already initialized in the bootloader, these components can be installed and the respective segments can be placed in PSRAM without installing the "PSRAM Core" component and without initializing PSRAM from the application.

  • For more information on configuring available parameters, see the respective peripheral example readme document.


Usage#

The PSRAM Driver and QSPI are initialized by the bootloader with Quad IO read-write type and QPI interface. The application is not required to reinitialize the PSRAM device and QSPI unless the configurations required are different from the default set by the bootloader.

The PSRAM device handle "PSRAM_Device" of type sl_psram_info_type_t is defined in "sl_si91x_psram_handle.c".

sl_si91x_psram_uninit assumes that PSRAM was initialized with QPI mode and exits QPI mode within the definition. If the PSRAM configuration in the boot code has SPI mode enabled, the user is expected to comment out the exit QPI mode function call in sl_si91x_psram_uninit.

To reconfigure and initialize PSRAM, set the required configurations from the PSRAM Core component and call sl_si91x_psram_init within the application.

Modules#

sl_psram_id_type_t

sl_psram_info_type_t

PSRAM Commands

PSRAM Timings

PSRAM GPIO Pin Sets

PSRAM Chip Select and Base Address

PSRAM Pin Configuration

Enumerations#

enum
PSRAM_SUCCESS
PSRAM_FAILURE
PSRAM_UNKNOWN
PSRAM_UNKNOWN_DEVICE
PSRAM_CLOCK_INIT_FAILURE
PSRAM_NOT_INITIALIZED
PSRAM_SUPPORTED_DEVICE
PSRAM_DEVICE_MISMATCH
PSRAM_INVALID_HSIZE
PSRAM_NULL_ADDRESS
PSRAM_INVALID_ADDRESS_LENGTH
PSRAM_AUTO_MODE
PSRAM_MANUAL_MODE
PSRAM_UNSUPPORTED_SECURITY
PSRAM_MAX_SEC_SEGMENT_REACH
}

PSRAM return error code.

enum
_WRAP16
_WRAP32
_WRAP64
_WRAP512
}

Wrap burst size enum.

enum
DMA_NONE
DMA_DONE
DMA_FAIL
}

PSRAM DMA status enum.

Functions#

To configure and initialize the PSRAM Device.

To uninitialize the PSRAM Device.

To reset the PSRAM Device.

sl_si91x_psram_manual_write_in_blocking_mode(uint32_t addr, void *SourceBuf, uint8_t hSize, uint32_t length)

To write data to PSRAM in manual mode.

sl_si91x_psram_manual_read_in_blocking_mode(uint32_t addr, void *DestBuf, uint8_t hSize, uint32_t length)

To read data from PSRAM in manual mode.

sl_si91x_psram_manual_write_in_dma_mode(uint32_t addr, void *SourceBuf, uint8_t hSize, uint32_t length, sl_psram_dma_status_type_t *dmaStatus)

To write data to PSRAM in manual mode using DMA.

sl_si91x_psram_manual_read_in_dma_mode(uint32_t addr, void *DestBuf, uint8_t hSize, uint32_t length, sl_psram_dma_status_type_t *dmaStatus)

To read data from PSRAM in manual mode using DMA.

To put the PSRAM device in sleep mode.

To exit the PSRAM device from sleep mode.

To enable CTR encryption-decryption on PSRAM.

Enumeration Documentation#

sl_psram_return_type_t#

sl_psram_return_type_t

PSRAM return error code.

Enumerator
PSRAM_SUCCESS

No error.

PSRAM_FAILURE

Generic error.

PSRAM_UNKNOWN

Unknown request.

PSRAM_UNKNOWN_DEVICE

Unknown PSRAM Device.

PSRAM_CLOCK_INIT_FAILURE

Clock init failure.

PSRAM_NOT_INITIALIZED

PSRAM not initialized.

PSRAM_SUPPORTED_DEVICE

PSRAM Device supported.

PSRAM_DEVICE_MISMATCH

PSRAM Device mismatch.

PSRAM_INVALID_HSIZE

Invalid size of element.

PSRAM_NULL_ADDRESS

Null address.

PSRAM_INVALID_ADDRESS_LENGTH

Invalid address length.

PSRAM_AUTO_MODE

PSRAM Auto mode.

PSRAM_MANUAL_MODE

PSRAM Manual mode.

PSRAM_UNSUPPORTED_SECURITY

Unsupported security.

PSRAM_MAX_SEC_SEGMENT_REACH

Maximum secure segment reached.


sl_psram_burst_size_type_t#

sl_psram_burst_size_type_t

Wrap burst size enum.

Enumerator
_WRAP16

Burst wrap size 16 Bytes.

_WRAP32

Burst wrap size 32 Bytes.

_WRAP64

Burst wrap size 64 Bytes.

_WRAP512

Burst wrap size 512 Bytes.


sl_psram_dma_status_type_t#

sl_psram_dma_status_type_t

PSRAM DMA status enum.

Enumerator
DMA_NONE

DMA status default.

DMA_DONE

DMA transfer completed.

DMA_FAIL

DMA transfer failed.


Function Documentation#

sl_si91x_psram_init#

sl_psram_return_type_t sl_si91x_psram_init (void )

To configure and initialize the PSRAM Device.

Parameters
TypeDirectionArgument NameDescription
voidN/A

Returns


  • Status code indicating the result.

    • PSRAM_SUCCESS: Initialization successful

    • PSRAM_FAILURE: Initialization failed

Note

  • The configurations for initialization are taken from the PSRAM Device config header file. The selection of the configuration file happens implicitly based on the radio board selection.


sl_si91x_psram_uninit#

sl_psram_return_type_t sl_si91x_psram_uninit (void )

To uninitialize the PSRAM Device.

Parameters
TypeDirectionArgument NameDescription
voidN/A

Returns


  • Status code indicating the result.

    • PSRAM_SUCCESS: Uninitialization successful

    • PSRAM_FAILURE: Uninitialization failed


sl_si91x_psram_reset#

sl_psram_return_type_t sl_si91x_psram_reset (void )

To reset the PSRAM Device.

Parameters
TypeDirectionArgument NameDescription
voidN/A

Returns

  • Status code indicating the result.

    • PSRAM_SUCCESS: Reset successful

    • PSRAM_FAILURE: Reset failed


sl_si91x_psram_manual_write_in_blocking_mode#

sl_psram_return_type_t sl_si91x_psram_manual_write_in_blocking_mode (uint32_t addr, void * SourceBuf, uint8_t hSize, uint32_t length)

To write data to PSRAM in manual mode.

Parameters
TypeDirectionArgument NameDescription
uint32_t[in]addr

PSRAM address for the write operation

void *[in]SourceBuf

Reference to the source buffer

uint8_t[in]hSize

Size of each element

uint32_t[in]length

Number of elements for the write operation

Returns

  • Status code indicating the result.

    • PSRAM_SUCCESS: Write operation successful

    • PSRAM_FAILURE: Write operation failed


sl_si91x_psram_manual_read_in_blocking_mode#

sl_psram_return_type_t sl_si91x_psram_manual_read_in_blocking_mode (uint32_t addr, void * DestBuf, uint8_t hSize, uint32_t length)

To read data from PSRAM in manual mode.

Parameters
TypeDirectionArgument NameDescription
uint32_t[in]addr

PSRAM address for the read operation

void *[in]DestBuf

Size of each element

uint8_t[in]hSize

Number of elements for the read operation

uint32_t[out]length

Reference to the destination buffer

Returns

  • Status code indicating the result.

    • PSRAM_SUCCESS: Read operation successful

    • PSRAM_FAILURE: Read operation failed


sl_si91x_psram_manual_write_in_dma_mode#

sl_psram_return_type_t sl_si91x_psram_manual_write_in_dma_mode (uint32_t addr, void * SourceBuf, uint8_t hSize, uint32_t length, sl_psram_dma_status_type_t * dmaStatus)

To write data to PSRAM in manual mode using DMA.

Parameters
TypeDirectionArgument NameDescription
uint32_t[in]addr

PSRAM address for the write operation

void *[in]SourceBuf

Reference to the source buffer

uint8_t[in]hSize

Size of each element

uint32_t[in]length

Number of elements for the write operation

sl_psram_dma_status_type_t *[out]dmaStatus

DMA operation completion status

Returns

  • Status code indicating the result.

    • PSRAM_SUCCESS: Write operation successful

    • PSRAM_FAILURE: Write operation failed


sl_si91x_psram_manual_read_in_dma_mode#

sl_psram_return_type_t sl_si91x_psram_manual_read_in_dma_mode (uint32_t addr, void * DestBuf, uint8_t hSize, uint32_t length, sl_psram_dma_status_type_t * dmaStatus)

To read data from PSRAM in manual mode using DMA.

Parameters
TypeDirectionArgument NameDescription
uint32_t[in]addr

PSRAM address for the read operation

void *[out]DestBuf

Reference to the destination buffer

uint8_t[in]hSize

Size of each element

uint32_t[in]length

Number of elements for the read operation

sl_psram_dma_status_type_t *[out]dmaStatus

DMA operation completion status

Returns

  • Status code indicating the result.

    • PSRAM_SUCCESS: Read operation successful

    • PSRAM_FAILURE: Read operation failed


sl_si91x_psram_sleep#

sl_psram_return_type_t sl_si91x_psram_sleep (void )

To put the PSRAM device in sleep mode.

Parameters
TypeDirectionArgument NameDescription
voidN/A

Sleep mode is a feature that puts the PSRAM device in an ultra-low power state, while retaining the stored data.

Returns

  • Status code indicating the result.

    • PSRAM_SUCCESS: Sleep mode enabled successfully

    • PSRAM_FAILURE: Failed to enable sleep mode


sl_si91x_psram_wakeup#

sl_psram_return_type_t sl_si91x_psram_wakeup (void )

To exit the PSRAM device from sleep mode.

Parameters
TypeDirectionArgument NameDescription
voidN/A

Returns

  • Status code indicating the result.

    • PSRAM_SUCCESS: Wakeup successful

    • PSRAM_FAILURE: Wakeup failed

Note

  • This function call re-initializes the PSRAM device after the wakeup sequence.


sl_si91x_psram_enable_encry_decry#

sl_psram_return_type_t sl_si91x_psram_enable_encry_decry (uint16_t keySize)

To enable CTR encryption-decryption on PSRAM.

Parameters
TypeDirectionArgument NameDescription
uint16_t[in]keySize

Pass 128/256-bit size

Returns

  • Status code indicating the result.

    • PSRAM_SUCCESS: Encryption-decryption enabled successfully

    • PSRAM_FAILURE: Failed to enable encryption-decryption