PSRAM GPIO Pin Sets#
Macros#
#define
GPIO Pin Set 52 to 57.
#define
GPIO Pin Set 0 to 5.
#define
GPIO Pin Set 46 to 51 with Chip Select 0.
#define
GPIO Pin Set 46 to 51 with Chip Select 1.
#define
GPIO Pin Set 46 to 57 with Chip Select 0.
#define
GPIO Pin Set 46 to 57 with Chip Select 1.
Macro Definition Documentation#
PSRAM_GPIO_PIN_SET_52_TO_57#
#define PSRAM_GPIO_PIN_SET_52_TO_57Value:
1
GPIO Pin Set 52 to 57.
Definition at line
40
of file components/device/silabs/si91x/mcu/drivers/unified_api/inc/sl_si91x_psram_handle.h
PSRAM_GPIO_PIN_SET_0_TO_5#
#define PSRAM_GPIO_PIN_SET_0_TO_5Value:
2
GPIO Pin Set 0 to 5.
Definition at line
41
of file components/device/silabs/si91x/mcu/drivers/unified_api/inc/sl_si91x_psram_handle.h
PSRAM_GPIO_PIN_SET_46_TO_51_CS_0#
#define PSRAM_GPIO_PIN_SET_46_TO_51_CS_0Value:
3
GPIO Pin Set 46 to 51 with Chip Select 0.
Definition at line
42
of file components/device/silabs/si91x/mcu/drivers/unified_api/inc/sl_si91x_psram_handle.h
PSRAM_GPIO_PIN_SET_46_TO_51_CS_1#
#define PSRAM_GPIO_PIN_SET_46_TO_51_CS_1Value:
4
GPIO Pin Set 46 to 51 with Chip Select 1.
Definition at line
43
of file components/device/silabs/si91x/mcu/drivers/unified_api/inc/sl_si91x_psram_handle.h
PSRAM_GPIO_PIN_SET_46_TO_57_CS_0#
#define PSRAM_GPIO_PIN_SET_46_TO_57_CS_0Value:
5
GPIO Pin Set 46 to 57 with Chip Select 0.
Definition at line
44
of file components/device/silabs/si91x/mcu/drivers/unified_api/inc/sl_si91x_psram_handle.h
PSRAM_GPIO_PIN_SET_46_TO_57_CS_1#
#define PSRAM_GPIO_PIN_SET_46_TO_57_CS_1Value:
6
GPIO Pin Set 46 to 57 with Chip Select 1.
Definition at line
45
of file components/device/silabs/si91x/mcu/drivers/unified_api/inc/sl_si91x_psram_handle.h