Structure to hold the parameters of Analog comparator configurations.

Public Attributes#

uint8_t

Comparator number, sl_analog_comparator_number_t for possible values.

uint8_t

Comparator non-inverting input, sl_analog_comparator_inputs_t for possible values.

uint8_t

Comparator inverting input, sl_analog_comparator_inputs_t for possible values.

uint8_t

Comparator hysteresis control value, sl_analog_comparator_hystersis_values_t.

boolean_t

True to enable and false to disable filter for comparator.

Public Attribute Documentation#

comparator_number#

uint8_t sl_analog_comparator_config_t::comparator_number

Comparator number, sl_analog_comparator_number_t for possible values.


Definition at line 177 of file components/device/silabs/si91x/mcu/drivers/unified_api/inc/sl_si91x_analog_comparator.h

non_inverting_input#

uint8_t sl_analog_comparator_config_t::non_inverting_input

Comparator non-inverting input, sl_analog_comparator_inputs_t for possible values.


Definition at line 179 of file components/device/silabs/si91x/mcu/drivers/unified_api/inc/sl_si91x_analog_comparator.h

inverting_input#

uint8_t sl_analog_comparator_config_t::inverting_input

Comparator inverting input, sl_analog_comparator_inputs_t for possible values.


Definition at line 180 of file components/device/silabs/si91x/mcu/drivers/unified_api/inc/sl_si91x_analog_comparator.h

hystersis_value#

uint8_t sl_analog_comparator_config_t::hystersis_value

Comparator hysteresis control value, sl_analog_comparator_hystersis_values_t.


Definition at line 181 of file components/device/silabs/si91x/mcu/drivers/unified_api/inc/sl_si91x_analog_comparator.h

is_filter_enabled#

boolean_t sl_analog_comparator_config_t::is_filter_enabled

True to enable and false to disable filter for comparator.


Definition at line 182 of file components/device/silabs/si91x/mcu/drivers/unified_api/inc/sl_si91x_analog_comparator.h