Structure to monitor and handle the sensors.
Public Attributes#
void *
Sensor handle.
void *
Sensor control handle.
uint8_t
Sensor event bits.
uint8_t
Sensor event acknowledge.
uint16_t
Maximum number of samples for the sensors.
Sensor configuration structure.
sl_sensor_impl_type_t *
Sensor implementation structure.
Sensor status.
TimerHandle_t
RTOS timer handle.
Public Attribute Documentation#
sensor_handle#
void* sl_sensor_handle_t::sensor_handle
Sensor handle.
Definition at line
218
of file components/device/silabs/si91x/mcu/drivers/service/sensorhub/inc/sensor_hub.h
ctrl_handle#
void* sl_sensor_handle_t::ctrl_handle
Sensor control handle.
Definition at line
219
of file components/device/silabs/si91x/mcu/drivers/service/sensorhub/inc/sensor_hub.h
sensor_event_bit#
uint8_t sl_sensor_handle_t::sensor_event_bit
Sensor event bits.
Definition at line
220
of file components/device/silabs/si91x/mcu/drivers/service/sensorhub/inc/sensor_hub.h
event_ack#
uint8_t sl_sensor_handle_t::event_ack
Sensor event acknowledge.
Definition at line
221
of file components/device/silabs/si91x/mcu/drivers/service/sensorhub/inc/sensor_hub.h
max_samples#
uint16_t sl_sensor_handle_t::max_samples
Maximum number of samples for the sensors.
Definition at line
222
of file components/device/silabs/si91x/mcu/drivers/service/sensorhub/inc/sensor_hub.h
config_st#
sl_sensor_info_t* sl_sensor_handle_t::config_st
Sensor configuration structure.
Definition at line
223
of file components/device/silabs/si91x/mcu/drivers/service/sensorhub/inc/sensor_hub.h
sensor_impl#
sl_sensor_impl_type_t* sl_sensor_handle_t::sensor_impl
Sensor implementation structure.
Definition at line
224
of file components/device/silabs/si91x/mcu/drivers/service/sensorhub/inc/sensor_hub.h
sensor_status#
sl_sensor_status_t sl_sensor_handle_t::sensor_status
Sensor status.
Definition at line
225
of file components/device/silabs/si91x/mcu/drivers/service/sensorhub/inc/sensor_hub.h
timer_handle#
TimerHandle_t sl_sensor_handle_t::timer_handle
RTOS timer handle.
Definition at line
226
of file components/device/silabs/si91x/mcu/drivers/service/sensorhub/inc/sensor_hub.h