Structure for storing the Sensor Configurations from the User.
Public Attributes#
char *
Name of the sensor.
int16_t
GPIO Interrupt Configurations.
uint16_t
GPIO pin for sampling the sensor data.
uint32_t
Sensor data sampling interval.
uint8_t
Address of sensor.
uint16_t
Channel for adc.
union sl_sensor_info_t::@2
sl_sensor_id_t
Sensor id.
sl_sensor_bus_t
Protocol for the sensor(spi/i2c/adc)
Sensor Mode(Enumeration)
sl_sensor_range_t
Range of sensor.
Data delivery mode for the sensor.
sl_sensor_data_group_t *
Pointer to Sensor data storage structure.
Public Attribute Documentation#
sensor_name#
char* sl_sensor_info_t::sensor_name
Name of the sensor.
Definition at line
197
of file components/device/silabs/si91x/mcu/drivers/service/sensorhub/inc/sensor_hub.h
sensor_intr_type#
int16_t sl_sensor_info_t::sensor_intr_type
GPIO Interrupt Configurations.
Definition at line
198
of file components/device/silabs/si91x/mcu/drivers/service/sensorhub/inc/sensor_hub.h
sampling_intr_req_pin#
uint16_t sl_sensor_info_t::sampling_intr_req_pin
GPIO pin for sampling the sensor data.
Definition at line
199
of file components/device/silabs/si91x/mcu/drivers/service/sensorhub/inc/sensor_hub.h
sampling_interval#
uint32_t sl_sensor_info_t::sampling_interval
Sensor data sampling interval.
Definition at line
200
of file components/device/silabs/si91x/mcu/drivers/service/sensorhub/inc/sensor_hub.h
address#
uint8_t sl_sensor_info_t::address
Address of sensor.
Definition at line
202
of file components/device/silabs/si91x/mcu/drivers/service/sensorhub/inc/sensor_hub.h
channel#
uint16_t sl_sensor_info_t::channel
Channel for adc.
Definition at line
203
of file components/device/silabs/si91x/mcu/drivers/service/sensorhub/inc/sensor_hub.h
@3#
union sl_sensor_info_t::@2 sl_sensor_info_t::@3
Definition at line
204
of file components/device/silabs/si91x/mcu/drivers/service/sensorhub/inc/sensor_hub.h
sensor_id#
sl_sensor_id_t sl_sensor_info_t::sensor_id
Sensor id.
Definition at line
205
of file components/device/silabs/si91x/mcu/drivers/service/sensorhub/inc/sensor_hub.h
sensor_bus#
sl_sensor_bus_t sl_sensor_info_t::sensor_bus
Protocol for the sensor(spi/i2c/adc)
Definition at line
206
of file components/device/silabs/si91x/mcu/drivers/service/sensorhub/inc/sensor_hub.h
sensor_mode#
sl_sensor_mode_t sl_sensor_info_t::sensor_mode
Sensor Mode(Enumeration)
Definition at line
207
of file components/device/silabs/si91x/mcu/drivers/service/sensorhub/inc/sensor_hub.h
sensor_range#
sl_sensor_range_t sl_sensor_info_t::sensor_range
Range of sensor.
Definition at line
208
of file components/device/silabs/si91x/mcu/drivers/service/sensorhub/inc/sensor_hub.h
data_deliver#
sl_data_deliver_type_t sl_sensor_info_t::data_deliver
Data delivery mode for the sensor.
Definition at line
209
of file components/device/silabs/si91x/mcu/drivers/service/sensorhub/inc/sensor_hub.h
sensor_data_ptr#
sl_sensor_data_group_t* sl_sensor_info_t::sensor_data_ptr
Pointer to Sensor data storage structure.
Definition at line
210
of file components/device/silabs/si91x/mcu/drivers/service/sensorhub/inc/sensor_hub.h