WebSocket send request structure.

This structure holds the parameters for sending a WebSocket frame, including the opcode, payload buffer, and payload length.

Public Attributes#

Opcode (TEXT, BINARY, and so on.).

const uint8_t *

Pointer to the payload.

size_t

Length of the payload.

Public Attribute Documentation#

opcode#

sl_websocket_opcode_t sl_websocket_send_request_t::opcode

Opcode (TEXT, BINARY, and so on.).


Definition at line 136 of file components/service/sl_websocket_client/inc/sl_websocket_client_types.h

buffer#

const uint8_t* sl_websocket_send_request_t::buffer

Pointer to the payload.


Definition at line 137 of file components/service/sl_websocket_client/inc/sl_websocket_client_types.h

length#

size_t sl_websocket_send_request_t::length

Length of the payload.


Definition at line 138 of file components/service/sl_websocket_client/inc/sl_websocket_client_types.h