Structure representing the AE (Advertising extension) device to periodic list.
Public Attribute Documentation#
type#
uint8_t rsi_ble_ae_dev_to_periodic_list_s::type
uint8_t, Type Type Values Description 1 Adding Device to Periodic Advertising list 2 Removing Device from Periodic Advertising list 3 Clearing Periodic Advertising List
adv_addr_type#
uint8_t rsi_ble_ae_dev_to_periodic_list_s::adv_addr_type
uint8_t, Advertiser Address Type, this parameter indicates the type of address being used in the connection request packets
      0x00          Public Device Address or Public Identity Address
      0x01          Random Device Address or Random (static) Identity Address
All other values Reserved for future use
adv_addr#
uint8_t rsi_ble_ae_dev_to_periodic_list_s::adv_addr[RSI_DEV_ADDR_LEN]
uint8_t, Advertiser Address[6]
adv_sid#
uint8_t rsi_ble_ae_dev_to_periodic_list_s::adv_sid
uint8_t, Advertising_Sid, Value of the Advertising SID subfield in the ADI field of the PDU, Range : 0x00 to 0x0F