Structure to set the scan parameters for BLE Active Scanning.
Public Attribute Documentation#
own_addr_type#
uint8_t rsi_ble_ae_set_scan_params_s::own_addr_type
unit8_t,The Own Address Type parameter indicates the type of address being used in the scan request packets Value Parameter Description 0x00 Public Device Address 0x01 Random Device Address 0x02 Controller generates the Resolvable Private Address based on the local IRK from the resolving list. If the resolving list contains no matching entry, then use the public address. 0x03 Controller generates the Resolvable Private Address based on the local IRK from the resolving list. If the resolving list contains no matching entry, then use the random address from LE_Set_Random_Address. All other values Reserved for future use
scanning_filter_policy#
uint8_t rsi_ble_ae_set_scan_params_s::scanning_filter_policy
uint8_t, It is used to determine whether the Filter Accept List is used
           0x00            Basic unfiltered scanning filter policy
           0x01            Basic filtered scanning filter policy
           0x02            Extended unfiltered scanning filter policy
           0x03            Extended filtered scanning filter policy
     All other values      Reserved for future use
scanning_phys#
uint8_t rsi_ble_ae_set_scan_params_s::scanning_phys
uint8_t, The Scanning_PHYs parameter indicates the PHY(s) on which the advertising packets should be received on the primary advertising physical channel.
       0             Scan advertisements on the LE 1M PHY
       2             Scan advertisements on the LE Coded PHY
 All other bits      Reserved for future use
ScanParams#
ae_scan_params_t rsi_ble_ae_set_scan_params_s::ScanParams[SUPPORTED_SCNNING_PHYS]
ScanParams is an array of variable of structure ae_scan_params_s