Structure indicates the received write information from the remote device.
Public Attribute Documentation#
pkt_type#
uint8_t rsi_ble_event_write_s::pkt_type
Type of the event received from the remote device
- RSI_BLE_WRITE_CMD_EVENT 0x01 
- RSI_BLE_WRITE_REQUEST_EVENT 0x02 
- RSI_BLE_NOTIFICATION_EVENT 0x03 
- RSI_BLE_INDICATION_EVENT 0x04 
att_value#
uint8_t rsi_ble_event_write_s::att_value[RSI_DEV_ATT_LEN]
This contains the attribute value. The maximum value is 240, refer to RSI_DEV_ATT_LEN Macro