MDNS instance configuration.

Public Attributes#

Protocol to use for mDNS from sl_mdns_protocol_t.

sl_ip_version_t

IP version to use for mDNS from sl_ip_version_t.

char

Host Name to use for the mDNS Instance. The host name Should contain dot(.) at the end (for example, "wiseconnect.local."). The string length should not exceed 32 including NULL terminator.

Public Attribute Documentation#

protocol#

sl_mdns_protocol_t sl_mdns_configuration_t::protocol

Protocol to use for mDNS from sl_mdns_protocol_t.


type#

sl_ip_version_t sl_mdns_configuration_t::type

IP version to use for mDNS from sl_ip_version_t.


host_name#

char sl_mdns_configuration_t::host_name[32]

Host Name to use for the mDNS Instance. The host name Should contain dot(.) at the end (for example, "wiseconnect.local."). The string length should not exceed 32 including NULL terminator.