mDNS service

Public Attributes#

const char *

mDNS instance service name

const char *

mDNS service type

const char *

mDNS service message

uint16_t

Service port number.

uint16_t

Service TTL.

sl_ipv4_address_t

IPv4 address of service. (In case of offload mode, it is provided by embedded network stack.)

sl_ipv6_address_t

IPv6 address of service. (In case of offload mode, it is provided by embedded network stack.)

Public Attribute Documentation#

instance_name#

const char* sl_mdns_service_t::instance_name

mDNS instance service name


service_type#

const char* sl_mdns_service_t::service_type

mDNS service type


service_message#

const char* sl_mdns_service_t::service_message

mDNS service message


port#

uint16_t sl_mdns_service_t::port

Service port number.


ttl#

uint16_t sl_mdns_service_t::ttl

Service TTL.


ipv4#

sl_ipv4_address_t sl_mdns_service_t::ipv4

IPv4 address of service. (In case of offload mode, it is provided by embedded network stack.)


ipv6#

sl_ipv6_address_t sl_mdns_service_t::ipv6

IPv6 address of service. (In case of offload mode, it is provided by embedded network stack.)