Boot configuration structure.

Note

Public Attributes#

uint16_t

Operation mode, one of the values from sl_wifi_operation_mode_t.

uint16_t

Coexistence mode, one of the values from sl_wifi_coex_mode_t.

uint32_t
uint32_t
uint32_t
uint32_t
uint32_t
uint32_t
uint32_t
uint32_t

Public Attribute Documentation#

oper_mode#

uint16_t sl_wifi_system_boot_configuration_t::oper_mode

Operation mode, one of the values from sl_wifi_operation_mode_t.


coex_mode#

uint16_t sl_wifi_system_boot_configuration_t::coex_mode

Coexistence mode, one of the values from sl_wifi_coex_mode_t.


feature_bit_map#

uint32_t sl_wifi_system_boot_configuration_t::feature_bit_map

Feature bit map, Feature Bitmap.


tcp_ip_feature_bit_map#

uint32_t sl_wifi_system_boot_configuration_t::tcp_ip_feature_bit_map

TCP/IP feature bit map, TCP/IP Feature Bitmap.


custom_feature_bit_map#

uint32_t sl_wifi_system_boot_configuration_t::custom_feature_bit_map

Custom feature bit map, Custom Feature Bitmap.


ext_custom_feature_bit_map#

uint32_t sl_wifi_system_boot_configuration_t::ext_custom_feature_bit_map

Extended custom feature bit map, Extended Custom Feature Bitmap.


bt_feature_bit_map#

uint32_t sl_wifi_system_boot_configuration_t::bt_feature_bit_map

BT featured bit map, Bluetooth Feature Bitmap.


ext_tcp_ip_feature_bit_map#

uint32_t sl_wifi_system_boot_configuration_t::ext_tcp_ip_feature_bit_map

Extended TCP/IP feature bit map, Extended TCP/IP Feature Bitmap.


ble_feature_bit_map#

uint32_t sl_wifi_system_boot_configuration_t::ble_feature_bit_map

BLE feature bitmap, BLE Feature Bitmap.


ble_ext_feature_bit_map#

uint32_t sl_wifi_system_boot_configuration_t::ble_ext_feature_bit_map

BLE extended feature bitmap, Extended BLE Custom Feature Bitmap.


config_feature_bit_map#

uint32_t sl_wifi_system_boot_configuration_t::config_feature_bit_map

Config feature bitmap, Configuration Feature Bitmap.