NWP buffer allocation command parameters The summation of all three ratios should max 10 and the ratio should be in decimal value.

Public Attributes#

uint8_t
uint8_t
uint8_t

Public Attribute Documentation#

tx_ratio_in_buffer_pool#

uint8_t sl_wifi_system_dynamic_pool_t::tx_ratio_in_buffer_pool

tx ratio


rx_ratio_in_buffer_pool#

uint8_t sl_wifi_system_dynamic_pool_t::rx_ratio_in_buffer_pool

rx ratio


global_ratio_in_buffer_pool#

uint8_t sl_wifi_system_dynamic_pool_t::global_ratio_in_buffer_pool

global ratio