You are viewing documentation for version:
Firmware version information structure.
Public Attributes#
uint8_t
Build number of the firmware.
uint8_t
Security version indicating if security is enabled or disabled.
uint8_t
Minor version number of the firmware.
uint8_t
Major version number of the firmware.
Public Attribute Documentation#
build_num#
uint8_t sl_wifi_system_fw_version_info_t::build_num
Build number of the firmware.
security_version#
uint8_t sl_wifi_system_fw_version_info_t::security_version
Security version indicating if security is enabled or disabled.
minor#
uint8_t sl_wifi_system_fw_version_info_t::minor
Minor version number of the firmware.
major#
uint8_t sl_wifi_system_fw_version_info_t::major
Major version number of the firmware.