Timeout Configuration Structure.
Public Attributes#
Time spent on each channel when performing active scan (milliseconds). Default value of 100 millisecs is used when SL_WIFI_DEFAULT_ACTIVE_CHANNEL_SCAN_TIME is passed.
Authentication and association timeout value. Default value of 300 millisecs is used when SL_WIFI_DEFAULT_AUTH_ASSOCIATION_TIMEOUT is passed.
Keep Alive Timeout value. Default value of 30 seconds is used when SL_WIFI_DEFAULT_KEEP_ALIVE_TIMEOUT is passed.
Time spent on each channel when performing passive scan (milliseconds). The minimum passive_scan_timeout_value is 5 millisecs, and maximum is 1000 milliseconds. Default value of 400 milliseconds is used when SL_WIFI_DEFAULT_PASSIVE_CHANNEL_SCAN_TIME is passed.
Public Attribute Documentation#
active_chan_scan_timeout_value#
uint16_t sl_wifi_timeout_t::active_chan_scan_timeout_value
Time spent on each channel when performing active scan (milliseconds). Default value of 100 millisecs is used when SL_WIFI_DEFAULT_ACTIVE_CHANNEL_SCAN_TIME is passed.
auth_assoc_timeout_value#
uint16_t sl_wifi_timeout_t::auth_assoc_timeout_value
Authentication and association timeout value. Default value of 300 millisecs is used when SL_WIFI_DEFAULT_AUTH_ASSOCIATION_TIMEOUT is passed.
keep_alive_timeout_value#
uint16_t sl_wifi_timeout_t::keep_alive_timeout_value
Keep Alive Timeout value. Default value of 30 seconds is used when SL_WIFI_DEFAULT_KEEP_ALIVE_TIMEOUT is passed.
passive_scan_timeout_value#
uint16_t sl_wifi_timeout_t::passive_scan_timeout_value
Time spent on each channel when performing passive scan (milliseconds). The minimum passive_scan_timeout_value is 5 millisecs, and maximum is 1000 milliseconds. Default value of 400 milliseconds is used when SL_WIFI_DEFAULT_PASSIVE_CHANNEL_SCAN_TIME is passed.