Network Credential AT Commands#
This section describes AT commands for managing network credentials.
Commands#
net-cred-wifipsk#
Configure a Pre-shared Key (PSK) for use while joining an Access Point.
Command Format#
at+net-cred-wifipsk=<credential-id>,<psk>Related SDK API
sl_net_wifi_psk_credential_entry_tin sl_net_wifi_types.h
Pre-conditions#
oper_mode=0(Wi-Fi Client)
Parameters#
credential-id#
A unique networking credentials identifier. Contains a numeric value that corresponds to one of the values of the enum sl_net_credential_id_t in sl_net_constants.h.
psk#
A string that contains the PSK to use for authentication with the specified SSID when connecting to the Access Point.
Response#
OKon successERROR <error code>in case of failure. Possible error codes are the same as those returned by the sl_net_set_credential API.
Notes#
This command sets a structure of type sl_net_wifi_psk_credential_entry_t with the given PSK and then invokes the sl_net_set_credential API to save the credential information under the given credential-id.
Examples#
// Set PSK "Silabs1234" for Credential ID 1
at+net-cred-wifipsk=1,"Silabs1234"