Network Profile AT Commands#
This section describes AT commands for configuring Wi-Fi client profiles.
Commands#
net-sta-cred#
Configure SSID, credentials, security, and encryption for connecting to an Access Point.
Command Format#
at+net-sta-cred=<profile-id>,<ssid>,<credential-id>,<security>,<encryption>Related SDK API
sl_net_wifi_client_profile_tin sl_net_wifi_types.h, which contains the following structures:sl_wifi_client_configuration_tin sl_wifi_types.h
Pre-conditions#
oper_mode=0(Wi-Fi Client)
Parameters#
profile-id#
A unique networking profile identifier. Contains a numeric value that corresponds to one of the values of the enum sl_net_profile_id_t.
ssid#
A string containing the SSID of the Access Point to connect to. Can optionally be enclosed in double quotes. Must be enclosed in double quotes (") if it contains commas.
credential-id#
A unique Wi-Fi credential set identifier which was previously configured using the net-set-credential command.
security#
Optional. The type of Wi-Fi authentication used by the Access Point (for example, WPA3). Contains a numeric value that corresponds to one of the values of the enum sl_wifi_security_t in sl_wifi_constants.h. Note some values are not currently supported, as indicated in the linked enum declaration. This is defaulted to WPA2 if not specified (for example, WPA3).
encryption#
Optional. The type of Wi-Fi encryption used by the Access Point. Contains a numeric value that corresponds to one of the values of the enum sl_wifi_encryption_t in sl_wifi_constants.h. This is set to 0 (default encryption) if not specified.
Response#
OKon successERROR <error code>in case of failure. Possible error codes are the same as those returned by the sl_net_set_profile API.
Notes#
When this command or any command beginning with
at-net-sta-is sent for the first time for a givenprofile-idvalue, the SiWx91x device will:Initialize an
sl_net_wifi_client_profile_tstructure instance (from sl_net_wifi_types.h) for the givenprofile-idvalue, with the initial values denoted by the macroDEFAULT_WIFI_CLIENT_PROFILE(from sl_net_default_values.h).Overwrite the specific structure members for the given
profile-idvalue, based on the parameters passed in this command.Invoke the sl_net_set_profile API to save the profile information under the given
profile-id.
When any subsequent command beginning with
at+net-sta-is sent for the sameprofile-id, the SiWx91x device will perform the second and third steps given above (that is, overwrite specific structure members and save the profile).
Examples#
// SSID set to "Silabs AP" and Credential ID to 1 with WPA3 authentication and default encryption
at+net-sta-cred=0,"Silabs AP",1,7,0net-sta-chan#
Configure the channel for connecting to the Access Point.
Command Format#
at+net-sta-chan=<profile-id>,<channel>,<band>,<bandwidth>Related SDK API
sl_net_wifi_client_profile_tin sl_net_wifi_types.h, which contains the following structures:sl_wifi_client_configuration_tin sl_wifi_types.h
Pre-conditions#
oper_mode=0(Wi-Fi Client)
Parameters#
profile-id#
A unique networking profile identifier. Contains a numeric value that corresponds to one of the values of the enum sl_net_profile_id_t.
channel#
Wi-Fi channel number.
band#
Optional. The Wi-Fi frequency band from which the channel is selected (for example, 2.4GHz). Contains a numeric value that corresponds to one of the values of the enum sl_wifi_band_t in sl_wifi_constants.h. Note some values are not currently supported, as indicated in the linked enum declaration.
bandwidth#
Optional. The width of the channel (for example, 20MHz). Contains a numeric value that corresponds to one of the values of the enum sl_wifi_bandwidth_t in sl_wifi_constants.h. Note some values are not currently supported, as indicated in the linked enum declaration.
Response#
OKon successERROR <error code>in case of failure. Possible error codes are the same as those returned by the sl_net_set_profile API.
Notes#
When this command or any command beginning with
at+net-sta-is sent for the first time for a givenprofile-idvalue, the SiWx91x device will:Initialize an
sl_net_wifi_client_profile_tstructure instance (from sl_net_wifi_types.h) for the givenprofile-idvalue, with the initial values denoted by the macroDEFAULT_WIFI_CLIENT_PROFILE(from sl_net_default_values.h).Overwrite the specific structure members for the given
profile-idvalue, based on the parameters passed in this command.Invoke the sl_net_set_profile API to save the profile information under the given
profile-id.
When any subsequent command beginning with
at+net-sta-is sent for the sameprofile-id, the SiWx91x device will perform the second and third steps given above i.e. just overwrite specific structure members and save the profile.
Examples#
// Connect over channel 1 with automatic selection of band and bandwidth
at+net-sta-chan=0,1,0,0net-sta-bss#
Configure the Basic Service Set Identifier (BSSID) for connecting to the Access Point.
Command Format#
at+net-sta-bss=<profile-id>,<bssid>,<bss-type>Related SDK API
sl_net_wifi_client_profile_tin sl_net_wifi_types.h, which contains the following structures:sl_wifi_client_configuration_tin sl_wifi_types.h
Pre-conditions#
oper_mode=0(Wi-Fi Client)
Parameters#
profile-id#
A unique networking profile identifier. Contains a numeric value that corresponds to one of the values of the enum sl_net_profile_id_t.
bssid#
The BSSID of the Access Point to connect to, represented as a 6-byte MAC address with a colon (:) separating every byte. Leave empty or set to 0 if there is no BSSID.
bss-type#
Optional. The type of BSSID that is specified for the Access Point. Contains a numeric value that corresponds to one of the values of the enum sl_wifi_bss_type_t in sl_wifi_constants.h.
Response#
OKon successERROR <error code>in case of failure. Possible error codes are the same as those returned by the sl_net_set_profile API.
Notes#
When this command or any command beginning with
at+net-sta-is sent for the first time for a givenprofile-idvalue, the SiWx91x device will:Initialize an
sl_net_wifi_client_profile_tstructure instance (from sl_net_wifi_types.h) for the given profile-id value, with the initial values denoted by the macroDEFAULT_WIFI_CLIENT_PROFILE(from sl_net_default_values.h).Overwrite the specific structure members for the given
profile-idvalue, based on the parameters passed in this command.Invoke the sl_net_set_profile API to save the profile information under the given
profile-id.
When any subsequent command beginning with at+net-sta- is sent for the same
profile-id, the SiWx91x device will perform the second and third steps given above i.e. just overwrite specific structure members and save the profile.
Examples#
// BSSID of 0 with BSS Type of 'Infrastructure'
at+net-sta-bss=0,0,0
// Set a specific BSSID
at+net-sta-bss=0,54:37:bb:ef:89:ddnet-sta-opt#
Configure the client options (such as scanning before the join) to use when connecting to the Access Point
Command Format#
at+net-sta-opt=<profile-id>,<client-options>,<channel-bitmap-2-4>,<channel-bitmap-5>,<priority>Related SDK API
sl_net_wifi_client_profile_tin sl_net_wifi_types.h, which contains the following structures:sl_wifi_client_configuration_tin sl_wifi_types.h
Pre-conditions#
oper_mode=0(Wi-Fi Client)
Parameters#
profile-id#
A unique networking profile identifier. Contains a numeric value that corresponds to one of the values of the enum sl_net_profile_id_t.
client-options#
Reserved
channel-bitmap-2-4#
A bitmap of channel numbers to scan for the given SSID from within the 2.4GHz band. Each channel number is selected by setting the (n - 1)th bit in the bitmap to 1 (channel 1 is selected by setting bit 0, channel 2 by setting bit 1, and so on). If this is left empty or passed as 0, all channels are scanned.
channel-bitmap-5#
Currently not supported. A bitmap of channel numbers to scan for the given SSID from within the 5GHz. Each channel number is selected by setting the (n - 1)th bit in the bitmap to 1 (channel 1 is selected by setting bit 0, channel 2 by setting bit 1, and so on). If this is left empty or passed as 0, all channels are scanned.
priority#
The relative priority of the network profile when Auto Join is invoked.
Note: Auto Join is invoked by issuing the net-up command with a
profile-idof0xFF.
Response#
OKon successERROR <error code>in case of failure. Possible error codes are the same as those returned by the sl_net_set_profile API.
Notes#
When this command or any command beginning with
at+net-sta-is sent for the first time for a givenprofile-idvalue, the SiWx91x device will:Initialize an
sl_net_wifi_client_profile_tstructure instance (from sl_net_wifi_types.h) for the givenprofile-idvalue, with the initial values denoted by the macroDEFAULT_WIFI_CLIENT_PROFILE(from sl_net_default_values.h).Overwrite the specific structure members for the given
profile-idvalue, based on the parameters passed in this command.Invoke the sl_net_set_profile API to save the profile information under the given
profile-id.
When any subsequent command beginning with
at+net-sta-is sent for the sameprofile-id, the SiWx91x device will perform the second and third steps given above i.e. just overwrite specific structure members and save the profile.
Examples#
// Configure the scanning of the 2.4GHz channel 1 prior to join
at+net-sta-opt=0,,1,0net-sta-ip#
Configure the IP address allocation to be performed by the IP networking layer after connecting to the Access Point.
Command Format#
at+net-sta-ip=<profile-id>,<ip-mode>,<ip-type>,<host-name>,<station-ip>,<ipv6-global-ip>,<gateway-ip>,<ipv4-netmask>Related SDK API
sl_net_wifi_client_profile_tin sl_net_wifi_types.h, which contains the following structures:sl_wifi_client_configuration_tin sl_wifi_types.h
Pre-conditions#
oper_mode=0(Wi-Fi Client)
Parameters#
profile-id#
A unique networking profile identifier. Contains a numeric value that corresponds to one of the values of the enum sl_net_profile_id_t.
ip-mode#
The type of IP address configuration used in the IP networking layer (for example, DHCP). Contains a numeric value that corresponds to one of the values of the enum sl_ip_management_t in sl_ip_types.h.
ip-type#
The type(s) of IP address to be configured (for example, an IPv4 address). Contains a numeric value that corresponds to one of the values of the enum sl_ip_address_type_t in sl_ip_types.h. You can combine multiple values by using a bitwise or (|) operator (for example, (1<<2) | (1<<3) (= 12) specifies both IPv5 and IPv6 address configurations).
host-name#
Optional. A string denoting the host name to be set for the SiWx91x device in the Wi-Fi network. Can be empty if host name does not need to be set to a specific string.
station-ip#
Human readable IPv4 address or IPv6 link-local address to be set for the SiWx91x device when ip-mode is 1 (Static).
ipv6-global-ip#
Human readable IPv6 global address whenip-mode is 1 (Static) and ip-version is 6 (IPv6).
gateway-ip#
Human readable Gateway IPv4/IPv6 address.
ipv4-netmask#
Human readable IPv4 subnet mask when ip-version is 4 (IPv4) and ip-mode is 1 (Static).
Response#
OKon successERROR <error code>in case of failure. Possible error codes are the same as those returned by the sl_net_set_profile API.
Notes#
When this command or any command beginning with
at+net-sta-is sent for the first time for a givenprofile-idvalue, the SiWx91x device will:Initialize an
sl_net_wifi_client_profile_tstructure instance (from sl_net_wifi_types.h) for the givenprofile-idvalue, with the initial values denoted by the macroDEFAULT_WIFI_CLIENT_PROFILE(from sl_net_default_values.h).Overwrite the specific structure members for the given
profile-idvalue, based on the parameters passed in this command.Invoke the sl_net_set_profile API to save the profile information under the given
profile-id.
When any subsequent command beginning with
at+net-sta-is sent for the sameprofile-id, the SiWx91x device will perform the second and third steps given above i.e. just overwrite specific structure members and save the profile.
Examples#
// DHCP IP allocation with IPv4 with no specific host name
at+net-sta-ip=0,2,4,,0,,0,0
// Static IP allocation
at+net-sta-ip=1,1,4,,192.168.1.51,,192.168.1.1,255.255.255.0