You are viewing documentation for version:
3.5.1
Structure representing the BLE enhanced connection request.
This structure is used to define the parameters for a BLE enhanced connection request, which includes the address type and address of the device to connect, filter policy, own address type, scan interval, scan window, connection interval, connection latency, supervision timeout, and connection event length.
Public Attribute Documentation# dev_addr_type# uint8_t rsi_ble_req_enhance_conn_s::dev_addr_type Address type of the device to connect
dev_addr# uint8_t rsi_ble_req_enhance_conn_s::dev_addr[RSI_DEV_ADDR_LEN] Address of the device to connect
filter_policy# uint8_t rsi_ble_req_enhance_conn_s::filter_policy Filter policy
own_addr_type# uint8_t rsi_ble_req_enhance_conn_s::own_addr_type Own address type
le_scan_interval# uint16_t rsi_ble_req_enhance_conn_s::le_scan_interval Scan interval
le_scan_window# uint16_t rsi_ble_req_enhance_conn_s::le_scan_window Scan window
conn_interval_min# uint16_t rsi_ble_req_enhance_conn_s::conn_interval_min Minimum connection interval
conn_interval_max# uint16_t rsi_ble_req_enhance_conn_s::conn_interval_max Maximum connection interval
conn_latency# uint16_t rsi_ble_req_enhance_conn_s::conn_latency Connection latency
supervision_tout# uint16_t rsi_ble_req_enhance_conn_s::supervision_tout Supervision timeout
min_ce_length# uint16_t rsi_ble_req_enhance_conn_s::min_ce_length Minimum connection event length
max_ce_length# uint16_t rsi_ble_req_enhance_conn_s::max_ce_length Maximum connection event length