Structure represents a BLE scan request.
Public Attribute Documentation#
scan_type#
uint8_t rsi_ble_req_scan_s::scan_type
Scanning type
SCAN_TYPE_ACTIVE 0x01
SCAN_TYPE_PASSIVE 0x00
filter_type#
uint8_t rsi_ble_req_scan_s::filter_type
To filter incoming advertising reports
FILTERING_DISABLED = 0 (default)
ACCEPTLIST_FILTERING = 1 Note
In order to allow only acceptlisted devices, need to add bd_addr into acceptlist by calling rsi_ble_addto_acceptlist() API
own_addr_type#
uint8_t rsi_ble_req_scan_s::own_addr_type
Address type of the local device
#define LE_PUBLIC_ADDRESS 0x00#define LE_RANDOM_ADDRESS 0x01#define LE_RESOLVABLE_PUBLIC_ADDRESS 0x02#define LE_RESOLVABLE_RANDOM_ADDRESS 0x03
scan_int#
uint16_t rsi_ble_req_scan_s::scan_int
Scan interval
This is defined as the time interval from when the Controller started its last LE scan until it begins the subsequent LE scan.Range: 0x0004 to 0x4000
scan_win#
uint16_t rsi_ble_req_scan_s::scan_win
Scan window
The duration of the LE scan. LE_Scan_Window should be less than or equal to LE_Scan_IntervalRange: 0x0004 to 0x4000