Summary of Certifications#

The SiWx917 underwent certification in the Connectivity, Security, and Optimization categories as part of the Wi-Fi Alliance. This is a station certification program. Below are the certification categories.

CLASSIFICATION CERTIFICATION
Connectivity
  • 2.4 GHz Spectrum Capabilities
  • Wi-Fi CERTIFIED 6® Release 2
  • Wi-Fi CERTIFIED™ b
  • Wi-Fi CERTIFIED™ g
  • Wi-Fi CERTIFIED™ n
Optimization
  • WMM®
  • Wi-Fi Agile Multiband™
Security
  • Protected Management Frames
  • WPA2™-Personal 2021-01
  • WPA3™-Personal 2023-12

Note: SiWx917 supports Wi-Fi CERTIFIED 6 with 20MHz STA-only certification and Wi-Fi Agile Multiband™.