Firmware Fallback A and B#

Introduction#

The Firmware Fallback feature provides mechanisms for managing A/B firmware upgrades and fallback operations in Si91x devices. It ensures system reliability by maintaining two firmware slots and enabling fallback to a stable firmware version in case of an upgrade failure Additionally, this functionality requires a specific MBR configuration to work.

Features#

  • A/B Slot Management: Maintains two firmware slots (Slot A and Slot B) for active and backup firmware.

  • Integrity Checks: Verifies firmware integrity using CRC and magic word validation.

  • Fallback Mechanism: Switches to a backup firmware slot in case of failure.

  • OTA Support: Supports Over-The-Air (OTA) firmware upgrades with slot management.

Usage#

The following steps outline the typical usage of the Firmware Fallback feature, providing clear guidance on how and when to use each API in the firmware update process:

  1. At OTA initiation:
    Use sl_si91x_ab_upgrade_get_rps_configs to parse the incoming firmware image header. This step extracts critical metadata, such as image size and type, and is typically performed when the first chunk of OTA data arrives. This information helps determine the type of update being performed and allocate the necessary resources for the update process.

  2. Preparing the inactive slot for new firmware:
    Before writing the new firmware, use sl_si91x_flash_erase to clear the inactive slot. This ensures the slot is ready to receive the new firmware image and prevents flash corruption. The inactive slot can be identified using sl_si91x_ab_get_slot_info, which retrieves the current slot configuration.

  3. Writing firmware during OTA download:
    Use sl_si91x_flash_write to store the received firmware chunks in the inactive slot as they arrive from the OTA source. This function should be called for each chunk of data received during the OTA session, ensuring proper addressing and offset management. This step ensures that the new firmware is written correctly to the designated slot.

  4. Validating the downloaded firmware:
    After the firmware download is complete, use sl_si91x_verify_image to validate the integrity of the downloaded firmware image. This step ensures that only properly formed and uncorrupted firmware is considered for activation.

  5. Updating slot metadata after successful validation:
    Once the new firmware is verified, use sl_si91x_ab_upgrade_set_slot_info to update the slot metadata with information about the new firmware. This prepares the slot for activation and ensures the slot information accurately reflects the valid firmware version. This step is essential to mark the new firmware as ready for execution.

  6. Retrieving current slot information:
    Use sl_si91x_ab_get_slot_info to determine which slot (A or B) is currently active for both M4 and NWP processors. This function also retrieves information about firmware locations and sizes in flash memory. It is typically called before performing any operation that depends on knowing the current slot configuration. This step is useful for diagnostics and ensuring the correct slot is being used.

  7. Switching slots manually or for recovery:
    Use sl_si91x_toggle_slot_info only in specific scenarios, such as recovering from a failed firmware update by switching back to the previously working slot or manually switching between existing firmware versions. After calling this function, the system must be reset to load the newly activated firmware. This function should not be part of the regular update process and should only be used when both slots contain valid firmware images.

  8. Burning NWP security version:
    Use sl_si91x_burn_nwp_security_version to burn the NWP security version to OTP memory. This step is critical for enforcing firmware security on the NWP (Network Wireless Processor). Burning the security version to OTP (One-Time Programmable) memory ensures that only firmware images with a security version equal to or greater than the burned value can be executed. This mechanism prevents rollback attacks by disallowing the loading of older, potentially vulnerable firmware versions. This operation is irreversible and should be performed with caution, typically after a successful firmware update or when upgrading the device's security requirements.

  9. Loading QSPI keys for inline decryption:
    Use sl_si91x_fallback_load_qspi_keys to load the QSPI keys for enabling inline decryption for M4 slot applications during fallback. This function is essential when firmware images are stored in encrypted form in QSPI flash. Loading the QSPI keys allows the hardware to transparently decrypt firmware as it is read and executed, ensuring both security and performance. This step should be performed before attempting to boot or validate encrypted firmware images, and the keys must be securely provisioned and managed.

  10. Soft reset for NWP firmware:
    Use sl_si91x_nwp_soft_reset_from_updater to perform a soft reset of the NWP firmware for fallback and keep the NWP firmware in boot mode. This function is typically used after updating or recovering the NWP firmware, ensuring that the NWP restarts cleanly and enters a known state. Keeping the NWP in boot mode allows for further maintenance operations, such as additional firmware updates, diagnostics, or recovery actions, before normal operation resumes. This step is important for robust fallback and recovery workflows.

  11. Default NWP firmware selection:
    Use sl_si91x_select_default_nwp_fw to select the default NWP firmware image to load. This API allows you to specify which NWP (Network Wireless Processor) firmware slot (A or B) should be used as the default on the next boot. The function takes a firmware image number as input (0 for slot A, 1 for slot B) and updates the boot configuration accordingly. This is particularly useful for scenarios where you want to manually control which firmware version is active, such as after a successful OTA update, for testing a new firmware image, or for recovery purposes if the current firmware is not functioning as expected. The function returns 0 on success, a negative value if the command fails.

  12. Executing the firmware from the active slot:
    Use sl_si91x_jump_to_m4_application to execute the firmware from the currently active slot. This function is primarily used by the M4 Updater to branch to the appropriate application after reading slot information. It transfers control from the updater to the main application, completing the boot process. This step ensures the system boots into the correct firmware version.

The following three APIs are required only when full encryption is enabled:

By following these steps, the Firmware Fallback feature ensures a seamless and reliable firmware update process, with mechanisms for recovery and fallback in case of failures. This design minimizes downtime and ensures the device remains operational even in the event of update issues.

Benefits#

  • Ensures system reliability with robust fallback mechanisms.

  • Simplifies OTA firmware upgrades with A/B slot management.

  • Eliminates the need to transfer the image from the download region to the execution region, enabling faster updates.

  • Provides APIs for seamless integration into application firmware.

  • Optimizes flash memory usage for firmware storage.

Modules#

ota_image_info_t

sl_si91x_fw_fallback_request_t

sl_si91x_fw_fallback_config_t

SlotInfo_t

M4_SlotManagement_t

NWP_SlotManagement_t

sl_si91x_fw_ab_slot_management_t

Enumerations#

enum
SL_SI91X_AB_OTA_IMAGE_TYPE_M4 = 1
SL_SI91X_AB_OTA_IMAGE_TYPE_NWP = 2
SL_SI91X_AB_OTA_IMAGE_TYPE_MAX
}

Enum for A/B OTA image types.

enum
SLOT_A = 1
SLOT_B = 2
SLOT_MAX
}

Enum for AB slot identifiers.

enum
SL_SI91X_DATA_PACKET = 0
SL_SI91X_HEADER_PACKET = 1
}

Enum for A/B chunk types(Payload / Header).

enum
SL_SI91X_AB_FALLBACK_WRITE_CMD = 1
SL_SI91X_AB_FALLBACK_READ_CMD = 2
SL_SI91X_AB_FALLBACK_ERASE_CMD = 3
SL_SI91X_AB_FALLBACK_INTEGRITY_CHECK_CMD = 4
SL_SI91X_AB_FALLBACK_BURN_SECURITY_VERSION = 5
SL_SI91X_AB_FALLBACK_LOAD_QSPI_KEYS = 6
SL_SI91X_AB_FALLBACK_SOFT_RESET = 7
SL_SI91X_AB_FALLBACK_MAX_CMD = 8
}

SI91x-specific A/B fallback command types.

Functions#

sl_status_t
sl_si91x_ab_upgrade_get_rps_configs(const uint8_t *image_buffer, ota_image_info_t *ota_st)

Retrieves A/B fallback OTA image configuration from the provided image buffer. This function checks the magic number in the image buffer to validate the firmware header. If valid, it populates the ota_image_info_t structure with the image offset and size from the firmware header.

sl_status_t
sl_si91x_flash_write(uint32_t address, const uint8_t *buffer, uint32_t length)

Write data to flash memory. This function writes data to the specified flash memory address. This function will work for A/B firmware only.

sl_status_t
sl_si91x_fw_fallback_ota_flash_write(const sl_si91x_fw_fallback_config_t *config, const uint8_t *data_buffer)

Unified flash write function for OTA firmware updates. This function handles all flash write operations for OTA firmware updates using the provided configuration structure and data buffer. This function will work for A/B firmware only.

sl_status_t
sl_si91x_flash_read(uint32_t address, uint8_t *buffer, uint32_t length)

Read data from flash memory. This function reads data from the specified flash memory address. This function will work for A/B firmware only.

sl_status_t
sl_si91x_ab_upgrade_set_slot_info(uint32_t new_image_offset, uint32_t new_image_size, sl_si91x_ab_image_type_t image_type)

Updates slot information and switches active slots on OTA updates. This function updates the slot information and switches the active slots based on the provided parameters. This function will work for A/B firmware only.

sl_status_t
sl_si91x_flash_erase(uint32_t address, uint32_t length)

Erases data from flash memory sector-wise.

sl_status_t
sl_si91x_ab_get_slot_info(sl_si91x_fw_ab_slot_management_t *slot_info_t)

Retrieves the current slot information. This function reads the current slot information from flash memory. This function will work for A/B firmware only.

sl_status_t
sl_si91x_toggle_slot_info(bool toggle_m4_image, bool toggle_nwp_image)

Toggles the active slot information for M4 or NWP. This function retrieves the current slot information, checks which slot is active, and switches to the other slot by calling the sl_si91x_set_slot_info API.

sl_status_t
sl_si91x_get_m4_app_addr(uint32_t *app_addr)

Retrieves the M4 application address from the active firmware slot. This function reads firmware slot information from flash memory, verifies its integrity using a magic word and CRC check, and determines the application address for the currently active M4 slot. This function will work for A/B firmware only.

void

Jumps to the M4 application.

sl_status_t
sl_si91x_verify_image(uint32_t flash_address)

Checks the integrity of the firmware for Fallback. This function sends a command to check the integrity of the firmware at the specified flash memory address. It populates the request structure with the necessary parameters and sends the command to the firmware. This function will work for A/B firmware only.

int16_t
sl_si91x_select_default_nwp_fw(const uint8_t fw_image_number)

Selects the default NWP firmware image to load. This function sends the appropriate command to select which firmware image (0 for slot A, 1 for slot B) should be loaded on boot.

sl_status_t
sl_si91x_burn_nwp_security_version(uint32_t flash_address)

Burns the NWP security version to OTP memory. This function reads the security version from the NWP firmware at the specified flash address and burns it into the One-Time Programmable (OTP) memory. This function will work for A/B fallback feature only and only for NWP Firmware.

sl_status_t
sl_si91x_fallback_load_qspi_keys(uint32_t image_offset)

Requests to load QSPI keys. This function requests to load QSPI keys for to enable the inline decryption for M4 slot firmware for fallback. This function will work for A/B firmware only.

void
sl_si91x_nwp_soft_reset_from_updater(const uint32_t m4_slot_image_offset)

Performs a soft reset of the NWP firmware.

Macros#

#define

Magic number located in RPS Header.

#define
SLI_SI91X_RPS_HEADER_SIZE sizeof(sl_si91x_firmware_header_t)

Firmware header size in bytes.

#define

Flash memory chunk size for erase operations.

#define

Base address of M4 and NWP flash memory.

#define

NWP flash base address.

#define

Slot information flash offsets.

#define
SLI_SI91X_BACKUP_SLOT_INFO_FLASH_OFFSET (SLI_SI91X_SLOT_INFO_FLASH_OFFSET + SL_SI91X_CHUNK_LENGTH)

Backup slot offset.

#define

Image type identifiers in RPS.

#define

NWP RPS image type.

#define

OTA image chunk size.

#define

Timeout for NWP responses.

#define

Timeout for selecting default firmware.

#define

Magic word to verify slot information integrity.

#define
CRC32_POLYNOMIAL 0x04C11DB7

CRC polynomial for slot information.

#define

Memory value to check for memory match.

#define

M4 updater OTA flag.

#define
SL_SI91X_AB_ERR_FLASH_READ ((sl_status_t)0xAB001)

A/B fallback: Flash read operation failed.

#define
SL_SI91X_AB_ERR_FLASH_VERIFY ((sl_status_t)0xAB002)

A/B fallback: Flash verification failure.

#define
SL_SI91X_AB_ERR_BACKUP_READ ((sl_status_t)0xAB003)

A/B fallback: Backup slot read failure.

#define
SL_SI91X_AB_ERR_BACKUP_VERIFY ((sl_status_t)0xAB004)

A/B fallback: CRC verification failed in backup slot.

#define
SL_SI91X_AB_ERR_CRC_MISMATCH ((sl_status_t)0xAB005)

A/B fallback: CRC mismatch detected.

#define
SL_SI91X_AB_ERR_MAGIC_NUMBER ((sl_status_t)0xAB006)

A/B fallback: Magic number mismatch error.

#define
SL_SI91X_AB_ERR_UNKNOWN_IMG ((sl_status_t)0xAB007)

A/B fallback: Unknown image type.

#define
SL_SI91X_AB_ERR_INVALID_SLOT_INFO ((sl_status_t)0xAB008)

A/B fallback: Invalid slot info.

#define
SL_SI91X_AB_ERR_ERASE_ACTIVE_SLOT ((sl_status_t)0xAB009)

A/B fallback: Invalid slot info.

Enumeration Documentation#

sl_si91x_ab_image_type_t#

sl_si91x_ab_image_type_t

Enum for A/B OTA image types.

Enumerator
SL_SI91X_AB_OTA_IMAGE_TYPE_M4

Image for M4 processor.

SL_SI91X_AB_OTA_IMAGE_TYPE_NWP

Image for NWP processor.

SL_SI91X_AB_OTA_IMAGE_TYPE_MAX

Maximum image type value.


sl_si91x_ab_slot_t#

sl_si91x_ab_slot_t

Enum for AB slot identifiers.

Enumerator
SLOT_A

Primary slot (typically the active firmware slot)

SLOT_B

Secondary slot (used for updates or fallback)

SLOT_MAX

Maximum number of slots (used for validation)


sl_si91x_chunk_type_t#

sl_si91x_chunk_type_t

Enum for A/B chunk types(Payload / Header).

Enumerator
SL_SI91X_DATA_PACKET

Chunk type for Data packet.

SL_SI91X_HEADER_PACKET

Chunk type for Header packet.


sl_si91x_ab_fallback_cmd_t#

sl_si91x_ab_fallback_cmd_t

SI91x-specific A/B fallback command types.

Enumerator
SL_SI91X_AB_FALLBACK_WRITE_CMD

Write firmware data for fallback.

SL_SI91X_AB_FALLBACK_READ_CMD

Read firmware data for verification.

SL_SI91X_AB_FALLBACK_ERASE_CMD

Erase fallback firmware slot.

SL_SI91X_AB_FALLBACK_INTEGRITY_CHECK_CMD

Perform integrity check before fallback.

SL_SI91X_AB_FALLBACK_BURN_SECURITY_VERSION

Burn security version.

SL_SI91X_AB_FALLBACK_LOAD_QSPI_KEYS

Load QSPI keys.

SL_SI91X_AB_FALLBACK_SOFT_RESET

NWP Soft reset for fallback.

SL_SI91X_AB_FALLBACK_MAX_CMD

Maximum fallback command value (for validation)


Function Documentation#

sl_si91x_ab_upgrade_get_rps_configs#

sl_status_t sl_si91x_ab_upgrade_get_rps_configs (const uint8_t * image_buffer, ota_image_info_t * ota_st)

Retrieves A/B fallback OTA image configuration from the provided image buffer. This function checks the magic number in the image buffer to validate the firmware header. If valid, it populates the ota_image_info_t structure with the image offset and size from the firmware header.

Parameters
TypeDirectionArgument NameDescription
const uint8_t *[in]image_buffer

Pointer to the buffer containing the firmware image.

ota_image_info_t *[out]ota_st

Pointer to the ota_image_info_t structure to be populated.

  • None

Returns

  • sl_status_t SL_STATUS_OK on success, or SL_STATUS_FAIL on failure. For more information on status codes, refer to SL STATUS DOCUMENTATION.


sl_si91x_flash_write#

sl_status_t sl_si91x_flash_write (uint32_t address, const uint8_t * buffer, uint32_t length)

Write data to flash memory. This function writes data to the specified flash memory address. This function will work for A/B firmware only.

Parameters
TypeDirectionArgument NameDescription
uint32_t[in]address

Flash memory address to write to.

const uint8_t *[in]buffer

Pointer to the data buffer.

uint32_t[in]length

Number of bytes to write (min 0 max 4096).

  • None

Returns

  • sl_status_t SL_STATUS_OK on success, error code otherwise. For more information on status codes, refer to SL STATUS DOCUMENTATION.


sl_si91x_fw_fallback_ota_flash_write#

sl_status_t sl_si91x_fw_fallback_ota_flash_write (const sl_si91x_fw_fallback_config_t * config, const uint8_t * data_buffer)

Unified flash write function for OTA firmware updates. This function handles all flash write operations for OTA firmware updates using the provided configuration structure and data buffer. This function will work for A/B firmware only.

Parameters
TypeDirectionArgument NameDescription
const sl_si91x_fw_fallback_config_t *[in]config

Pointer to the firmware fallback configuration structure.

const uint8_t *[in]data_buffer

Pointer to the data buffer to write.

  • None

Returns

  • sl_status_t SL_STATUS_OK on success, error code otherwise. For more information on status codes, refer to SL STATUS DOCUMENTATION.


sl_si91x_flash_read#

sl_status_t sl_si91x_flash_read (uint32_t address, uint8_t * buffer, uint32_t length)

Read data from flash memory. This function reads data from the specified flash memory address. This function will work for A/B firmware only.

Parameters
TypeDirectionArgument NameDescription
uint32_t[in]address

Flash memory address to read from M4.

uint8_t *[in]buffer

Pointer to the buffer to store read data.

uint32_t[in]length

Number of bytes to read.

  • None

Returns

  • sl_status_t SL_STATUS_OK on success, error code otherwise. For more information on status codes, refer to SL STATUS DOCUMENTATION.


sl_si91x_ab_upgrade_set_slot_info#

sl_status_t sl_si91x_ab_upgrade_set_slot_info (uint32_t new_image_offset, uint32_t new_image_size, sl_si91x_ab_image_type_t image_type)

Updates slot information and switches active slots on OTA updates. This function updates the slot information and switches the active slots based on the provided parameters. This function will work for A/B firmware only.

Parameters
TypeDirectionArgument NameDescription
uint32_t[in]new_image_offset

New image base address (used only during OTA update).

uint32_t[in]new_image_size

New image size (used only during OTA update).

sl_si91x_ab_image_type_t[in]image_type

Type of the image (M4 or NWP).

  • None

Returns

  • sl_status_t SL_STATUS_OK if successful, error code otherwise. For more information on status codes, refer to SL STATUS DOCUMENTATION.


sl_si91x_flash_erase#

sl_status_t sl_si91x_flash_erase (uint32_t address, uint32_t length)

Erases data from flash memory sector-wise.

Parameters
TypeDirectionArgument NameDescription
uint32_t[in]address

Starting flash memory address to erase (must be sector-aligned).

uint32_t[in]length

Number of bytes to erase (will be rounded up to sector size).

  • None

This function erases data from the specified flash memory address in sector-sized blocks. The erase operation will only work for A/B firmware slots and ensures that no partial sector erases occur.

Note

  • The erase operation is performed in full sectors. If the provided address or length does not align with sector boundaries, the function will round to the nearest sector boundary.

Returns

  • sl_status_t SL_STATUS_OK on success, error code otherwise. For more information on status codes, refer to SL STATUS DOCUMENTATION.


sl_si91x_ab_get_slot_info#

sl_status_t sl_si91x_ab_get_slot_info (sl_si91x_fw_ab_slot_management_t * slot_info_t)

Retrieves the current slot information. This function reads the current slot information from flash memory. This function will work for A/B firmware only.

Parameters
TypeDirectionArgument NameDescription
sl_si91x_fw_ab_slot_management_t *[out]slot_info_t

Pointer to the sl_si91x_fw_ab_slot_management_t structure to store the slot information.

  • None

Returns

  • sl_status_t SL_STATUS_OK if successful, error code otherwise.


sl_si91x_toggle_slot_info#

sl_status_t sl_si91x_toggle_slot_info (bool toggle_m4_image, bool toggle_nwp_image)

Toggles the active slot information for M4 or NWP. This function retrieves the current slot information, checks which slot is active, and switches to the other slot by calling the sl_si91x_set_slot_info API.

Parameters
TypeDirectionArgument NameDescription
bool[in]toggle_m4_image

Set to 1 to toggle M4 slot, 0 otherwise.

bool[in]toggle_nwp_image

Set to 1 to toggle NWP slot, 0 otherwise.

  • None

Returns

  • sl_status_t SL_STATUS_OK if successful, error code otherwise. For more information on status codes, refer to SL STATUS DOCUMENTATION.


sl_si91x_get_m4_app_addr#

sl_status_t sl_si91x_get_m4_app_addr (uint32_t * app_addr)

Retrieves the M4 application address from the active firmware slot. This function reads firmware slot information from flash memory, verifies its integrity using a magic word and CRC check, and determines the application address for the currently active M4 slot. This function will work for A/B firmware only.

Parameters
TypeDirectionArgument NameDescription
uint32_t *[out]app_addr

Pointer to store the retrieved application address.

  • None

If a CRC failure is detected in the primary slot information,
the function attempts to retrieve the slot information from a backup slot. Returns

  • SL_STATUS_OK If the operation is successful.

  • SL_SI91X_AB_ERR_FLASH_READ If reading slot information from flash fails.

  • SL_SI91X_AB_ERR_MAGIC_NUMBER If the magic word does not match the expected value.

  • SL_SI91X_AB_ERR_CRC_MISMATCH If the CRC verification fails.

  • SL_STATUS_INVALID_PARAMETER If the active slot is invalid. For more information on status codes, refer to SL STATUS DOCUMENTATION.


sl_si91x_jump_to_m4_application#

void sl_si91x_jump_to_m4_application (uint32_t app_addr)

Jumps to the M4 application.

Parameters
TypeDirectionArgument NameDescription
uint32_t[in]app_addr

Address of the application to jump to.

This function disables interrupts, fetches the stack pointer and reset handler from the application's vector table, sets the VTOR to point to the new application vector table, and branches to the reset handler. This function will work for A/B firmware only.


sl_si91x_verify_image#

sl_status_t sl_si91x_verify_image (uint32_t address)

Checks the integrity of the firmware for Fallback. This function sends a command to check the integrity of the firmware at the specified flash memory address. It populates the request structure with the necessary parameters and sends the command to the firmware. This function will work for A/B firmware only.

Parameters
TypeDirectionArgument NameDescription
uint32_t[in]address

Flash memory address to check integrity.

  • None

Returns

  • sl_status_t SL_STATUS_OK on success, error code otherwise. For more information on status codes, refer to SL STATUS DOCUMENTATION.


sl_si91x_select_default_nwp_fw#

int16_t sl_si91x_select_default_nwp_fw (const uint8_t fw_image_number)

Selects the default NWP firmware image to load. This function sends the appropriate command to select which firmware image (0 for slot A, 1 for slot B) should be loaded on boot.

Parameters
TypeDirectionArgument NameDescription
const uint8_t[in]fw_image_number

Firmware image number to select (0 for slot A, 1 for slot B)

  • None

Returns

  • int16_t - Error code

    • 0 : SUCCESS

    • < 0 : Command issue failed

    • -14 : Valid Firmware not present

    • -15 : Invalid Option/Command not supported For more information on status codes, refer to SL STATUS DOCUMENTATION.


sl_si91x_burn_nwp_security_version#

sl_status_t sl_si91x_burn_nwp_security_version (uint32_t flash_address)

Burns the NWP security version to OTP memory. This function reads the security version from the NWP firmware at the specified flash address and burns it into the One-Time Programmable (OTP) memory. This function will work for A/B fallback feature only and only for NWP Firmware.

Parameters
TypeDirectionArgument NameDescription
uint32_t[in]flash_address

Flash address of the NWP firmware to extract security version.

  • None

Returns

  • sl_status_t SL_STATUS_OK on success, error code otherwise. For more information on status codes, refer to SL STATUS DOCUMENTATION.


sl_si91x_fallback_load_qspi_keys#

sl_status_t sl_si91x_fallback_load_qspi_keys (uint32_t image_offset)

Requests to load QSPI keys. This function requests to load QSPI keys for to enable the inline decryption for M4 slot firmware for fallback. This function will work for A/B firmware only.

Parameters
TypeDirectionArgument NameDescription
uint32_t[in]image_offset

Offset of the image to load the QSPI keys to enable inline decryption for M4 slot firmware for fallback.

  • None

Returns

  • sl_status_t SL_STATUS_OK on success, error code otherwise. For more information on status codes, refer to SL STATUS DOCUMENTATION.


sl_si91x_nwp_soft_reset_from_updater#

void sl_si91x_nwp_soft_reset_from_updater (const uint32_t m4_slot_image_offset)

Performs a soft reset of the NWP firmware.

Parameters
TypeDirectionArgument NameDescription
const uint32_t[in]m4_slot_image_offset

Offset of the M4 slot image for fallback

This function sends a soft reset command to the NWP firmware for fallback and keep the NWP firmware in the boot mode. This function will work for A/B firmware only.


Macro Definition Documentation#

SLI_SI91X_RPS_MAGIC_NO#

#define SLI_SI91X_RPS_MAGIC_NO
Value:
0x900D900D

Magic number located in RPS Header.

Magic number in RPS header


SLI_SI91X_RPS_HEADER_SIZE#

#define SLI_SI91X_RPS_HEADER_SIZE
Value:
sizeof(sl_si91x_firmware_header_t)

Firmware header size in bytes.

Firmware RPS header size


SL_SI91X_CHUNK_LENGTH#

#define SL_SI91X_CHUNK_LENGTH
Value:
4096

Flash memory chunk size for erase operations.

Flash erase chunk length (4KB)


SLI_SI91X_M4_FLASH_BASE_ADDR#

#define SLI_SI91X_M4_FLASH_BASE_ADDR
Value:
0x8000000

Base address of M4 and NWP flash memory.

M4 flash base address


SLI_SI91X_NWP_FLASH_BASE_ADDR#

#define SLI_SI91X_NWP_FLASH_BASE_ADDR
Value:
0x4000000

NWP flash base address.


SLI_SI91X_SLOT_INFO_FLASH_OFFSET#

#define SLI_SI91X_SLOT_INFO_FLASH_OFFSET
Value:
0x81F1000

Slot information flash offsets.

Primary slot information offset


SLI_SI91X_BACKUP_SLOT_INFO_FLASH_OFFSET#

#define SLI_SI91X_BACKUP_SLOT_INFO_FLASH_OFFSET
Value:
  (SLI_SI91X_SLOT_INFO_FLASH_OFFSET + SL_SI91X_CHUNK_LENGTH)

Backup slot offset.


SL_SI91X_M4_RPS_BIT#

#define SL_SI91X_M4_RPS_BIT
Value:
1

Image type identifiers in RPS.

M4 RPS image type


SL_SI91X_NWP_RPS_BIT#

#define SL_SI91X_NWP_RPS_BIT
Value:
0

NWP RPS image type.


SL_SI91X_MAX_OTA_IMAGE_CHUNK_SIZE#

#define SL_SI91X_MAX_OTA_IMAGE_CHUNK_SIZE
Value:
1024

OTA image chunk size.

OTA firmware chunk size


SL_SI91X_NWP_RESPONSE_TIMEOUT#

#define SL_SI91X_NWP_RESPONSE_TIMEOUT
Value:
30000

Timeout for NWP responses.

NWP response timeout (30s)


SL_SI91X_DEFAULT_FW_SELECT_CMD_TIMEOUT#

#define SL_SI91X_DEFAULT_FW_SELECT_CMD_TIMEOUT
Value:
10000

Timeout for selecting default firmware.

Timeout for selecting default firmware (10s)


SLI_SI91X_AB_FW_SLOT_MAGIC_WORD#

#define SLI_SI91X_AB_FW_SLOT_MAGIC_WORD
Value:
0xA5A5B5B5

Magic word to verify slot information integrity.

Slot information magic word


CRC32_POLYNOMIAL#

#define CRC32_POLYNOMIAL
Value:
0x04C11DB7

CRC polynomial for slot information.

This macro defines the polynomial used for CRC32 calculation.


SL_SI91X_MEM_CHECK_VALUE#

#define SL_SI91X_MEM_CHECK_VALUE
Value:
0xAB11

Memory value to check for memory match.

Memory value to check for memory match


SL_SI91X_M4_UPDATER_OTA_FLAG#

#define SL_SI91X_M4_UPDATER_OTA_FLAG
Value:
0xEF

M4 updater OTA flag.

M4 updater OTA flag


SL_SI91X_AB_ERR_FLASH_READ#

#define SL_SI91X_AB_ERR_FLASH_READ
Value:
((sl_status_t)0xAB001)

A/B fallback: Flash read operation failed.


SL_SI91X_AB_ERR_FLASH_VERIFY#

#define SL_SI91X_AB_ERR_FLASH_VERIFY
Value:
((sl_status_t)0xAB002)

A/B fallback: Flash verification failure.


SL_SI91X_AB_ERR_BACKUP_READ#

#define SL_SI91X_AB_ERR_BACKUP_READ
Value:
((sl_status_t)0xAB003)

A/B fallback: Backup slot read failure.


SL_SI91X_AB_ERR_BACKUP_VERIFY#

#define SL_SI91X_AB_ERR_BACKUP_VERIFY
Value:
((sl_status_t)0xAB004)

A/B fallback: CRC verification failed in backup slot.


SL_SI91X_AB_ERR_CRC_MISMATCH#

#define SL_SI91X_AB_ERR_CRC_MISMATCH
Value:
((sl_status_t)0xAB005)

A/B fallback: CRC mismatch detected.


SL_SI91X_AB_ERR_MAGIC_NUMBER#

#define SL_SI91X_AB_ERR_MAGIC_NUMBER
Value:
((sl_status_t)0xAB006)

A/B fallback: Magic number mismatch error.


SL_SI91X_AB_ERR_UNKNOWN_IMG#

#define SL_SI91X_AB_ERR_UNKNOWN_IMG
Value:
((sl_status_t)0xAB007)

A/B fallback: Unknown image type.


SL_SI91X_AB_ERR_INVALID_SLOT_INFO#

#define SL_SI91X_AB_ERR_INVALID_SLOT_INFO
Value:
((sl_status_t)0xAB008)

A/B fallback: Invalid slot info.


SL_SI91X_AB_ERR_ERASE_ACTIVE_SLOT#

#define SL_SI91X_AB_ERR_ERASE_ACTIVE_SLOT
Value:
((sl_status_t)0xAB009)

A/B fallback: Invalid slot info.