Access Point#

Functions#

sl_status_t
sl_wifi_start_ap(sl_wifi_interface_t interface, const sl_wifi_ap_configuration_t *configuration)

Start a Wi-Fi access point (AP) interface.

sl_status_t
sl_wifi_reconfigure_ap(sl_wifi_interface_t interface, sl_wifi_ap_reconfiguration_t config)

Reconfigure the dynamic parameters of a Wi-Fi Access point (AP) interface.

sl_status_t
sl_wifi_set_ap_configuration(sl_wifi_interface_t interface, const sl_wifi_ap_configuration_t *configuration)

Set the configuration of a running Wi-Fi AP.

sl_status_t
sl_wifi_get_ap_configuration(sl_wifi_interface_t interface, sl_wifi_ap_configuration_t *configuration)

Get the configuration of a Wi-Fi AP interface.

sl_status_t
sl_wifi_set_advanced_ap_configuration(sl_wifi_interface_t interface, const sl_wifi_advanced_ap_configuration_t *configuration)

Set the advanced configuration options of a running Wi-Fi access point (AP).

sl_status_t
sl_wifi_get_advanced_ap_configuration(sl_wifi_interface_t interface, const sl_wifi_advanced_ap_configuration_t *configuration)

Get the advanced configuration options of a running Wi-Fi access point interface.

sl_status_t
sl_wifi_stop_ap(sl_wifi_interface_t interface)

Stop Wi-Fi access point.

sl_status_t
sl_wifi_disconnect_ap_client(sl_wifi_interface_t interface, const sl_mac_address_t *mac, sl_wifi_deauth_reason_t reason)

Disconnects a client with the specified MAC address from Access Point (AP).

sl_status_t
sl_wifi_get_ap_client_info(sl_wifi_interface_t interface, sl_wifi_client_info_response_t *client_info)

Return the Wi-Fi client information of all clients connected to the AP.

sl_status_t
sl_wifi_get_ap_client_list(sl_wifi_interface_t interface, uint16_t client_list_count, sl_mac_address_t *client_list)

Return a list of Wi-Fi clients connected to the Wi-Fi access point.

sl_status_t
sl_wifi_get_ap_client_count(sl_wifi_interface_t interface, uint32_t *client_count)

Provide the number of Wi-Fi clients connected to the Wi-Fi access point.

Function Documentation#

sl_wifi_start_ap#

sl_status_t sl_wifi_start_ap (sl_wifi_interface_t interface, const sl_wifi_ap_configuration_t * configuration)

Start a Wi-Fi access point (AP) interface.

Parameters
TypeDirectionArgument NameDescription
sl_wifi_interface_t[in]interface

Wi-Fi interface as identified by sl_wifi_interface_t

const sl_wifi_ap_configuration_t *[in]configuration

Wi-Fi AP configuration. See sl_wifi_ap_configuration_t

  • Pre-conditions:

Returns

Note

  • For AP mode with WPA3 security, only SAE-H2E method is supported. SAE hunting and pecking method is not supported. TKIP encryption mode is not supported. Encryption mode is automatically configured to CCMP. PMKSA is not supported in WPA3 AP mode.

  • Management Frame Protection (MFP) behavior in AP mode:

    • For WPA2 security: MFP is NOT automatically enabled. Use sl_wifi_set_mfp before calling this API if MFP is required.

    • For WPA3 security: MFP is automatically enabled as required by the WPA3 standard.


  • In FCC-certified modules,

    1. Region configuration is not supported and if triggered returns error SL_STATUS_SI91X_FEATURE_NOT_AVAILABLE.

    2. AP supports only 1 to 11 channels.

    3. AP does not advertise the Country IE.


sl_wifi_reconfigure_ap#

sl_status_t sl_wifi_reconfigure_ap (sl_wifi_interface_t interface, sl_wifi_ap_reconfiguration_t config)

Reconfigure the dynamic parameters of a Wi-Fi Access point (AP) interface.

Parameters
TypeDirectionArgument NameDescription
sl_wifi_interface_t[in]interface

Wi-Fi interface as identified by sl_wifi_interface_t

sl_wifi_ap_reconfiguration_t[in]config

Wi-Fi AP dynamic configuration. See sl_wifi_ap_reconfiguration_t

Returns

Note

  • The access point continues to transmit beacons when a client is connected, regardless of the beacon_stop configuration.


sl_wifi_set_ap_configuration#

sl_status_t sl_wifi_set_ap_configuration (sl_wifi_interface_t interface, const sl_wifi_ap_configuration_t * configuration)

Set the configuration of a running Wi-Fi AP.

Parameters
TypeDirectionArgument NameDescription
sl_wifi_interface_t[in]interface

Wi-Fi interface as identified by sl_wifi_interface_t

const sl_wifi_ap_configuration_t *[in]configuration

Wi-Fi AP configuration. See sl_wifi_ap_configuration_t

If the new configuration modifies vital settings such as SSID or security, the AP will be stopped and restarted automatically. Returns

Note

  • This API is not yet implemented.


sl_wifi_get_ap_configuration#

sl_status_t sl_wifi_get_ap_configuration (sl_wifi_interface_t interface, sl_wifi_ap_configuration_t * configuration)

Get the configuration of a Wi-Fi AP interface.

Parameters
TypeDirectionArgument NameDescription
sl_wifi_interface_t[in]interface

Wi-Fi interface as identified by sl_wifi_interface_t

sl_wifi_ap_configuration_t *[out]configuration

sl_wifi_ap_configuration_t object that contains the AP configuration.

  • Pre-conditions:

Returns


sl_wifi_set_advanced_ap_configuration#

sl_status_t sl_wifi_set_advanced_ap_configuration (sl_wifi_interface_t interface, const sl_wifi_advanced_ap_configuration_t * configuration)

Set the advanced configuration options of a running Wi-Fi access point (AP).

Parameters
TypeDirectionArgument NameDescription
sl_wifi_interface_t[in]interface

Wi-Fi interface as identified by sl_wifi_interface_t

const sl_wifi_advanced_ap_configuration_t *[in]configuration

Wi-Fi AP advanced configuration. See sl_wifi_advanced_ap_configuration_t

Returns

Note

  • This API is not yet implemented.


sl_wifi_get_advanced_ap_configuration#

sl_status_t sl_wifi_get_advanced_ap_configuration (sl_wifi_interface_t interface, const sl_wifi_advanced_ap_configuration_t * configuration)

Get the advanced configuration options of a running Wi-Fi access point interface.

Parameters
TypeDirectionArgument NameDescription
sl_wifi_interface_t[in]interface

Wi-Fi interface as identified by sl_wifi_interface_t

const sl_wifi_advanced_ap_configuration_t *[out]configuration

sl_wifi_advanced_ap_configuration_t object that will contain the AP advanced configuration.

Returns

Note

  • This API is not yet implemented.


sl_wifi_stop_ap#

sl_status_t sl_wifi_stop_ap (sl_wifi_interface_t interface)

Stop Wi-Fi access point.

Parameters
TypeDirectionArgument NameDescription
sl_wifi_interface_t[in]interface

Wi-Fi Access Point interface as identified by sl_wifi_interface_t

Returns

Note

  • All si91x, BSD, and IoT sockets associated with the AP interface must be closed before invoking this API.


sl_wifi_disconnect_ap_client#

sl_status_t sl_wifi_disconnect_ap_client (sl_wifi_interface_t interface, const sl_mac_address_t * mac, sl_wifi_deauth_reason_t reason)

Disconnects a client with the specified MAC address from Access Point (AP).

Parameters
TypeDirectionArgument NameDescription
sl_wifi_interface_t[in]interface

Wi-Fi Access Point interface as identified by sl_wifi_interface_t

const sl_mac_address_t *[in]mac

Wi-Fi client's MAC address of type sl_mac_address_t

sl_wifi_deauth_reason_t[in]reason

Reason for de-authentication as specified in sl_wifi_deauth_reason_t

Use this function to disassociate (disconnect) a client from Access Point. This API is used when the device is in AP mode.

Returns

Note

  • This API is supported only in AP mode.


sl_wifi_get_ap_client_info#

sl_status_t sl_wifi_get_ap_client_info (sl_wifi_interface_t interface, sl_wifi_client_info_response_t * client_info)

Return the Wi-Fi client information of all clients connected to the AP.

Parameters
TypeDirectionArgument NameDescription
sl_wifi_interface_t[in]interface

Wi-Fi Access Point interface as identified by sl_wifi_interface_t

sl_wifi_client_info_response_t *[out]client_info

sl_wifi_client_info_response_t object to store the client info.

Returns

Note

  • This API is supported only in AP mode.


sl_wifi_get_ap_client_list#

sl_status_t sl_wifi_get_ap_client_list (sl_wifi_interface_t interface, uint16_t client_list_count, sl_mac_address_t * client_list)

Return a list of Wi-Fi clients connected to the Wi-Fi access point.

Parameters
TypeDirectionArgument NameDescription
sl_wifi_interface_t[in]interface

Wi-Fi Access Point interface as identified by sl_wifi_interface_t

uint16_t[in]client_list_count

The number of sl_mac_address_t objects the client_list can store.

sl_mac_address_t *[out]client_list

A pointer to an array of client_list_count number of sl_mac_address_t objects where the client list will be copied to.

Returns

Note

  • This API is supported only in AP mode.


sl_wifi_get_ap_client_count#

sl_status_t sl_wifi_get_ap_client_count (sl_wifi_interface_t interface, uint32_t * client_count)

Provide the number of Wi-Fi clients connected to the Wi-Fi access point.

Parameters
TypeDirectionArgument NameDescription
sl_wifi_interface_t[in]interface

Wi-Fi Access Point interface as identified by sl_wifi_interface_t

uint32_t *[out]client_count

A uint32_t pointer that will store the number of associated clients.

Returns

Note

  • This API is supported only in AP mode.