Power and Performance#

Functions#

sl_status_t
sl_wifi_set_performance_profile(const sl_wifi_performance_profile_t *profile) SL_DEPRECATED_API_WISECONNECT_3_5

Set Wi-Fi performance profile.

sl_status_t
sl_wifi_set_performance_profile_v2(const sl_wifi_performance_profile_v2_t *profile)

Set Wi-Fi performance profile.

sl_status_t
sl_wifi_get_performance_profile(sl_wifi_performance_profile_t *profile) SL_DEPRECATED_API_WISECONNECT_3_5

Get Wi-Fi performance profile.

sl_status_t
sl_wifi_get_performance_profile_v2(sl_wifi_performance_profile_v2_t *profile)

Get Wi-Fi performance profile.

Function Documentation#

sl_wifi_set_performance_profile#

sl_status_t sl_wifi_set_performance_profile (const sl_wifi_performance_profile_t * profile)

Set Wi-Fi performance profile.

Parameters
TypeDirectionArgument NameDescription
const sl_wifi_performance_profile_t *[in]profile

Wi-Fi performance profile as indicated by sl_wifi_performance_profile_t

  • Pre-conditions:

Returns

Note


sl_wifi_set_performance_profile_v2#

sl_status_t sl_wifi_set_performance_profile_v2 (const sl_wifi_performance_profile_v2_t * profile)

Set Wi-Fi performance profile.

Parameters
TypeDirectionArgument NameDescription
const sl_wifi_performance_profile_v2_t *[in]profile

Wi-Fi performance profile as indicated by sl_wifi_performance_profile_v2_t

  • Pre-conditions:

Returns

Note

  • For SI91x chips Enhanced MAX PSP is supported when profile is set to ASSOCIATED_POWER_SAVE_LOW_LATENCY and SL_WIFI_ENABLE_ENHANCED_MAX_PSP bit is enabled in config feature bitmap

  • This v2 API is defined due to a new configuration member beacon_miss_ignore_limit added to the structure sl_wifi_performance_profile_v2_t. Default value for beacon_miss_ignore_limit is 1. Recommended max value is 10. Higher value may cause interop issues.

  • For POWER_SAVE_PROFILE with DEEP_SLEEP_WITHOUT_RAM_RETENTION, call sl_net_deinit before calling sl_net_init.

  • For more details about connected and non-connected mode, see https://www.silabs.com/documents/public/application-notes/an1430-siwx917-soc-low-power.pdf.


sl_wifi_get_performance_profile#

sl_status_t sl_wifi_get_performance_profile (sl_wifi_performance_profile_t * profile)

Get Wi-Fi performance profile.

Parameters
TypeDirectionArgument NameDescription
sl_wifi_performance_profile_t *[out]profile

Wi-Fi performance profile as indicated by sl_wifi_performance_profile_t

  • Pre-conditions:

Returns

Note


sl_wifi_get_performance_profile_v2#

sl_status_t sl_wifi_get_performance_profile_v2 (sl_wifi_performance_profile_v2_t * profile)

Get Wi-Fi performance profile.

Parameters
TypeDirectionArgument NameDescription
sl_wifi_performance_profile_v2_t *[out]profile

Wi-Fi performance profile as indicated by sl_wifi_performance_profile_v2_t

  • Pre-conditions:

Returns