Wi-Fi Power and Performance AT Commands#

Overview#

This section describes common AT commands for adjusting Wi-Fi power profiles and performance settings on SiWx91x devices.

Commands#

wifi-perf-prof#

Configures the power and performance profile of the network processor of the SiWx91x device.

Command Format#

at+wifi-perf-prof=<profile>,<dtim-aligned-type>,<num-of-dtim-skip>,<listen-interval>,<monitor-interval>

Related SDK API#

sl_wifi_set_performance_profile_v2

Pre-conditions#

Parameters#

profile#

The power or performance mode to set for the network processor of the SiWx91x device. Contains a numeric value that corresponds to one of the values of the enum sl_wifi_performance_profile_v2_t.

dtim-aligned-type#

Optional. The type of Listen Interval alignment, which can be set either to the number of DTIM beacons or the number of regular beacons. This setting is represented by a numeric value that corresponds to one of the permitted DTIM Alignment Type values.

num-of-dtim-skip#

Optional. The number of DTIM intervals to skip.

listen-interval#

Optional. Listen Interval expressed in the number of beacons of the type set by dtim-aligned-type.

monitor-interval#

Optional. Monitor Interval in milliseconds. Used when profile is set to Associated Power Save with Low Latency.

Notes#

  • Parameters related to Target Wake Time are currently unsupported.

Response#

Examples#

at+wifi-perf-prof=1,0,0,10,0            # Associated Power Save with Listen Interval set to 10 beacon intervals

wifi-perf-prof?#

Queries the power and performance profile of the network processor of the SiWx91x device.

Command Format#

at+wifi-perf-prof?

Related SDK API#

sl_wifi_get_performance_profile_v2

Pre-conditions#

Parameters#

None

Notes#

  • Parameters related to Target Wake Time are currently unsupported.

Response#

  • OK <profile> <dtim-aligned-type> <num-of-dtim-skip> <listen-interval> <monitor-interval> in case of success, where:

    • profile is the power or performance profile currently active on the SiWx91x device, and populated with a numeric value corresponding to one of the values of the enum sl_si91x_performance_profile_v2_t.

    • dtim-aligned-type is the type of beacon that the Listen Interval value is based on, and populated with one of the numeric values of the DTIM Alignment Type.

    • num-of-dtim-skip is the number of DTIM Intervals to skip. This parameter allows the device to skip a specified number of DTIM beacons during power save mode, effectively extending sleep duration and reducing power consumption.

    • listen-interval is the Listen Interval expressed in the number of beacons of type specified by dtim-aligned-type.

    • monitor-interval is the Monitor Interval in milliseconds or 0 or 0 to indicate that is using the default value of 500 milliseconds.

  • ERROR <error code> in case of error. The error codes returned are the same as those returned by the sl_wifi_get_performance_profile_v2 API.

Examples#

at+wifi-perf-prof?
OK 1 0 0 10 1000