Implement the Hardware Abstraction Layer#

This section explains how to define the HAL API functions using host MCU platform-specific drivers.

GPIO Handling#

For the SDK’s HAL to communicate to SiWx917™ NCP through the host MCU platform, certain GPIOs on the host MCU platform should be configured. The following tables explain the GPIOs on SiWx917 NCP that need to be configured by the host MCU.

Note: The BRD8045A Board Pins indicate the EXP Interface (J100) Pin numbers. The BRD8045C Pins indicate the SPI Shield Interface( P101, P102, P103, and P104) Pin numbers. Check the Schematics of BRD8045A and BRD8045C for more details.

Common GPIOs#

Signal name

Pin name on chip as per SiWx917 NCP datasheet

BRD8045A EXP Adapter Board Pin

BRD8045C Shield Adapter Board Pin

I/O direction to host MCU

Description

Reset

RESET_N

J100.11

P101.2

Output

The host MCU must use this GPIO to reset the SiWx917 NCP.

Note: The Reset pin should be configured in Open-drain mode. For more information, refer to SiWx917 NCP datasheet.

Low Power GPIOs#

Signal name

Pin name of chip as per SiWx917 NCP datasheet

BRD8045A EXP Adapter Board Pin

BRD8045C Shield Adapter Board Pin

I/O direction to host MCU

Description

Sleep/Wake indications from SiWx917 NCP

UULP_VBAT_GPIO_0 / SLEEP_IND_FROM_DEV

J100.7

P103.5

Input

The host MCU must use this GPIO to get sleep/wake indications from SiWx917 NCP.

Sleep/Wake requests from host MCU

UULP_VBAT_GPIO_2 / HOST_BYP_ULP_WAKEUP

J100.9

P103.3

Output

The host MCU must use this GPIO to make sleep/wake requests to SiWx917 NCP .

Communication Interface GPIOs#

Currently, the SDK supports SPI and UART interfaces. Let us go through the interface signals connected between the host MCU and the SiWx917 NCP.

SPI Interface#

For SPI interface, the host MCU should be configured as SPI master and SiWx917 should be configured as SPI Slave. For SPI interface, an additional signal – GPIO interrupt signal needs to be configured at the host MCU.

Signal name

Pin name of chip as per SiWx917 NCP datasheet

BRD8045A EXP Adapter Board Pin

BRD8045C Shield Adapter Board Pin

I/O direction to host MCU

Description

SPI Clock

GPIO_25/SPI_CLK

J100.8

P101.6

Output

The host MCU must use this GPIO to source SPI Clock for data synchronization

SPI MISO

GPIO_28/SPI_MISO

J100.6

P101.5

Input

The host MCU must use this GPIO to receive data/command responses from SiWx917 NCP

SPI MOSI

GPIO_27/SPI_MOSI

J100.4

P101.4

Output

The host MCU must use this GPIO to send data/commands to SiWx917 NCP

SPI CS

GPIO_26/SPI_CSN

J100.10

P101.3

Output

The host MCU must use this GPIO to select the SiWx917 chip as its slave whenever it wants to communicate to SiWx917 NCP

GPIO Interrupt

GPIO_29/SPI_INTR

J100.13

P101.1

Input

The host MCU must use this GPIO to get frame pending interrupts from SiWx917 NCP

GPIO Interrupt Handling for SPI Interface#

The SiWx917 NCP shall raise frame pending interrupt to the host MCU indicating that it is about to send a frame. Upon reception of frame, the SDK’s NCP_HOST_BUS_RX_EVENT event should be set, for the SDK to process the incoming frame. This requires a GPIO Interrupt to be configured at the host end. The GPIO Interrupt should contain a logic that would set NCP_HOST_BUS_RX_EVENT event.

For example:

  • For STM32, the GPIO Interrupt Pin selected is PA9. The Interrupt Request (EXTI9_5_IRQn) related to PA9 GPIO is enabled. As per STM32F411RE, the Interrupt Request (EXTI9_5_IRQn) is mapped to EXTI9_5_IRQHandler(). The EXTI9_5_IRQHandler() should contain a logic to set the NCP_HOST_BUS_RX_EVENT event and clear the interrupt as well. This can be done by setting NCP_HOST_BUS_RX_EVENT (BIT(2)) using osEventFlagsSet() function or by calling the utility function sl_si91x_bus_rx_irq_handler() (prototype is present at components/device/silabs/si91x/wireless/inc/sl_rsi_utility.h).

  • For EFR32xG24, the GPIO Interrupt Pin selected is PA7. For the Interrupts that arrive on Odd Pin numbers (here PA7 is an Odd pin number), the interrupt/callback handler that shall be invoked is GPIO_ODD_IRQHandler(). The GPIO_ODD_IRQHandler() should contain a logic to set the NCP_HOST_BUS_RX_EVENT event and clear the interrupt as well.

UART Interface#

For UART interface, no additional GPIO interrupt signal is needed.

Signal name

Pin name of chip as per SiWx917 NCP datasheet

BRD8045A EXP Adapter Board Pin

BRD8045C Shield Adapter Board

Pin I/O direction to host MCU

Description

UART RX

GPIO_8/UART1_RX

J100.14

P103.1

Output

The host MCU must use this GPIO to receive data/command responses from SiWx917 NCP

UART TX

GPIO_9/UART1_TX

J100.12

P103.2

Input

The host MCU must use this GPIO to send data/commands to SiWx917 NCP

UART CTS

GPIO_15/UART1_CTS

J101.35

Not yet routed

Input

The host MCU must use this GPIO to receive CTS signal

UART RTS

GPIO_12/UART1_RTS

BO105

Not yet routed

Output

The host MCU must use this GPIO to send RTS signal

Mapping to the Host#

Choose the host MCU GPIOs and map them to SiWx917 NCP as mentioned above.

For EFR32xG24, the mapping is as follows with a SPI interface:

Signal name

Pin name of chip as per SiWx917 NCP datasheet

EFR32xG24 Pin number

SPI Clock

GPIO_25/SPI_CLK

PC3

SPI MISO

GPIO_28/SPI_MISO

PC2

SPI MOSI

GPIO_27/SPI_MOSI

PC1

SPI CS

GPIO_26/SPI_CSN

PC0

GPIO Interrupt

GPIO_29/SPI_INTR

PA7

Sleep/Wake indications from SiWx917 NCP

UULP_VBAT_GPIO_0 / SLEEP_IND_FROM_DEV

PA5

Sleep/Wake requests from host MCU

UULP_VBAT_GPIO_2 / HOST_BYP_ULP_WAKEUP

PD2

Reset

RESET_N

PA6

For STM32, the mapping is as follows with a SPI interface:

Signal name

Pin name of chip as per SiWx917 NCP datasheet

STM32 Pin number

SPI Clock

GPIO_25/SPI_CLK

PA5

SPI MISO

GPIO_28/SPI_MISO

PA6

SPI MOSI

GPIO_27/SPI_MOSI

PA7

SPI CS

GPIO_26/SPI_CSN

PB6

GPIO Interrupt

GPIO_29/SPI_INTR

PA9

Sleep/Wake indications from SiWx917 NCP

UULP_VBAT_GPIO_0 / SLEEP_IND_FROM_DEV

PB5

Sleep/Wake requests from host MCU

UULP_VBAT_GPIO_2 / HOST_BYP_ULP_WAKEUP

PA10

Reset

RESET_N

PC7

Create HAL Files#

Two HAL files should be created. One is a c header file to keep track of definitions of GPIOs and the other is a c source file to define HAL functions.

  1. It is important to keep track of definitions for GPIO Ports and Pins used for interfacing SiWx917 with host MCU for better readability and maintenance. The GPIO definitions should be provided in a file name sl_board_configuration.h and this file should be included in your application project. For this, create a header file with name sl_board_configuration.h and include it in your project.

    For sl_board_configuration.h in case of EFR32xG24, refer here.

    For sl_board_configuration.h in case of STM32, create a new folder with name stm32f411re within the Sample STM32 Project at components/device/silabs/si91x/wireless/host_mcu and add all the GPIO definitions.

    STM32 Board ConfigurationSTM32 Board Configuration

  2. The C source file should be created to define the HAL API functions. The HAL API functions prototypes are present in the file sl_si91x_host_interface.h located at WSDK/components/device/silabs/si91x/wireless/inc. The function definitions for EFR32xG24 and STM32 shall be explained in the following sections.

    HAL API Function DefinitionsHAL API Function Definitions

  3. The following HAL API functions are explained in the following sections. There are listed here in alphabetical order:

sl_si91x_host_clear_sleep_indicator | sl_si91x_host_deinit | sl_si91x_host_disable_bus_interrupt | sl_si91x_host_enable_bus_interrupt | sl_si91x_host_enable_high_speed_bus | sl_si91x_host_get_wake_indicator | sl_si91x_host_hold_in_reset | sl_si91x_host_init | sl_si91x_host_release_from_reset | sl_si91x_host_set_sleep_indicator | sl_si91x_host_spi_transfer | sl_si91x_host_uart_transfer

Host Initialization Functions#

The following functions are covered in this section. These are mentioned in the sequence in which they occur in the flow of an application:

sl_si91x_host_init | sl_si91x_host_deinit

sl_si91x_host_init#

Prototype#

sl_status_t sl_si91x_host_init(sl_si91x_host_init_configuration *config);

Description#

In this function, the host must configure the interface-related, low power, common GPIOs and Interrupts that are required to communicate with SiWx917 NCP.

Parameters#

The sl_si91x_host_init_configuration structure is defined as below:

typedef sl_status_t (*sl_si91x_host_rx_irq_handler)(void);
typedef void (*sl_si91x_host_rx_done_handler)(void);

typedef struct {
  sl_si91x_host_rx_irq_handler rx_irq;
  sl_si91x_host_rx_done_handler rx_done;
} sl_si91x_host_init_configuration;

The structure can be passed as NULL or can be used as a utility to set SDK’s Bus RX event upon receiving an Incoming frame pending Interrupt from the SiWx917 NCP for SPI Interface. For details, see the GPIO Interrupt Handling for SPI Interface section.

Return values#

  • SL_STATUS_OK - if the host initialization is successful.

  • SL_STATUS_FAIL - if the host initialization fails.

Note: These status codes are from sl_status.h file of SiSDK (formerly GSDK).

Examples#

  • EFR32: Refer here for the definition of function.

  • STM32:

sl_status_t sl_si91x_host_init(sl_si91x_host_init_configuration *config)
{
  UNUSED_PARAMETER(config);
  uint32_t status = 0;

  //! Initialize the host platform GPIOs
  MX_GPIO_Init();

  //! Initialize DMA
  MX_DMA_Init();

  //! Initialize SPI
  MX_SPI1_Init();
  if (init_error != 0) {
    return SL_STATUS_FAIL;
  }

  return SL_STATUS_OK;
}

sl_si91x_host_deinit#

Prototype#

sl_status_t sl_si91x_host_deinit(void);

Description#

In this function, the host must de-initialize the things related to SiWx917 if any, such as memory allocation.

Parameters#

None

Return values#

  • SL_STATUS_OK - if the host deinitialization is successful.

  • SL_STATUS_FAIL - if the host deinitialization fails.

Examples#

  • EFR32: Refer here for the definition of function.

  • STM32:

sl_status_t sl_si91x_host_deinit(void)
{
  return SL_STATUS_OK;
}

Host Interface Functions#

The following functions are covered in this section for various types of interfaces between the application and the SiWx91x network processor for the Serial Peripheral Interface (SPI), and Universal Asynchronous Receiver-Transmitter (UART) interface respectively:

sl_si91x_host_spi_transfer | sl_si91x_host_enable_high_speed_bus | sl_si91x_host_uart_transfer

sl_si91x_host_spi_transfer#

Prototype#

sl_status_t sl_si91x_host_spi_transfer(const void *tx_buffer, void *rx_buffer, uint16_t buffer_length);

Description#

In this function, the host must write an implementation to transfer/receive data to/from the SiWx917 through the SPI interface.

Parameters#

  • tx_buffer - a void pointer that points to the address of data buffer to be transmitted to the SiWx91x NCP

  • rx_buffer - a void pointer that points to the address of data buffer to be received from the SiWx91x NCP

  • buffer_length - Length of data to be transmitted/received

Note: In the SDK, for certain sl_si91x_host_spi_transfer() API calls, the tx_buffer and rx_buffer are passed as NULL.

Return values#

  • SL_STATUS_OK - if successful.

  • SL_STATUS_FAIL - if fails.

Examples#

  • EFR32: Refer here for the definition of function.

  • STM32:

#define SPI_BUFFER_LENGTH 1600
uint8_t spi_buffer[SPI_BUFFER_LENGTH];
sl_status_t sl_si91x_host_spi_transfer(const void *tx_buffer, void *rx_buffer, uint16_t buffer_length)
{
  if (rx_buffer == NULL) {
    rx_buffer = spi_buffer;
  }
  if (tx_buffer == NULL) {
    tx_buffer = spi_buffer;
  }

#ifdef DMA_ENABLED
  HAL_SPI_TransmitReceive_DMA(&hspi1, (uint8_t *)tx_buffer, (uint8_t *)rx_buffer, buffer_length);
  while (!dma_tx_rx_completed) {
  }
  dma_tx_rx_completed = 0;
#else
  HAL_SPI_TransmitReceive(&hspi1, (uint8_t *)tx_buffer, (uint8_t *)rx_buffer, buffer_length, 10);
#endif
  return SL_STATUS_OK;
}

sl_si91x_host_enable_high_speed_bus#

Prototype#

void sl_si91x_host_enable_high_speed_bus();

Description#

In case of using SPI with high clock frequency> 25 MHz, the host must initialize the interface with a clock frequency less than 25 MHz. In this function, a logic should be implemented to switch the host’s SPI Clock frequency to > 25 MHz. This function can be left empty if SPI Clock frequency > 25 MHz is not required.

Parameters#

None

sl_si91x_host_uart_transfer#

Prototype#

sl_status_t sl_si91x_host_uart_transfer(const void *tx_buffer, void *rx_buffer, uint16_t buffer_length);

Description#

In this function, the host must write an implementation to transfer/receive data to/from the SiWx917 through the UART interface.

Parameters#

  • tx_buffer - a void pointer that points to the address of data buffer to be transmitted to the SiWx91x NCP

  • rx_buffer - a void pointer that points to the address of data buffer to be received from the SiWx91x NCP

  • buffer_length - Length of data to be transmitted/received

Return values#

  • SL_STATUS_OK - if successful.

  • SL_STATUS_FAIL - if fails.

Examples#

  • EFR32: Refer here for the definition of function.

  • STM32: To be implemented.

Return values#

None

GPIO Functions#

The following functions are covered in this section for reset, sleep indicator, and wake indicator GPIOs respectively:

sl_si91x_host_hold_in_reset | sl_si91x_host_release_from_reset | sl_si91x_host_set_sleep_indicator | sl_si91x_host_clear_sleep_indicator | sl_si91x_host_get_wake_indicator

sl_si91x_host_hold_in_reset#

Prototype#

void sl_si91x_host_hold_in_reset(void);

Description#

This function should contain the host platform specific GPIO function call to drive the RESET_N GPIO from high to low (resets the SiWx917 NCP).

Parameters#

None.

Return values#

None

Examples#

  • EFR32:

 void sl_si91x_host_hold_in_reset(void)
{
  GPIO_PinModeSet(RESET_PIN.port, RESET_PIN.pin, gpio-ModePushPull, 1);
  GPIO_PinOutClear(RESET_PIN.port, RESET_PIN.pin);
}	
  • STM32:

void sl_si91x_host_hold_in_reset(void)
{
  HAL_GPIO_WritePin(RESET_PIN_GPIO_Port, RESET_PIN_Pin, GPIO_PIN_RESET);
}

sl_si91x_host_release_from_reset#

Prototype#

void sl_si91x_host_release_from_reset(void);

Description#

This function should contain the host platform specific GPIO function call to drive the RESET_N GPIO high (releases SiWx917 from reset).

Parameters#

None

Return values#

None

Examples#

  • EFR32:

void sl_si91x_host_release_from_reset(void)
{
  GPIO_PinModeSet(RESET_PIN.port, RESET_PIN.pin, gpioMode-WiredOrPullDown, 1);
}
  • STM32:

void sl_si91x_host_release_from_reset(void)
{
  HAL_GPIO_WritePin(RESET_PIN_GPIO_Port, RESET_PIN_Pin, GPIO_PIN_SET);
}

sl_si91x_host_set_sleep_indicator#

Prototype#

void sl_si91x_host_set_sleep_indicator(void);

Description#

This function should contain the host platform specific GPIO function call to assert UULP_VBAT_GPIO_2/ HOST_BYP_ULP_WAKEUP GPIO.

Parameters#

None

Return values#

None

Examples#

  • EFR32:

void sl_si91x_host_set_sleep_indicator(void)
{
  GPIO_PinOutSet(SLEEP_CONFIRM_PIN.port, SLEEP_CONFIRM_PIN.pin);
}	
  • STM32:

void sl_si91x_host_set_sleep_indicator(void)
{
  HAL_GPIO_WritePin(SLEEP_CONFIRM_PIN_GPIO_Port, SLEEP_CONFIRM_PIN_Pin, GPIO_PIN_SET);
}

sl_si91x_host_clear_sleep_indicator#

Prototype#

void sl_si91x_host_clear_sleep_indicator(void);

Description#

This function should contain the host platform specific GPIO function call to de-assert UULP_VBAT_GPIO_2/ HOST_BYP_ULP_WAKEUP GPIO.

Parameters#

None

Return values#

None

Examples#

  • EFR32:

void sl_si91x_host_clear_sleep_indicator(void)
{
  GPIO_PinOutClear(SLEEP_CONFIRM_PIN.port, SLEEP_CONFIRM_PIN.pin);
}	
  • STM32:

void sl_si91x_host_clear_sleep_indicator(void)
{
  HAL_GPIO_WritePin(SLEEP_CONFIRM_PIN_GPIO_Port, SLEEP_CONFIRM_PIN_Pin, GPIO_PIN_RESET);
}

sl_si91x_host_get_wake_indicator#

Prototype#

uint32_t sl_si91x_host_get_wake_indicator(void);

Description#

This function should contain the host platform specific GPIO function call to get the value of UULP_VBAT_GPIO_0/ SLEEP_IND_FROM_DEV GPIO.

Parameters#

None

Return values#

  • 0 - Low

  • 1 - High

Examples#

  • EFR32:

uint32_t sl_si91x_host_get_wake_indicator(void)
{
  return GPIO_PinInGet(WAKE_INDICATOR_PIN.port, WAKE_INDICATOR_PIN.pin);
}
  • STM32:

uint32_t sl_si91x_host_get_wake_indicator(void)
{
  return HAL_GPIO_ReadPin(WAKE_INDICATOR_PIN_GPIO_Port, WAKE_INDICATOR_PIN_Pin);
}

GPIO Interrupt Functions#

The following functions are covered in this section. These are mentioned in the sequence in which they occur in the flow of an application:

sl_si91x_host_enable_bus_interrupt | sl_si91x_host_disable_bus_interrupt

sl_si91x_host_enable_bus_interrupt#

Prototype#

void sl_si91x_host_enable_bus_interrupt(void);

Description#

This function should contain the host platform-specific function calls that enables the GPIO-based interrupts (SPI_INTR) from the SiWx91x NCP.

Parameters#

None

Return values#

None

Examples#

  • EFR32:

#define NCP_RX_IRQ GPIO_ODD_IRQn
void sl_si91x_host_enable_bus_interrupt(void)
{
  NVIC_ClearPendingIRQ(NCP_RX_IRQ);
  NVIC_EnableIRQ(NCP_RX_IRQ);
}	
  • STM32:

void sl_si91x_host_enable_bus_interrupt(void)
{
  HAL_NVIC_EnableIRQ(EXTI9_5_IRQn);
}

For STM32 host platform, the appropriate Interrupt Requests (EXTI9_5_IRQn) relevant to the GPIO pin (INTERRUPT_PIN_Pin) has been enabled.

sl_si91x_host_disable_bus_interrupt#

Prototype#

void sl_si91x_host_disable_bus_interrupt(void);

Description#

This function should contain the host platform-specific function calls that disables the GPIO-based interrupts (SPI_INTR) from the SiWx91x NCP.

Parameters#

None

Return values#

None

Examples#

  • EFR32:

#define NCP_RX_IRQ GPIO_ODD_IRQn

void sl_si91x_host_disable_bus_interrupt(void)
{
  NVIC_DisableIRQ(NCP_RX_IRQ);
}
  • STM32:

	void sl_si91x_host_disable_bus_interrupt(void)
{
  HAL_NVIC_EnableIRQ(EXTI9_5_IRQn);
}