Define Preprocessor Macros#
The following macros should be defined for SiWx917™:
SLI_SI917SLI_SI917B0SLI_SI91X_MCU_CONFIG_RADIO_BOARD_VER2SL_WIFI_COMPONENT_INCLUDED- this macro should be defined when your application uses Wi-Fi functionality (i.e., Wi-Fi component from SDK).SL_NET_COMPONENT_INCLUDED- this macro should be defined when your application uses Network management API (i.e., sl_net component from SDK).
The following macros are optional and can be defined based on your application requirements.
SL_SI91X_SPI_HIGH_SPEED_ENABLE– this macro should be defined when the host SPI Clock speed sourced to SiWx917 NCP is greater than 25 MHz.SLI_SI91X_OFFLOAD_NETWORK_STACK– this macro should be defined to use the network or TCP/IP stack from the SiWx917 NCP.SLI_SI91X_SOCKETS– this macro should be defined when using socket functionality.