Boot Configurations Update – eFuse#

This section provides the commands to read and write eFuse data along with the list of the available configurations in eFuse that can be programmed by the user.

Once all the development and testing work is complete, the next step would be to program the eFuses. It is important to note that this is a permanent and one-time operation.

SiWG917 has eFuse memory of 1024 bytes. This memory is divided into four sections with control to enable write locks for each of these sections.

eFuse section

Byte Range

R1

0-127

R2

128-255

R3

256-767

R4

768-1024

Note: You cannot write to eFuse through the M4 application image or through NWP via APIs. You must have an active JTAG connection to write the eFuse bits.

Read eFuse Data#

You can read the eFuse data/contents to an .json (for example, efuse_value.json) file. The command to read eFuse data is as follows.

Syntax:

commander mfg917 read efuse --out efuse_value.json -d <full opn>

Example:

commander mfg917 read efuse –out efuse_value.json -d SiWG917M111MGTBA

Write eFuse Data#

In the case of eFuse (one time programmable) data, simplicity commander CLI first checks whether the requested update is possible (since bits can only be set to 1 and never cleared). Then it will ask for your confirmation.

The possible eFuse configurations are mentioned in the section Possible Boot Configurations.

You can modify the eFuse bits in the efuse_value.json file which is read in the section Read eFuse Data and use the following command which are used to write efuse data into flash.

Syntax:

commander mfg917 write efuse --data efuse_value.json -d <OPN Number> [--skipload] [--pinset n] [-s jlinkserialno] [--noprompt] [--dryrun]

  • --noprompt: It is possible to skip the confirmation, although users need to note that this is a one-time operation.

  • --dryrun: It is possible to check the results of the operation before physically going ahead with the one-time programming.

Example:

commander mfg917 write efuse --data efuse_value.json -d SiWG917M111MGTBA -skipload --dryrun

Possible Boot Configurations#

The following table shows the available user configurable eFuse bits.

Note: The following fields can also be configured in MBR, you can modify them during development in the MBR and program in the eFuse once all the development and testing is completed.

# Field Description Number of bits Default Setting Default value in NWP eFuse
1 safe_upgrade_frm_host When set to 1 – upgrade the:
  • NWP and M4 images from backup, instead of overwriting directly
  • M4 OTA and Public keys from backup, instead of overwriting directly
When set to 0, the images or the keys will be directly overwritten to the target locations based on the target address, which comes from the RPS header.
1 Enabled 1
2 ta_secure_boot_enable Enable NWP Secure Boot
1: Secure boot is enabled for NWP
0: Secure boot is disabled in NWP
1 Disabled 0
3 ta_anti_roll_back 1: Anti roll back check is enabled for NWP firmware (will not allow to update old versions)
0: Anti roll back check is not enabled for NWP firmware
1 IC: Disabled
Module: Enabled
IC: 0
Module: 1
4 ta_digital_signature_validation 1: Digital signature validation is enabled for NWP firmware
0: Digital signature validation is disabled for NWP firmware
1 Digital signature validation is disabled for NWP firmware 0
5 m4_anti_roll_back 1: Anti roll back check is enabled for M4 firmware (will not allow to update old versions)
0: Anti roll back check is not enabled for M4 firmware
1 Disabled 0
6 m4_digital_signature_validation 1: Digital signature validation is enabled for M4 firmware
0: Digital signature validation is disabled for M4 firmware
1 Disabled 0
7 enable_autobaud_detection 1: Auto baud rate detection for UART is enabled
0: Auto baud disabled – Default config – 115200 bps
1 Disabled 0
8 ta_encrypt_firmware 00: NWP firmware stored in unencrypted form in flash
01: NWP firmware stored in encrypted form in flash with CTR mode encryption
10: NWP firmware stored in encrypted form in flash with XTS mode encryption
11: Reserved
2 Disabled: NWP firmware stored in unencrypted form in flash 0
9 m4_flash_present This field indicates that the M4 has a separate flash. This field is not applicable to the current configuration.
1: M4 has flash
0: M4 doesn't have flash
1 Disabled: M4 doesn't have flash – it's a common flash device 0
10 m4_flash_pinset M4 flash pin set. This field is not applicable to the current configuration.
1: GPIO_46_TO_51
2: GPIO_52_TO_57
4 Not applicable as the m4_flash_present bit is not set by default; device will not use the values from this field 0
11 m4_secure_boot_enable 1: Secure boot is enabled for M4
0: Secure boot is not enabled for M4
1 Secure boot is not enabled for M4 0
12 m4_encrypt_firmware 0: M4 firmware stored in unencrypted form in flash
1: M4 firmware stored in encrypted form in flash
1 M4 firmware is stored in unencrypted form in the flash 0
13 common_flash_enabled Enable common flash configuration. Note: If enabled from eFuse, cannot be overridden from MBR.
1: Common flash mode is enabled
0: Common flash mode not selected

The value written for this bit during manufacturing changes between device types:

  • If the OPN is no in-package OPN, the eFuse configs written in eFuse will have this value set to 0 so that the customer can update it when a flash is connected.
  • If the OPN is with flash, the eFuse configs are written as part of MBR configs in flash. In that case the value is set as 1.
1 If writing in eFuse, the value is set to 0. If writing to MBR, the value is set to 1. 0
14 ta_otp_lock NWP eFuse programming lock for R1 address region (0–127)
1: NWP eFuse programming is locked
0: NWP eFuse programming is not locked
When eFuse is locked, you won’t be able to modify secure boot related parameters present in R1 address region.
1 NWP eFuse programming is not locked for 0–127 range 0
15 disable_ta_jtag Disable NWP JTAG interface. Write 0 for enabling NWP JTAG.
0: Enable NWP JTAG interface
1: Disable NWP JTAG interface
1 NWP JTAG interface enabled 0
16 otp_lock_1 NWP eFuse programming lock for address region (128–255) of eFuse. This is enabled by programming the eFuse offset 255 with value 1.
1: NWP eFuse programming is locked
0: NWP eFuse programming is not locked
When eFuse is locked, you won’t be able to modify secure boot related parameters present in R2 address region.
1 NWP eFuse programming is not locked in range 128–255 0
17 otp_lock_2 NWP eFuse programming lock for address region (256–767). This is enabled by programming the eFuse offset 766 with value 1.
1: NWP eFuse programming is locked
0: NWP eFuse programming is not locked
When eFuse is locked, you won’t be able to modify secure boot related parameters present in R3 address region.
1 NWP eFuse programming is not locked in range 256–767 0
18 otp_lock_3 NWP eFuse programming lock for R4 address region (768–1024). This is enabled by programming the eFuse offset 1023 with value 1.
1: NWP eFuse programming is locked
0: NWP eFuse programming is not locked
When eFuse is locked, you won’t be able to modify secure boot related parameters present in R4 address region.
1 NWP eFuse programming is not locked in range 768–1024 0
19 m4_otp_programming_lock 1: M4 eFuse programming is locked
0: M4 eFuse programming is not locked
When eFuse is locked, you won’t be able to modify secure boot related parameters.
1 M4 eFuse programming is not locked 0
20 disable_m4_jtag Disable M4 JTAG interface.
0: Enable M4 JTAG interface (default)
1: Disable M4 JTAG interface
1 JTAG enabled 0
21 disable_m4_access_frm_tass_sec When set, M4 can't access NWP memory or registers except for host communication registers.
Note: Setting this eFuse must be the last step in manufacturing. Once set, any further operations with manufacturing tools will not be possible.
1 This is secure zone which is disabled by default 0
22 mbr_mic_sign_enable MIC/signature for combined region of MBR, boot descriptor, and key descriptor table.
00: CRC
01: MIC – Applicable only when OTP Symmetric key is written
10: Reserved
11: Sign – Applicable only when OTP public key is written
2 CRC check enabled 00
23 MIC protected content length This field depicts how much space is MIC protected using the OTP key stored in eFuse at offset 659. The MIC value is stored in eFuse at offset 643. 4 Not applicable 0000
24 m4_firmware_encryption_mode Indicates M4 firmware encryption mode. Valid only if m4_encrypt_firmware is set to 1; otherwise ignored.
00: NA
01: Firmware stored in encrypted form in M4 flash – CTR mode
10: Firmware stored in encrypted form in M4 flash – XTS mode
11: Reserved
2 Not applicable as m4_encrypt_firmware is disabled by default. This field will be neglected. 00
25 disable_psram_encryption Contents in PSRAM will be encrypted if this bit is enabled. This field explicitly disables PSRAM encryption irrespective of whether M4 firmware encryption is enabled while firmware is in flash.
0: PSRAM encryption using same key config as M4 flash. PSRAM encryption mode will be CTR independent of M4 flash encryption mode.
1: PSRAM encryption disabled.
1 PSRAM encryption enabled 0