Getting Started with the WiSeConnect™ SDK#

To get started with using the WiSeConnect™ SDK, download Simplicity Studio 6.2.0 and select one of the getting started guides in this section:

  • System-on-chip (SoC) mode - both the application and connectivity stack run on the SiWx91x™ chipset.

  • Network co-processor (NCP) mode - application runs on external microcontroller unit (MCU) host, connectivity stack runs on the SiWx91x chipset.

    Note: The following alternative interfaces are supported between the SiWx91x chipset and the EFR32 host:

    • Serial Peripheral Interface (SPI)

    • Universal Asynchronous Receiver-Transmitter (UART) interface

  • Radio co-processor (RCP) mode - application and upper Wi-Fi network layers (transport and network) run on external Linux host, lower Wi-Fi network layers (MAC and PHY) run on the SiWx91x chipset. A Linux driver is available for connecting a Linux host to Wi-Fi in this mode using the SiWx91x connectivity stack.

    Note: The WiSeConnect SDK does not support the RCP mode.

  • Matter Quick-Start Guides provide steps to set up your first example application using the Matter protocol: