Functions#

This section provides a reference to the MQTT API functions.

Note

  • Stack overflows may occur if you invoke functions or use your own variables or data structures while handling callbacks. Please configure the stack size by modifying the pre-processor macro SL_SI91X_EVENT_HANDLER_STACK_SIZE as per your application's requirements. See here for the instructions for modifying a pre-processor macro.

  • Event/Callback handlers must not contain function calls or code which can block or delay the execution of the event/callback handler. Doing so will cause all the other events to queue up and delay the execution of other events because all the events are invoked and handled from a single thread.

  • Do not call any synchronous SDK APIs from within the Event/Callback handlers.

Functions#

sl_status_t
sl_mqtt_client_init(sl_mqtt_client_t *client, sl_mqtt_client_event_handler_t event_handler)

Initialize the MQTT client and register the event handler.

sl_status_t
sl_mqtt_client_deinit(sl_mqtt_client_t *client)

Deinitialize the MQTT client.

sl_status_t
sl_mqtt_client_connect(sl_mqtt_client_t *client, const sl_mqtt_broker_t *broker, const sl_mqtt_client_last_will_message_t *last_will_message, const sl_mqtt_client_configuration_t *configuration, uint32_t timeout) SL_DEPRECATED_API_WISECONNECT_4_0

Connect the client to an MQTT broker.

sl_status_t
sl_mqtt_client_connect_v2(sl_mqtt_client_t *client, const sl_mqtt_broker_v2_t *broker, const sl_mqtt_client_last_will_message_t *last_will_message, const sl_mqtt_client_configuration_t *configuration, uint32_t connect_timeout)

Connect the client to an MQTT broker using the extended v2 configuration.

sl_status_t
sl_mqtt_client_disconnect(sl_mqtt_client_t *client, uint32_t timeout)

Disconnect the client from the MQTT broker.

sl_status_t
sl_mqtt_client_publish(sl_mqtt_client_t *client, const sl_mqtt_client_message_t *message, uint32_t timeout, void *context)

Publishes the message to the MQTT broker.

sl_status_t
sl_mqtt_client_subscribe(sl_mqtt_client_t *client, const uint8_t *topic, uint16_t topic_length, sl_mqtt_qos_t qos_level, uint32_t timeout, sl_mqtt_client_message_received_t message_handler, void *context)

Subscribe a client to a specific topic on the MQTT broker.

sl_status_t
sl_mqtt_client_unsubscribe(sl_mqtt_client_t *client, const uint8_t *topic, uint16_t topic_length, uint32_t timeout, void *context)

Unsubscribe a client from a specific topic on the MQTT broker.

sl_status_t
sl_mqtt_client_set_tcp_tls_advanced_configuration(sl_mqtt_client_t *client, const sl_mqtt_client_tcp_tls_advanced_options_t *options)

Configures advanced TCP/TLS options for an MQTT client.

Function Documentation#

sl_mqtt_client_init#

sl_status_t sl_mqtt_client_init (sl_mqtt_client_t * client, sl_mqtt_client_event_handler_t event_handler)

Initialize the MQTT client and register the event handler.

Parameters
TypeDirectionArgument NameDescription
sl_mqtt_client_t *[in]client

Pointer to the MQTT client structure of type sl_mqtt_client_t. This pointer must not be NULL.

sl_mqtt_client_event_handler_t[in]event_handler

Event handler of type sl_mqtt_client_event_handler_t that would be called for various events on the client. This pointer must not be NULL.

This function initializes the MQTT client by setting up the event handler, and initializing the subscription list. It also assigns the provided client structure to the global MQTT client pointer.

Returns


sl_mqtt_client_deinit#

sl_status_t sl_mqtt_client_deinit (sl_mqtt_client_t * client)

Deinitialize the MQTT client.

Parameters
TypeDirectionArgument NameDescription
sl_mqtt_client_t *[in]client

Pointer to the MQTT client structure of type sl_mqtt_client_t. This pointer must not be NULL.

This function deinitializes the MQTT client by clearing its state and resetting the global MQTT client pointer. It ensures that the client is in a disconnected state before deinitializing.

  • The MQTT client must be in the disconnected state before calling this function.

Returns


sl_mqtt_client_connect#

sl_status_t sl_mqtt_client_connect (sl_mqtt_client_t * client, const sl_mqtt_broker_t * broker, const sl_mqtt_client_last_will_message_t * last_will_message, const sl_mqtt_client_configuration_t * configuration, uint32_t timeout)

Connect the client to an MQTT broker.

Parameters
TypeDirectionArgument NameDescription
sl_mqtt_client_t *[in]client

Pointer to the MQTT client structure of type sl_mqtt_client_t that would be connected to the broker.

const sl_mqtt_broker_t *[in]broker

Pointer to the broker configuration of type sl_mqtt_broker_t. This parameter could be NULL for subsequent calls to retain the previous broker configuration.

const sl_mqtt_client_last_will_message_t *[in]last_will_message

Pointer to the last will message of the client of type sl_mqtt_client_last_will_message_t. This parameter could be NULL for subsequent calls if no will message is to be sent.

const sl_mqtt_client_configuration_t *[in]configuration

Pointer to the client configuration of type sl_mqtt_client_configuration_t. This parameter could be NULL for subsequent calls to retain the previous configuration.

uint32_t[in]timeout

Timeout for the API is in milliseconds. If the value is zero, the API operates in asynchronous mode.

This function connects the MQTT client to the specified broker using the provided configuration and last will message. It supports both synchronous, and asynchronous operations based on the timeout value.

Returns

Note

  • In subsequent calls to connect, it is optional to provide broker, last_will_message, and configuration parameters. If broker and configuration parameters are assigned as NULL, the values are retains from the first connect() call. For the last_will_message parameter, values assigned in each connect() call are considered. If the last_will_message parameter value is NULL, no will message are sent to the broker. is_clean_session, credential_id, client_id, and client_id_length of sl_mqtt_client_configuration_t are consider. The topic length of the last_will_message must be less than SI91X_MQTT_CLIENT_WILL_TOPIC_MAXIMUM_LENGTH. The client ID length should be less than SI91X_MQTT_CLIENT_CLIENT_ID_MAXIMUM_LENGTH. The username and password length must be less than SI91X_MQTT_CLIENT_USERNAME_MAXIMUM_LENGTH and SI91X_MQTT_CLIENT_PASSWORD_MAXIMUM_LENGTH, respectively. MQTT 3.1.1 version is supported.

  • This function uses a user-configurable timeout parameter that is not affected by the global timeout scaling factors (SL_WIFI_INTERNAL_COMMANDS_TIMEOUT_SF, SL_WIFI_MANAGEMENT_COMMANDS_TIMEOUT_SF, SL_WIFI_NETWORK_COMMANDS_TIMEOUT_SF) or the additional wait time configuration (SL_TX_ADDITIONAL_WAIT_TIME).

  • Moving forward, this API will be deprecated. Instead, use the sl-mqtt-client-connect-v2 API. This is retained for backward compatibility.


sl_mqtt_client_connect_v2#

sl_status_t sl_mqtt_client_connect_v2 (sl_mqtt_client_t * client, const sl_mqtt_broker_v2_t * broker, const sl_mqtt_client_last_will_message_t * last_will_message, const sl_mqtt_client_configuration_t * configuration, uint32_t connect_timeout)

Connect the client to an MQTT broker using the extended v2 configuration.

Parameters
TypeDirectionArgument NameDescription
sl_mqtt_client_t *[in]client

Pointer to the MQTT client structure of type sl_mqtt_client_t that would be connected to the broker.

const sl_mqtt_broker_v2_t *[in]broker

Pointer to the broker configuration of type sl_mqtt_broker_v2_t. You can set this parameter to NULL in later calls to reuse the previous broker configuration.

const sl_mqtt_client_last_will_message_t *[in]last_will_message

Pointer to the last will message of the client of type sl_mqtt_client_last_will_message_t. You can set this parameter to NULL in later calls if no will message is to be sent.

const sl_mqtt_client_configuration_t *[in]configuration

Pointer to the client configuration of type sl_mqtt_client_configuration_t. You can set this parameter to NULL in later calls to reuse the previous broker configuration.

uint32_t[in]connect_timeout

Timeout for the API is in milliseconds. If the value is zero, the API operates in asynchronous mode.

This function connects the MQTT client to the specified broker using the provided v2 configuration and last will message. It supports both synchronous and asynchronous operations based on the connect_timeout value. The v2 configuration allows enabling Server Name Indication (SNI) via the 'enable_sni' field and passing additional parameters for advanced TLS features.

Returns

Note

  • In subsequent calls to connect, it is optional to provide broker, last_will, and configuration parameters. If broker and configuration parameters are assigned as NULL, the values are retained from the first connect_v2() call. For the last_will parameter, values assigned in each connect_v2() call are considered. If the last_will parameter value is NULL, no will message is sent to the broker. The v2 configuration allows enabling SNI via the 'enable_sni' field and passing a hostname or SNI extension for advanced TLS features. The topic length of the last_will message must be less than SI91X_MQTT_CLIENT_WILL_TOPIC_MAXIMUM_LENGTH. The client ID length should be less than SI91X_MQTT_CLIENT_CLIENT_ID_MAXIMUM_LENGTH. The username and password length must be less than SI91X_MQTT_CLIENT_USERNAME_MAXIMUM_LENGTH and SI91X_MQTT_CLIENT_PASSWORD_MAXIMUM_LENGTH, respectively. MQTT 3.1.1 version is supported.

  • This function uses a user-configurable timeout parameter that is not affected by the global timeout scaling factors (SL_WIFI_INTERNAL_COMMANDS_TIMEOUT_SF, SL_WIFI_MANAGEMENT_COMMANDS_TIMEOUT_SF, SL_WIFI_NETWORK_COMMANDS_TIMEOUT_SF) or the additional wait time configuration (SL_TX_ADDITIONAL_WAIT_TIME).

  • SNI Limitation:

    • Only one SNI command can be active at a time, irrespective of protocol (MQTT or HTTP).

    • You must wait for the connection to be fully established before initiating another connection with SNI.

    • If multiple SNI commands are sent simultaneously, SL_STATUS_SI91X_FEATURE_NOT_AVAILABLE will be returned.

    • For reconnection scenarios, set SNI before calling reconnect.


sl_mqtt_client_disconnect#

sl_status_t sl_mqtt_client_disconnect (sl_mqtt_client_t * client, uint32_t timeout)

Disconnect the client from the MQTT broker.

Parameters
TypeDirectionArgument NameDescription
sl_mqtt_client_t *[in]client

Pointer to the MQTT client structure of type sl_mqtt_client_t disconnects from the broker. The pointer value must not be NULL.

uint32_t[in]timeout

Timeout for the API in milliseconds. If the value is zero, the API is asynchronous.

This function disconnects the MQTT client from the broker and deinitializes the client context. It supports synchronous, and asynchronous operations based on the timeout value. The function ensures that the client is in a valid state before attempting to disconnect.

  • Synchronous Mode: If the timeout value is non-zero then, the function waits for the disconnect operation to complete within the specified timeout period.

  • Asynchronous Mode: If the timeout value is zero then, the function returns immediately, and the results are provided via the sl_mqtt_client_event_handler_t callback.

Returns

  • sl_status_t - Status of the operation. For more details, see https://docs.silabs.com/gecko-platform/latest/platform-common/status.

    • SL_STATUS_OK: Operation successful.

    • SL_STATUS_IN_PROGRESS: Operation is in progress (for asynchronous calls).

    • SL_STATUS_INVALID_PARAMETER: One or more parameters are invalid.

    • SL_STATUS_INVALID_STATE: The client is not in a valid state to disconnect.

    • SL_STATUS_FAIL: Operation failed.

Note

  • The function deinitializes the MQTT client context after the disconnection. The client must be in one of the following states to call this function: SL_MQTT_CLIENT_CONNECTED, SL_MQTT_CLIENT_TA_DISCONNECTED, or SL_MQTT_CLIENT_CONNECTION_FAILED.

  • This function uses a user-configurable timeout parameter that is not affected by the global timeout scaling factors (SL_WIFI_INTERNAL_COMMANDS_TIMEOUT_SF, SL_WIFI_MANAGEMENT_COMMANDS_TIMEOUT_SF, SL_WIFI_NETWORK_COMMANDS_TIMEOUT_SF) or the additional wait time configuration (SL_TX_ADDITIONAL_WAIT_TIME).


sl_mqtt_client_publish#

sl_status_t sl_mqtt_client_publish (sl_mqtt_client_t * client, const sl_mqtt_client_message_t * message, uint32_t timeout, void * context)

Publishes the message to the MQTT broker.

Parameters
TypeDirectionArgument NameDescription
sl_mqtt_client_t *[in]client


Pointer to the MQTT client structure of type sl_mqtt_client_t publishes the message. This pointer value must not be NULL, and the client must be in a connected state.

const sl_mqtt_client_message_t *[in]message


Pointer publishes the message structure of sl_mqtt_client_message_t type.The pointer must not be NULL, and the topic lenth value must be less than SI91X_MQTT_CLIENT_TOPIC_MAXIMUM_LENGTH.

uint32_t[in]timeout


Timeout for the API is in milliseconds. If the value is zero, the API is asynchronous.

void *[in]context


Pointer to the context returns the event handler if the API is called asynchronously. The caller ensures that the lifecycle of the context is retained until the callback is invoked. The deallocation of the context is the responsibility of the caller.

This function publishes a message to the specified topic of the MQTT broker. It supports both synchronous, and asynchronous operations based on the timeout value. The function ensures that the client is in the connected state before attempting to publish the message.

Returns


  • sl_status_t - Status of the operation. For more details, see https://docs.silabs.com/gecko-platform/latest/platform-common/status.

    • SL_STATUS_OK: Operation successful.

    • SL_STATUS_IN_PROGRESS: Operation is in progress (for asynchronous calls).

    • SL_STATUS_INVALID_PARAMETER: One or more parameters are invalid.

    • SL_STATUS_INVALID_STATE: The client is not in a valid state to publish.

    • SL_STATUS_ALLOCATION_FAILED: Memory allocation failed.

    • SL_STATUS_FAIL: Operation failed.

Note

  • The maximum length of the topic must be less than SI91X_MQTT_CLIENT_TOPIC_MAXIMUM_LENGTH. The function allocates memory for the publish request, and free the space after the operation.

  • This function uses a user-configurable timeout parameter that is not affected by the global timeout scaling factors (SL_WIFI_INTERNAL_COMMANDS_TIMEOUT_SF, SL_WIFI_MANAGEMENT_COMMANDS_TIMEOUT_SF, SL_WIFI_NETWORK_COMMANDS_TIMEOUT_SF) or the additional wait time configuration (SL_TX_ADDITIONAL_WAIT_TIME).


sl_mqtt_client_subscribe#

sl_status_t sl_mqtt_client_subscribe (sl_mqtt_client_t * client, const uint8_t * topic, uint16_t topic_length, sl_mqtt_qos_t qos_level, uint32_t timeout, sl_mqtt_client_message_received_t message_handler, void * context)

Subscribe a client to a specific topic on the MQTT broker.

Parameters
TypeDirectionArgument NameDescription
sl_mqtt_client_t *[in]client


Pointer to the MQTT client structure of type sl_mqtt_client_t that needs to subscribe to the topic. This pointer must not be NULL and the client must be in a connected state.

const uint8_t *[in]topic

Pointer to the topic string that the client wants to subscribe to. This pointer must not be NULL.

uint16_t[in]topic_length


Length of the topic string. The maximum length must be less than SI91X_MQTT_CLIENT_TOPIC_MAXIMUM_LENGTH.

sl_mqtt_qos_t[in]qos_level


Quality of Service level of type sl_mqtt_qos_t is subscribed by the client to use the topic.

uint32_t[in]timeout


Timeout for the API is in milliseconds. If the value is zero, the API operates in asynchronous mode.

sl_mqtt_client_message_received_t[in]message_handler


Pointer to the message handler function of type sl_mqtt_client_message_received_t that will be invoked for messages published on the subscribed topic. This pointer must not be NULL.

void *[in]context

Pointer to the context that will be sent back to the message handler. The caller must ensure that the lifecycle of the context is retained until the callback is invoked. The deallocation of the context is also the responsibility of the caller.

This function subscribes the specified client to a given topic on the MQTT broker. It supports both synchronous, and asynchronous operations based on the timeout value. The function ensures that the client is in a connected state before attempting to subscribe to the topic.

Returns


  • sl_status_t - Status of the operation. For more details, see https://docs.silabs.com/gecko-platform/latest/platform-common/status.

    • SL_STATUS_OK: Operation successful.

    • SL_STATUS_IN_PROGRESS: Operation is in progress (for asynchronous calls).

    • SL_STATUS_INVALID_PARAMETER: One or more parameters are invalid.

    • SL_STATUS_INVALID_STATE: The client is not in a valid state to subscribe.

    • SL_STATUS_ALLOCATION_FAILED: Memory allocation failed.

    • SL_STATUS_FAIL: Operation failed.

Note

  • The maximum length of the topic should be less than SI91X_MQTT_CLIENT_TOPIC_MAXIMUM_LENGTH.

  • This function uses a user-configurable timeout parameter that is not affected by the global timeout scaling factors (SL_WIFI_INTERNAL_COMMANDS_TIMEOUT_SF, SL_WIFI_MANAGEMENT_COMMANDS_TIMEOUT_SF, SL_WIFI_NETWORK_COMMANDS_TIMEOUT_SF) or the additional wait time configuration (SL_TX_ADDITIONAL_WAIT_TIME).


sl_mqtt_client_unsubscribe#

sl_status_t sl_mqtt_client_unsubscribe (sl_mqtt_client_t * client, const uint8_t * topic, uint16_t topic_length, uint32_t timeout, void * context)

Unsubscribe a client from a specific topic on the MQTT broker.

Parameters
TypeDirectionArgument NameDescription
sl_mqtt_client_t *[in]client


Pointer to the MQTT client structure of type sl_mqtt_client_t that needs to unsubscribe from the topic. This pointer must not be NULL and the client must be in a connected state.

const uint8_t *[in]topic

Pointer to the topic string that the client wants to unsubscribe from. This pointer must not be NULL.

uint16_t[in]topic_length


Length of the topic string. The maximum length should be less than SI91X_MQTT_CLIENT_TOPIC_MAXIMUM_LENGTH.

uint32_t[in]timeout


Timeout for the API in milliseconds. If the value is zero, the API is asynchronous.

void *[in]context

Pointer to the context that will be sent back to the event handler if the API is called asynchronously. The caller must ensure that the lifecycle of the context is retained until the callback is invoked. The deallocation of the context is also the responsibility of the caller.

This function unsubscribes the specified client from a given topic on the MQTT broker. It supports both synchronous, and asynchronous operations based on the timeout value. The function ensures that the client is in a connected state before attempting to unsubscribe from the topic.

Returns


  • sl_status_t - Status of the operation. For more details, see https://docs.silabs.com/gecko-platform/latest/platform-common/status.

    • SL_STATUS_OK: Operation successful.

    • SL_STATUS_IN_PROGRESS: Operation is in progress (for asynchronous calls).

    • SL_STATUS_INVALID_PARAMETER: One or more parameters are invalid.

    • SL_STATUS_INVALID_STATE: The client is not in a valid state to unsubscribe.

    • SL_STATUS_ALLOCATION_FAILED: Memory allocation failed.

    • SL_STATUS_FAIL: Operation failed.

Note

  • The maximum length of the topic must be less than SI91X_MQTT_CLIENT_TOPIC_MAXIMUM_LENGTH.

  • This function uses a user-configurable timeout parameter that is not affected by the global timeout scaling factors (SL_WIFI_INTERNAL_COMMANDS_TIMEOUT_SF, SL_WIFI_MANAGEMENT_COMMANDS_TIMEOUT_SF, SL_WIFI_NETWORK_COMMANDS_TIMEOUT_SF) or the additional wait time configuration (SL_TX_ADDITIONAL_WAIT_TIME).


sl_mqtt_client_set_tcp_tls_advanced_configuration#

sl_status_t sl_mqtt_client_set_tcp_tls_advanced_configuration (sl_mqtt_client_t * client, const sl_mqtt_client_tcp_tls_advanced_options_t * options)

Configures advanced TCP/TLS options for an MQTT client.

Parameters
TypeDirectionArgument NameDescription
sl_mqtt_client_t *[in]client

Pointer to the MQTT client structure of type sl_mqtt_client_t. Must not be NULL.

const sl_mqtt_client_tcp_tls_advanced_options_t *[in]options

Pointer to an sl_mqtt_client_tcp_tls_advanced_options_t structure containing the TCP/TLS options. Must not be NULL.

This function stores the provided advanced TCP and TLS configuration options in the MQTT client handle. The options are applied automatically when the client connects to the broker via sl_mqtt_client_connect or sl_mqtt_client_connect_v2. Call this function after sl_mqtt_client_init and before connecting.

Returns