Edit

WiSeConnect - Multiprotocol Version 4.1.2 (Oct 14, 2026) - Release Notes#

Wi-Fi 6 + BLE (WiSeConnect) SDK Version 4.1.2

Simplicity SDK Version 2026.6.2

The Multiprotocol Software Development Kit (SDK) provides Wi-Fi and BLE coexistence and packet traffic arbitration (PTA) features.

See WiSeConnect releases for earlier releases.

Release Summary#

Key Features | API Changes | Bug Fixes | Chip Enablement

Key Features#

Added in 4.1.2#

  • Added PSRAM project configurations for Wi-Fi and BLE coexistence examples.

Added in 4.1.1#

None

Added in 4.1.0#

  • Added support for dynamically enabling or disabling BLE, BLE memory can now be reused for Network Stack memory and packet buffers once BLE is disabled.

  • Support for concurrent operation of eight BLE peripheral connections, two BLE central devices, and WLAN MQTT data transfer in NCP mode.

  • Support for concurrent two BLE connections with advertising extensions and WLAN TCP TX data transfer in NCP.

  • Optimized NWP RAM utilization by disabling the low-power mode bit (BIT(19)) in the opermode configuration.

API Changes#

Added in 4.1.2#

None

Added in 4.1.1#

None

Added in 4.1.0#

None

Bug Fixes#

Fixed in 4.1.2#

  • Fixed an assertion failure during BLE re-enable while running Wi-Fi and BLE disable enable Loop with BLE powersave enabled.

  • Fixed an issue where Wi-Fi scanning failed after a BLE connection was established and subsequently disconnected in wifi_station_ble_provisioning_aws_devkit.

  • Fixed an issue where the WLAN multi-socket application could become unresponsive during BLE data transfer with a connected remote device.

  • Provided an application level API to disconnect all BLE connections before calling sl_net_deinit to avoid the 0x1C issue.

  • Fixed an intermittent unresponsive condition observed during repeated BLE enable/disable cycles in the BLE Wi-Fi provisioning scenario.

Fixed in 4.1.1#

  • Fixed the "Unsupported LMP Parameter" issue in Matter commissioning with the Amazon ecosystem.

  • Fixed an issue where the application stopped responding intermittently during BLE enable/disable cycles in the BLE Wi-Fi provisioning scenario when set_adv_param failed after BLE was successfully enabled.

  • Fixed an issue where sl_wifi_deinit() did not respond after repeated Wi-Fi + BLE coexistence initialization and deinitialization cycles.

  • Fixed a power management issue where, after upgrading from WiseConnect 4.0.3 to 4.1.0, the NWP did not go to sleep properly.

Fixed in 4.1.0#

  • Fixed an issue where LTK storage failures and security key list errors were reported during repeated BLE connect/disconnect cycles from remote devices while Wi‑Fi scan, connect, and disconnect operations were running concurrently.

  • Disabled the unsupported AE feature in the wlan_ble_unified_coex_app_soc application.

Chip Enablement#

Added in 4.1.2#

  • Added support for 16 MB flash.

Added in 4.1.1#

None

Added in 4.1.0#

None

Key Features#

New Features | Enhancements | Removed Features | Deprecated Features

Note: See Feature Matrix for a list of any applicable APIs, examples, software variants, modes, hardware, and host interfaces applicable for each feature.

New Features#

Added in 4.1.2#

None

Added in 4.1.1#

None

Added in 4.1.0#

  • BLE memory can now be reused for Network Stack memory and packet buffers once BLE is disabled.

  • Support for concurrent operation of eight BLE peripheral connections, two BLE central devices, and WLAN MQTT data transfer in NCP mode.

  • Support for concurrent two BLE connections with advertising extensions and WLAN TCP TX data transfer in NCP.

  • Optimized NWP RAM utilization by disabling the low-power mode bit (BIT(19)) in the opermode configuration.

Enhancements#

Added in 4.1.2#

  • Added PSRAM project configurations for Wi-Fi and BLE coexistence examples.

Added in 4.1.1#

None

Added in 4.1.0#

  • Added support for the SL_DEBUG_LOG_V2 logging backend in coex snippets across Wi-Fi and BLE paths.

Removed Features#

Removed in 4.1.2#

None

Removed in 4.1.1#

None

Removed in 4.1.0#

None

Deprecated Features#

Deprecated in 4.1.2#

None

Deprecated in 4.1.1#

None

Deprecated in 4.1.0#

None

API Changes#

New APIs | Modified APIs | Removed APIs | Deprecated APIs

New APIs#

Added in 4.1.2#

None

Added in 4.1.1#

None

Added in 4.1.0#

None

Modified APIs#

Modified in 4.1.2#

None

Modified in 4.1.1#

None

Modified in 4.1.0#

None

Removed APIs#

Removed in 4.1.2#

None

Removed in 4.1.1#

None

Removed in 4.1.0#

None

Deprecated APIs#

Deprecated in 4.1.2#

None

Deprecated in 4.1.1#

None

Deprecated in 4.1.0#

None

Bug Fixes#

Note: See the Feature Matrix section for a list of all hardware parts that work with the WiSeConnect SDK.

Fixed in 4.1.2#

ID Issue Description GitHub / Salesforce Reference (if any) Workaround (if any) Affected Software Variants, OPNs, Boards, Modes, Host Interfaces
1667465 Fixed an assert during BLE re-enable while running Wifi and BLE disable enable Loop with BLE powersave. None None
  • Software variants: Standard and Lite
  • OPNs: All
  • Boards: All
  • Modes: SoC
  • Host interfaces: N/A
1756195 Fixed an issue where Wi-Fi scanning failed after a BLE connection was established and subsequently disconnected in wifi_station_ble_provisioning_aws_devkit. None None
  • Software variants: Standard and Lite
  • OPNs: All
  • Boards: All
  • Modes: SoC
  • Host interfaces: N/A
1671050 Fixed an issue where the WLAN multi-socket application could become unresponsive during BLE data transfer with a connected remote device. None None
  • Software variants: Standard and Lite
  • OPNs: All applicable
  • Boards: All applicable
  • Modes: SoC
  • Host interfaces: N/A
1806540 Added an application level API to disconnect all BLE connections before calling sl_net_deinit to avoid the 0x1C issue. None None
  • Software variants: Standard and Lite
  • OPNs: All
  • Boards: All
  • Modes: SoC
  • Host interfaces: N/A
1659825, 1733548 Fixed an intermittent unresponsive condition observed during repeated BLE enable/disable cycles in the BLE Wi-Fi provisioning scenario. None None
  • Software variants: Standard and Lite
  • OPNs: All applicable
  • Boards: All applicable
  • Modes: SoC
  • Host interfaces: N/A

Fixed in 4.1.1#

ID Issue Description GitHub / Salesforce Reference (if any) Workaround (if any) Affected Software Variants, OPNs, Boards, Modes, Host Interfaces
1660521 Fixed an issue where sl_wifi_deinit() did not respond after repeated Wi-Fi + BLE coexistence initialization and deinitialization cycles. None None
  • Software variants: Standard and Lite
  • OPNs: All
  • Boards: All
  • Modes: SoC
  • Host interfaces: N/A
1642593 Fixed the "Unsupported LMP Parameter" issue in Matter commissioning with the Amazon ecosystem. None None
  • Software variants: Standard and Lite
  • OPNs: All
  • Boards: All
  • Modes: SoC
  • Host interfaces: SPI, UART
1703681 Fixed an issue where the application stopped responding intermittently during BLE enable/disable cycles in the BLE Wi-Fi provisioning scenario when set_adv_param failed after BLE was successfully enabled. None None
  • Software variants: Standard and Lite
  • OPNs: All
  • Boards: All
  • Modes: SoC
  • Host interfaces: SPI, UART
1694605 Fixed a power management issue where, after upgrading from WiseConnect 4.0.3 to 4.1.0, the NWP did not go to sleep properly. None None
  • Software variants: Standard and Lite
  • OPNs: All
  • Boards: All
  • Modes: SoC, NCP
  • Host interfaces: N/A

Fixed in 4.1.0#

ID Issue Description GitHub / Salesforce Reference (if any) Workaround (if any) Affected Software Variants, OPNs, Boards, Modes, Host Interfaces
1611556 Fixed an issue where LTK storage failures and security key list errors were reported during repeated BLE connect/disconnect cycles from remote devices while Wi‑Fi scan, connect, and disconnect operations were running concurrently. None None
  • Software variants: Standard and Lite
  • OPNs: All
  • Boards: All
  • Modes: SoC, NCP
  • Host interfaces: SPI, UART
1618511 Fixed an issue in the NCP wifi_power_save_deep_sleep application where invoking the power save API caused an unintended device deinitialization, resulting in a 0x11 deinitialization failure. None None
  • Software variants: Standard and Lite
  • OPNs: All
  • Boards: All
  • Modes: SoC, NCP
  • Host interfaces: SPI, UART
1530255 Fixed an issue where the deep-sleep system application could become unresponsive during extended Wi-Fi and Bluetooth® operation because the RX buffer was not released in certain data event handler error paths. None None
  • Software variants: Standard and Lite
  • OPNs: All
  • Boards: All
  • Modes: SoC, NCP
  • Host interfaces: SPI, UART
1649868 Disabled the AE feature in the wlan_ble_unified_coex_app_soc application, as this application is designed for the 8P + 2C BLE use case along with WLAN activity. None None
  • Software variants: Standard and Lite
  • OPNs: All
  • Boards: All
  • Modes: SoC
  • Host interfaces: N/A

Chip Enablement#

Added in 4.1.2#

  • Added support for 16 MB flash.

Added in 4.1.1#

None

Added in 4.1.0#

None

Application Example Changes#

New Examples | Modified Examples | Removed Examples | Deprecated Examples

Note: See the Feature Matrix section for a list of all hardware parts that work with the WiSeConnect SDK.

New Examples#

Added in 4.1.2#

None

Added in 4.1.1#

None

Added in 4.1.0#

None

Modified Examples#

Modified in 4.1.2#

None

Modified in 4.1.1#

None

Modified in 4.1.0#

Example Name Changes Supported Software Variants (if applicable) Supported Modes Supported OPNs / Boards / OPN Combinations Supported Host Interfaces
  • Wi-Fi Coex - Out-of-Box Demo
  • Concurrent NAT with BLE Provisioning
  • HTTPS BLE Dual Role
  • Station BLE Throughput App
  • Unified Coex App

See README

Updated the unified BLE component and the MQTT error-handler pattern, and fixed datatype for high_performance_socket (uint8 → uint32). Standard and Lite
  • SoC
  • NCP
  • OPNs: All
  • Boards: All
SPI, UART

Wi-Fi Coex - Wi-Fi Client BLE Provisioning with AWS (wifi_station_ble_provisioning_aws)

See README

Added optional runtime BLE enable/disable functionality using rsi_ble_enable() and rsi_ble_disable(), controlled by SL_BLE_DYNAMIC_ENABLE_DISABLE_DEMO in wifi_config.h. When enabled, the application disables BLE after Wi-Fi join, runs an optional 16k-record TLS lab demo, re-enables BLE, and reconnects Wi-Fi before MQTT. Standard
  • SoC
  • NCP
  • OPNs: All
  • Boards: All
SPI, UART

Wi-Fi Coex - Wi-Fi Client BLE Throughput App (wifi_station_ble_throughput_app)

See README

Added optional dynamic BLE disable for WLAN throughput measurement using rsi_ble_enable() and rsi_ble_disable(), controlled by SL_BLE_DYNAMIC_DISABLE_THROUGHPUT_DEMO in wifi_config.h. When enabled, the application runs WLAN throughput with BLE connected, then disables BLE, measures throughput again, and re-enables BLE with Wi-Fi reconnect. Standard
  • SoC
  • NCP
  • OPNs: All
  • Boards: All
SPI, UART

Removed Examples#

Removed in 4.1.2#

None

Removed in 4.1.1#

None

Removed in 4.1.0#

None

Deprecated Examples#

Deprecated in 4.1.2#

None

Deprecated in 4.1.1#

None

Deprecated in 4.1.0#

None

Known Issues and Limitations#

Note: See the Feature Matrix section for a list of all hardware parts that work with the WiSeConnect SDK.

Added in 4.1.2#

ID Issue or Limitation Description GitHub / Salesforce Reference (if any) Workaround (if any) Affected Software Variants, OPNs, Boards, Modes, Host Interfaces
1844697 Observed an intermittent hang issue during repeated execution of the following Wi-Fi/BLE operation sequence: BLE Connect → Wi-Fi Connect → Multi-socket Wi-Fi Data Transfer → Disconnect Wi-Fi → Disconnect BLE → Repeat. None None
  • Firmware variants: Standard and Lite
  • OPNs: All
  • Boards: All
  • Modes: SoC
  • Host interfaces: SPI, UART
1673887 In the BLE/Wi-Fi provisioning application, the DUT may become unresponsive and stop updating scan results under continuous scan requests from a third-party STA connected to the APUT. None None
  • Software variants: Standard and Lite
  • OPNs: All
  • Boards: All
  • Modes: SoC, NCP
  • Host interfaces: SPI, UART
1813357 When power save is enabled and BLE scanning is active in coexistence mode, HTTP/HTTPS downloads may not succeed. None None
  • Software variants: Standard and Lite
  • OPNs: All
  • Boards: All
  • Modes: SoC, NCP
  • Host interfaces: SPI, UART
1830732 HTTPS operations in Matter + HTTPS applications may fail with error 0x1BBD2 during TLS/SSL handshake. None None
  • Software variants: Standard and Lite
  • OPNs: All
  • Boards: All
  • Modes: SoC, NCP
  • Host interfaces: SPI, UART

Added in 4.1.1#

None

Added in 4.1.0#

ID Issue or Limitation Description GitHub / Salesforce Reference (if any) Workaround (if any) Affected Software Variants, OPNs, Boards, Modes, Host Interfaces
NA In AP + BLE mode, usage is restricted to Wi-Fi provisioning only; at any given time, only a single protocol connection is permitted, meaning that a connection can be established with either the SiWx917's Wi-Fi SoftAP or its BLE interface, but not both simultaneously. Additionally, third-party BLE connections are not supported if a third-party STA is connected to the 917 Wi-Fi SoftAP, and likewise, third-party STA connections are not supported if a third-party BLE device is already connected to the 917 BLE interface. None None
  • Software variants: Standard and Lite
  • OPNs: All
  • Boards: All
  • Modes: SoC, NCP
  • Host interfaces: SPI, UART
1455876 MQTT publish failure (error code -7) occurs for QoS 0 messages after 30 minutes when running 10 concurrent BLE connections and GATT notifications without SMP on an encrypted connectivity (network processor) firmware image. None None
  • Software variants: Standard and Lite
  • OPNs: All except IC OPNs
  • Boards: All
  • Modes: SoC, NCP
  • Host interfaces: SPI, UART
1451820 SiWx917 fails to re-connect after a few MQTT disconnections during a BLE scan start and stop loop with the wlan_ble_unified_coex_app_soc example application. None None
  • Software variants: Standard and Lite
  • OPNs: All
  • Boards: All
  • Modes: SoC, NCP
  • Host interfaces: SPI, UART
1479757 A bus thread looping issue was observed while running a multi-socket application. None None
  • Software variants: Standard and Lite
  • OPNs: All
  • Boards: All
  • Modes: SoC, NCP
  • Host interfaces: SPI, UART
1444697 BLE disconnections occur when loading or clearing the TLS certificate. None None
  • Software variants: Standard and Lite
  • OPNs: All
  • Boards: All
  • Modes: SoC, NCP
  • Host interfaces: SPI, UART
1512574 When the DUT is configured to advertise with BLE SMP enabled and a continuous WLAN scan is active, the remote BLE central device may frequently fail to pair and occasionally fail to connect. None None
  • Software variants: Standard and Lite
  • OPNs: All
  • Boards: All
  • Modes: SoC, NCP
  • Host interfaces: SPI, UART
N/A In co-existence mode, configuring 480 KB of RAM for the network processor and 192 KB for the application processor can reduce Wi-Fi throughput by approximately 10 Mbps due to limited memory available for data packets. None None
  • Software variants: Standard and Lite
  • OPNs: All
  • Boards: All
  • Modes: SoC, NCP
  • Host interfaces: SPI, UART
N/A Multiprotocol operation (Wi-Fi station + BLE) with EAP security modes is supported only for memory configurations EXT_FEAT_416K_M4SS_256K (416 KB network processor + 256 KB application processor) and EXT_FEAT_480K_M4SS_192K (480 KB network processor + 192 KB application processor). None None
  • Software variants: Standard and Lite
  • OPNs: All
  • Boards: All
  • Modes: SoC, NCP
  • Host interfaces: SPI, UART
N/A System-level changes introduced to enhance stability have resulted in some increase in power numbers (up to 15% for smaller connection intervals of 200 ms) for BLE-connected only cases for modules. Impact is smaller for longer connection intervals. None None
  • Software variants: Standard and Lite
  • OPNs: All
  • Boards: All
  • Modes: SoC, NCP
  • Host interfaces: SPI, UART
1557787 The Wi-Fi station returns error 0x1FF9C (SL_STATUS_SI91X_DHCP_HANDSHAKE_FAILURE) in congested environments when operating in concurrent mode with both NAT and PAT features enabled. None None
  • Software variants: Standard and Lite
  • OPNs: All
  • Boards: All
  • Modes: SoC, NCP
  • Host interfaces: SPI, UART
1574418 Using slc generate --toolchain gcc or slc generate --with toolchain_gcc may fail with exclusivity errors due to the wiseconnect_toolchain_gcc_standard component incorrectly providing toolchain_gcc, resulting in a conflict with the Simplicity SDK toolchain_gcc component. If using those two command line options results in exclusivity errors, then you can remove them. Note that in a future WiseConnect release, you might have to reintroduce the toolchain option on the command line. Refer to future WiseConnect release notes for updates on possible behavior changes. None None
  • Software variants: Standard and Lite
  • OPNs: All
  • Boards: All
  • Modes: SoC, NCP
  • Host interfaces: SPI, UART
1678706, 1667465 Observed an intermittent issue where the rsi_ble_enable() API does not respond during the following Wi-Fi/BLE operation sequence: BLE Connect → Wi-Fi Connect → Power Save → Disable BLE → Disconnect Wi-Fi → Enable BLE. None None
  • Software variants: Standard and Lite
  • OPNs: All
  • Boards: All
  • Modes: SoC, NCP
  • Host interfaces: SPI, UART
1659825 An intermittent hang may occur during repeated BLE enable/disable and Wi-Fi disconnect/reconnect cycles in BLE Wi-Fi Provisioning. This issue is not observed during a single run and occurs only during long-duration stress testing. None None
  • Software variants: Standard and Lite
  • OPNs: All
  • Boards: All
  • Modes: SoC, NCP
  • Host interfaces: SPI, UART
1647768 BLE disconnections may be observed intermittently when running BLE throughput, Wi-Fi UDP TX, RTC read operations continuously in a loop. None None
  • Software variants: Standard and Lite
  • OPNs: All
  • Boards: All
  • Modes: SoC
  • Host interfaces: SPI, UART
1660521 Intermittent failure or incomplete execution of sl_wifi_deinit() may occur when Wi-Fi is repeatedly initialized and deinitialized while BLE activities are concurrently running. This issue can manifest on the first cycle or after multiple cycles and is non-deterministic. None Stop all BLE scanning and advertising before initiating Wi-Fi deinitialization, allow sufficient time for the stack to reach an idle state, and avoid repeated Wi-Fi cycling in BLE coexistence scenarios.
  • Software variants: Standard and Lite
  • OPNs: All
  • Boards: All
  • Modes: SoC, NCP
  • Host interfaces: SPI, UART