Edit

Simplicity SDK Version 2026.6.2 - Release Notes (Oct 14, 2026)#

The primary tool for the Silicon Labs IoT software development ecosystem, combining wireless software development kits (SDKs) and platform into a single, integrated package.

Release Announcements#

LLVM Compiler Support Now Available#

The Simplicity SDK now supports the LLVM/Clang 21.1.1 compiler across all Series 2 and Series 3 devices, giving developers another powerful option for building high-performance, memory-efficient applications.

LLVM/Clang delivers improvements in code size and significant execution performance, with greater than 20% gains depending on their application and workload. Its advanced optimization capabilities and enhanced math libraries help developers maximize the performance of Silicon Labs MCUs while reducing flash memory requirements.

LLVM/Clang support is fully integrated into the Simplicity development environment and is available through both:

  • Simplicity Studio VS Code extension

  • CMake / Ninja CLI build system

Optimized for Series 3#

LLVM/Clang is particularly beneficial for Series 3 devices, including xG301, where its enhanced optimization pipeline and improved math libraries can help developers take full advantage of the architecture. Compute-intensive workloads (including AI/ML, DSP, sensor processing, and signal analysis) can benefit from improved execution efficiency while maintaining a smaller application footprint.

Flexible Optimization Options#

The Simplicity SDK supports both:

  • Standard LLVM/Clang compilation

  • LLVM/Clang with Link Time Optimization (LTO) for even greater whole-program optimization, enabling additional reductions in code size and further performance improvements.

By adding LLVM/Clang support, the Simplicity SDK gives developers greater flexibility to optimize their applications for performance, memory footprint, and power efficiency— helping accelerate development while maximizing the capabilities of Silicon Labs Series 2 and Series 3 devices.

Release Model#

Beginning with the 2026.6 release, Simplicity SDK releases follow a predictable biannual release model with two release types:

  • June Long-Term Support (LTS) release: The recommended baseline for production programs. During the 30-month standard maintenance window, an LTS release may receive maintenance patches and is eligible for technical support.

  • December Interim release: A shorter-maintained release for prototyping, early feature access, and development work that will move to a later LTS release. The December Interim release receives 6 months of standard maintenance and support.

Simplicity SDK releases prior to 2026.6 provide 18 months of maintenance and support.

Gecko SDK 4.5 LTS provides on-going support and maintenance for active Series 0 and 1 devices.

Customers who need to remain on a specific SDK release beyond the standard maintenance window may use Silicon Labs' SDK Extended Maintenance Service to extend maintenance for that release.

Simplicity SDK Packaging and Distribution#

Starting with the 2025.12 release, the Simplicity SDK transitions from GitHub-based monolithic delivery to a modular, Conan-based package model.

To obtain and work with the Simplicity SDK 2025.12, customers must use Silicon Labs Tool (SLT) v1.1.0 or newer, available through:

  • SLT-CLI (v1.1.0+) – a standalone command-line tool

  • Simplicity Installer (v1.1.0+) – a graphical installer that integrates SLT-CLI functionality

This update also introduces a new directory structure organized by technology and functional domain, which may affect how SDKs are integrated, consumed, and automated in developer workflows.

Developer Guidance#

CLI development (Headless or CI/CD dev setups)#

  • Need to update scripts that rely on ‘git clone’ and integrate SLT to manage and automate the SDK delivery.

  • Any tooling, scripts, or manual workflows that rely on fixed SDK paths may need to be updated accordingly.

GUI development (Simplicity Studio 6)#

  • No SLT-CLI integration is needed, but note that SDKs are now stored in versioned Conan package directories managed by SLT.

  • Directory path changes:

    • Studio 5 (SDK 2025.6): ~/SimplicityStudio/SDKs/simplicity_sdk

    • Studio 6 (SDK 2025.12): ~/.silabs/slt/installs/conan/p/simplxxxxxxxxxxx/p

Resources#

Note: This Simplicity SDK release will be published on GitHub for reference purposes only, not recommended for development. Development should use the SDK packages delivered via SLT.

Release Summary#

Release Item Version Release Date Key Features Chip Enablement

Platform

6.1.2

Oct 14, 2026

Platform MCU

  • Debug Logger: Logger support added (evaluation quality).
  • Watchdog Manager: Watchdog manager support added (evaluation quality).
  • sl_main: Added a new app_init_post_platform application hook in sl_main_second_stage_init, called after sl_platform_init, sl_driver_init, and sl_service_init complete and before sl_stack_init. This hook lets applications run initialization that depends on platform components, drivers, and services but must run before stacks are initialized.
  • Linker: Added support for RAM-only execution for provisioning applications (GCC toolchain).
  • Startup code: Added an assembly reset handler trampoline so safe code can execute before the C environment is loaded.

Security

  • None

Bootloader

  • None

Micrium OS

  • None

CPC

  • None

MVP Math Library

  • None

Platform MCU

  • Added EFR32BG29/EFR32MG29 OPN and radio board support.
  • Added EFR32FG2D and WPK Main Board (BRD4002B) support.

Security

  • None

Bootloader

  • Added support for BRD2608B, BRD2602B, BRD2600C, and BRD2603C.
  • Added support for the bootloader-spi-ezsp application on xG2B OPNs and radio boards.

RAIL Library

3.1.2

Oct 14, 2026

None None

RAIL SDK

3.1.2

Oct 14, 2026

None

None

USB

1.7.2

Oct 14, 2026

None None

Wi-Fi 6 + BLE (WiSeConnect)

4.1.2

Oct 14, 2026

Wi-Fi
  • Added LLVM compiler support, including LTO validation for Wi-Fi examples.

Network Stack

  • Added Server Name Indication (SNI) support for HTTPS PUT requests.

SiWx91x Bluetooth LE

  • Added support for LLVM compiler for BLE PSRAM examples.

Multiprotocol

  • Added PSRAM project configurations for Wi-Fi and BLE coexistence examples.
SiWx91x Platform
  • Added LTO support for PSRAM-enabled applications compiled using the LLVM or GCC toolchain.
Wi-Fi
  • Added support for 16 MB flash.
  • Added support for the EOL Sensors board (BRD2605B).

Network Stack

  • None

SiWx91x Bluetooth LE

  • Added support for the EOL Sensors BRD2605B board across all BLE examples.
  • Added support for 16 MB flash.

Multiprotocol

  • Added support for 16 MB flash.
SiWx91x Platform
  • Added SDK support for 16 MB flash.
  • Added support for the BRD2605B radio board.

OpenThread

3.1.2

Oct 14, 2026

None None

Zigbee

9.1.2

Oct 14, 2026

  • Reporting component: New configuration item SL_ZIGBEE_AF_PLUGIN_REPORTING_ENABLE_RETRY to control whether attribute reports request an APS acknowledgment.
  • End Device Support component: New configuration item SL_ZIGBEE_AF_PLUGIN_END_DEVICE_SUPPORT_START_MOVE_DELAY_JITTER_SECONDS for an optional random delay before the first rejoin/move attempt after parent loss.
None

Bluetooth LE

11.1.2

Oct 14, 2026

Example and Middleware

  • Added Serial Port Profile middleware through the new spp component and related configuration and GATT service content.
  • Added new Bluetooth peer manager and peer security middleware components for central, peripheral, filter, common, and security flows.

Host Stack

  • New flag SL_BT_PERIODIC_ADVERTISER_INCLUDE_ADVERTISING_DATA_INFORMATION in sl_bt_periodic_advertiser_flags enables the inclusion of Advertising Data Information (ADI) in transmitted periodic advertising PDUs.
  • New command sl_bt_periodic_advertiser_refresh_data_id enables refreshing the Advertising Data ID (DID) without the need to provide the same data again.
  • New mode sl_bt_sync_report_non_duplicate in sl_bt_sync_reporting_mode_t enables filtering duplicate periodic advertisements.
  • The bluetooth_feature_linklayer_interface component provides new commands sl_bt_linklayer_get_hci_connection_handle and sl_bt_linklayer_get_bgapi_connection_handle for converting between link layer HCI connection handles and the BGAPI host stack connection handles. The application needs to convert between handle types when it uses the linklayer class to access low-level link layer functionality that uses connection handles.
  • The bluetooth_feature_connection_analyzer feature can now maintain synchronization to the analyzed connection even if connection parameters or channel map is updated. The LLCP events need to be passed from the Central device to the connection analyzer device by the application. Use the bluetooth_feature_connection_analyzer_llcp_report component and the sl_bt_linklayer_event_info_reporting_enable command to enable the LLCP reporting on the Central. Pass the corresponding LLCP events from sl_bt_evt_linklayer_event_info_report events to the connection analyzer device and use sl_bt_connection_analyzer_process_llcp_event to process the event.
  • New command sl_bt_gap_set_privacy_mode_with_rpa_randomization enables configuring local privacy with separate minimum and maximum RPA rotation intervals. When the interval bounds differ, advertiser and central-side RPAs are refreshed at randomized times within the configured range. Keeping the interval bounds equal preserves deterministic rotation behavior.
  • New events sl_bt_evt_gap_random_address_refresh and sl_bt_evt_advertiser_random_address_refresh notify the application when the scanner/initiator or a stack-managed advertiser starts using a new private address. The related privacy mode commands document these events.
  • New command sl_bt_resolving_list_read_peer_resolvable_address reads the current peer resolvable private address tracked by the controller for a device in the Resolving List.
  • The bluetooth_feature_cs component adds Channel Sounding (CS) handover commands and events to the cs BGAPI class. Use the bluetooth_feature_cs_handover_leader and bluetooth_feature_cs_handover_follower components to enable the corresponding controller-side handover roles. Retrieve CS procedure parameters from the CS Leader, pass them to the CS Follower, and use the handover commands and events to synchronize the Follower to the CS procedure and LE connection and to control scheduled CS procedure execution.

Controller

  • Added support for ADI in Periodic Advertising and Periodic Advertising with Responses, improving interoperability with devices expecting this capability.
  • Added Channel Map Update Indication support for the Periodic Advertising advertiser, enabling Adaptive Frequency Hopping with Periodic Advertising for improved reliability in congested or noisy RF environments.

Multiprotocol

CMP + BLE-RCP sample applications (Zigbee NCP + OpenThread RCP + Bluetooth RCP)

  • Added new Concurrent Multiprotocol (CMP) co-processor sample projects that run Zigbee NCP, OpenThread RCP, and Bluetooth RCP on one EFR device. The Bluetooth side exposes a BLE controller over CPC so a Linux host can use the Silicon Labs RCP with CPCd and a standard Bluetooth stack (i.e. BlueZ). Zigbee and OpenThread host applications use the same CPC multiplexer model as existing NCP / RCP designs.

None.

Bluetooth Mesh

11.0.2

Oct 14, 2026

None None

Bluetooth Location Services

11.1.2

Oct 14, 2026

Real-Time Locationing Service

The RTL Service (rtl_service) is a new software component providing a unified API that works in both RTOS and bare-metal environments.

  • The service automatically adapts: in RTOS mode it runs a dedicated processing task; in bare-metal mode it processes within the application main-loop.
  • All API functions can be called from any task or interrupt context. The service handles mutual exclusion internally.
  • Submit CS or Ranging Service (RAS) procedure data and receive distance estimates asynchronously through a result callback.

RTL Library Version Function

  • A function sl_rtl_get_lib_version() was added to return the exact library version.

Algorithm Mode Enum Renaming

The enum sl_rtl_cs_algo_mode field names have been renamed as follows:

  • SL_RTL_CS_ALGO_MODE_REAL_TIME_BASIC renamed to SL_RTL_CS_ALGO_MODE_TRACKING_ACCURACY_OPTIMIZED
  • SL_RTL_CS_ALGO_MODE_REAL_TIME_FAST renamed to SL_RTL_CS_ALGO_MODE_TRACKING_LATENCY_OPTIMIZED
  • SL_RTL_CS_ALGO_MODE_STATIC_HIGH_ACCURACY renamed to SL_RTL_CS_ALGO_MODE_STATIONARY

Z-Wave

8.1.2

Oct 14, 2026

  • The Silicon Labs Bootloader now supports switching multiprotocol solutions. See the Creating Z-Wave-BLE SMP solution instruction for an example how to build a switched multiprotocol (SMP) firmware which combines a Z-Wave Switch On/Off application and a Bluetooth OTA DFU application that can upgrade the Z-Wave app
  • Added an API to customize the DTPA noise margin from the application.

    Note: The noise margin is not stored in NVM. Applications must set the customized value after each initialization.

  • Added component zw_host_hibernation to support hibernating host controller.
  • Added component zw_cc_wakeoncriticalmessage to support alpha command class Wake On Critical Message.
  • Supported new variant of Pro Kit Mainboard: BRD4002B. The new SHT40 sensor and the previous sensor are supported by a unidriver component for dynamic run-time selection in the sample applications. Note that it causes a RAM usage increase. To avoid increased RAM usage in production, use a dedicated driver for the sensors.
None

Wi-SUN

2.13.1

Oct 14, 2026

None

None

Silicon Labs Matter

2.9.2

Oct 15, 2026

None

Added support for the redesigned BRD2605B and BRD2608B sensor boards.

Silicon Labs Aliro

2.0.1

Oct 14, 2026

  • CSA Aliro Specification 1.0.0 reader implementation for NFC and Bluetooth LE on EFR32 MG24 and MG26.
  • Aliro Minimal Reader and AliroMatterLock sample applications (NFC and BLE variants).
  • Matter over Thread integration for Aliro-enabled door lock applications (AliroMatterLock).
  • BRD4186C / SLWSTK6006A / Wireless Starter Kit / 2.4 GHz @ 10 dBm - xG24-RB4186C
  • BRD4187C / SLWSTK6006A / Wireless Starter Kit / 2.4 GHz @ 20 dBm - xG24-RB4187C
  • BRD2601B / MG24 Developer Kit - xG24-DK2601B
  • BRD4116A, BRD4117A, BRD4118A, BRD4120A, BRD4121A

Amazon Sidewalk

2.9.2

Oct 14, 2026

  • Cloud Light SoC Sample application.
  • Supporting new Temperature sensor on WPK board.
  • Application tab enablement in Sidewalk Assistant.
  • Updated libraries to Amazon Stack 1.19.4.
  • Stability improvements.
None

Connect

4.3.2

Oct 14, 2026

None

None

Machine Learning

3.0.2

Oct 14, 2026

  • New DX for adding ML Models to new or existing projects.
  • New APIs to initialize, execute, and de-initialize ML models.
  • Project upgrades require manual effort. See the AI-assisted migration prompt.
  • Multiple-Model feature to add and execute multiple ML models in a project.
Added support for EFM32 devices.

Simplicity Connect Mobile App

3.3.2

Oct 14, 2026

    None
None

Note: Click here for earlier releases on GitHub.

Looking for older release notes? You can still access previous versions for both Simplicity SDK (prior to 2025.6.0) and Gecko SDK here.