RAIL SDK Version 3.1.2 - Release Notes (Oct 14, 2026)#

The RAIL SDK is a complete software development suite for proprietary wireless applications. It was previously part of the Proprietary SDK. Starting with the RAIL SDK 2.18.0 release, Proprietary SDK is split into RAIL SDK and Connect SDK.

Silicon Labs RAIL (Radio Abstraction Interface Layer) is an intuitive and easily-customizable radio interface layer designed to support both proprietary and standards-based wireless protocols.

The RAIL SDK is supplied with extensive documentation and sample applications.

Release Summary#

Key Features | API Changes | Bug Fixes | Chip Enablement

Key Features#

Added in 3.1.2#

None.

Added in 3.1.1#

None.

Added in 3.1.0#

None.

API Changes#

Changed in 3.1.2#

None.

Changed in 3.1.1#

None.

Changed in 3.1.0#

None.

Bug Fixes#

Fixed in 3.1.2#

None.

Fixed in 3.1.1#

None.

Fixed in 3.1.0#

None.

Chip Enablement#

New Chip Supported in 3.1.2#

None.

New Chip Supported in 3.1.1#

None.

New Chip Supported in 3.1.0#

None.

Key Features#

New Features | Enhancements | Removed Features | Deprecated Features

New Features#

Added in 3.1.2#

None.

Added in 3.1.1#

None.

Added in 3.1.0#

None.

Enhancements#

Added in 3.1.2#

None.

Added in 3.1.1#

None.

Added in 3.1.0#

None.

Removed Features#

Removed in 3.1.2#

None.

Removed in 3.1.1#

None.

Removed in 3.1.0#

None.

Deprecated Features#

None.

API Changes#

New APIs | Modified APIs | Removed APIs | Deprecated APIs

New APIs#

Added in 3.1.2#

None.

Added in 3.1.1#

None.

Added in 3.1.0#

None.

Modified APIs#

Modified in 3.1.2#

None.

Modified in 3.1.1#

None.

Modified in 3.1.0#

None.

Removed APIs#

Removed in 3.1.2#

None.

Removed in 3.1.1#

None.

Removed in 3.1.0#

None.

Deprecated APIs#

None.

Bug Fixes#

Fixed in 3.1.2#

None.

Fixed in 3.1.1#

None.

Fixed in 3.1.0#

None.

Chip Enablement#

None.

Application Example Changes#

New Examples | Modified Examples | Removed Examples | Deprecated Examples

New Examples#

None.

Modified Examples#

None.

Removed Examples#

None.

Deprecated Examples#

None.

Impact of Release Changes#

Impact Statements | Migration Guide

Impact Statements#

None.

Migration Guide#

For a list of deprecated, removed, and modified items, see the migration guide.

Known Issues and Limitations#

ID Issue or Limitation Description GitHub / Salesforce Reference (if any) Workaround (if any) Affected Software Variants, Hardware, Modes, Host Interfaces
1268208 The power consumption of DK2600 can't be optimized if the configuration time for EM2 and if UART are both being used, as the value of SL_IOSTREAM_USART_{instance}_BAUDRATE does not take effect. The default value used instead is 115200 bps. Typical use case is RAIL - SoC Wireless M-bus Meter with DK2600 board. None Update UART baud rate to 9600 bps at Simplicity Studio Admin Console. This is necessary for EM2.
  • RAIL SDK sample applications
  • BRD2600A
  • SoC
  • UART interface
1274248 Range Test DMP instabilities in case of LTO. None Do not use LTO.
  • Range Test DMP sample applications
  • All supported boards
  • SoC
1375450 Wi-SUN HAN phys aren't supported by Standard packet assembler and Packet Assistant components. None Do not use Wi-SUN HAN phys with RAIL SDK sample applications.
  • RAIL SDK sample applications
  • All supported boards
  • SoC, NCP mode
  • UART, SPI interface
Updating the Baremetal sample applications to RTOS causes build errors. None

Follow the Platforms guide sl_main Baremetal to RTOS Application Transition.

  • RAIL SDK Baremetal sample applications
  • All supported boards
  • SoC, NCP mode
  • UART, SPI interface

Using This Release#

What's in the Release? | Compatible Software | Installation and Use | Help and Feedback

What's in the Release?#

RAIL SDK showcasing the usage of the RAIL library

Compatible Software#

None.

Installation and Use#

To upgrade your existing software with this release, see instructions in the migration guide.

To run your first demo, see our Getting Started Guides.

To kick start your development, see our Developer's Guide.

For information about Secure Vault Integration, see Secure Vault.

To review Security and Software Advisory notifications and manage your notification preferences:

  1. Go to https://community.silabs.com/.

  2. Log in with your account credentials.

  3. Click your profile icon in the upper-right corner of the page.

  4. Select Notifications from the dropdown menu.

  5. In the Notifications section, go to the My Product Notifications tab to review historical Security and Software Advisory notifications

  6. To manage your preferences, use the Manage Notifications tab to customize which product updates and advisories you receive.

To learn more about the software in this release, dive into our online documentation.

Help and Feedback#

SDK Release and Maintenance Policy#

See our SDK Release and Maintenance Policy.