Edit

Bluetooth Location Services Version 11.1.2 - Release Notes (Oct 14, 2026)#

The Real-Time Locating (RTL) library contains features for high accuracy distance estimation, Angle of Arrival / Departure estimation and spatial positioning. The software library comes with a C-programming language API for ARM Cortex M33, Windows (x86_64) and Linux (ARM Cortex A, x86_64) hosts.

Click here for earlier releases.

Release Summary#

Key Features | API Changes | Bug Fixes | Chip Enablement

Key Features#

Added in 11.1.2#

None.

Added in 11.1.1#

  • Added configurable likeliness threshold for CS distance estimation, allowing filtering of low-confidence results.

Added in 11.1.0#

  • Added new RTL Service component (rtl_service) providing a unified, thread-safe API for RTOS and bare-metal environments.

  • Added sl_rtl_get_lib_version() function to retrieve the RTL library version.

  • Renamed algorithm mode enums with backward-compatible defines.

  • Improved PBR distance measurement accuracy for SL_RTL_CS_ALGO_MODE_STATIONARY.

API Changes#

Changed in 11.1.2#

None.

Changed in 11.1.1#

  • Added SL_RTL_LIKELINESS_THRESHOLD to sl_rtl_cs_estimator_param_type and SL_RTL_ERROR_LIKELINESS_BELOW_THRESHOLD error code.

Changed in 11.1.0#

  • Added RTL Service APIs for context and instance lifecycle, configuration, and result queries.

  • Added sl_rtl_get_lib_version() function.

  • Modified sl_rtl_util_validate_bluetooth_cs_channel_map to add sub_mode parameter.

  • Old sl_bt_cs_ APIs now return error when running in RTOS mode.

Bug Fixes#

Fixed in 11.1.2#

None.

Fixed in 11.1.1#

None.

  • Removed maximum distance limitation of 40 m for PBR estimation in SL_RTL_CS_ALGO_MODE_TRACKING_ACCURACY_OPTIMIZED.

  • CS API now returns error for unsupported submode and channel map combinations.

Chip Enablement#

None.

Key Features#

New Features | Enhancements | Removed Features | Deprecated Features

New Features#

Added in 11.1.2#

None.

Added in 11.1.1#

Likeliness Threshold for CS Distance Estimation#

Added SL_RTL_LIKELINESS_THRESHOLD to the sl_rtl_cs_estimator_param_type enum and likeliness_threshold to the sl_rtl_cs_estimator_param_value union, allowing the customer to set a configurable likeliness limit for CS distance estimation results. When a procedure result falls below the configured threshold, the error SL_RTL_ERROR_LIKELINESS_BELOW_THRESHOLD is returned. The default value is 0.0 (no filtering).

Added in 11.1.0#

Real-Time Locationing Service#

The RTL Service (rtl_service) is a new software component providing a unified API that works in both RTOS and bare-metal environments.

  • The service automatically adapts: in RTOS mode it runs a dedicated processing task; in bare-metal mode it processes within the application main-loop.

  • All API functions can be called from any task or interrupt context. The service handles mutual exclusion internally.

  • Submit CS or Ranging Service (RAS) procedure data and receive distance estimates asynchronously through a result callback.

RTL Library Version Function#

A function sl_rtl_get_lib_version() was added to return the exact library version.

Algorithm Mode Enum Renaming#

The enum sl_rtl_cs_algo_mode field names have been renamed as follows:

  • SL_RTL_CS_ALGO_MODE_REAL_TIME_BASIC renamed to SL_RTL_CS_ALGO_MODE_TRACKING_ACCURACY_OPTIMIZED

  • SL_RTL_CS_ALGO_MODE_REAL_TIME_FAST renamed to SL_RTL_CS_ALGO_MODE_TRACKING_LATENCY_OPTIMIZED

  • SL_RTL_CS_ALGO_MODE_STATIC_HIGH_ACCURACY renamed to SL_RTL_CS_ALGO_MODE_STATIONARY

Backward-compatible defines are provided for existing code. Additionally, SL_RTL_CS_ALGO_MODE_INVALID has been added.

Enhancements#

Added in 11.1.2#

None.

Added in 11.1.1#

None.

Added in 11.1.0#

Improved PBR Distance Measurement Accuracy#

PBR distance measurement accuracy has been improved for SL_RTL_CS_ALGO_MODE_STATIONARY.

Removed Features#

Removed in 11.1.2#

None.

Removed in 11.1.1#

None.

Removed in 11.1.0#

LOW Preset Channel Map Removed#

The LOW preset channel map has been removed. Attempting to configure RTLLib with LOW channel map preset will result in an error during estimator creation.

Deprecated Features#

Deprecated in 11.1.2#

None.

Deprecated in 11.1.1#

None.

API Changes#

New APIs | Modified APIs | Removed APIs | Deprecated APIs

New APIs#

Added in 11.1.2#

None.

Added in 11.1.1#

None.

Added in 11.1.0#

New API Signature

Deprecated API replaced by this

sl_rtl_get_lib_version()

N/A

sl_rtl_service_init_cs()

N/A

sl_rtl_service_deinit_cs()

N/A

sl_rtl_service_create_cs_instance()

N/A

sl_rtl_service_destroy_cs_instance()

N/A

sl_rtl_service_set_cs_algo_mode()

N/A

sl_rtl_service_set_cs_mode()

N/A

sl_rtl_service_set_cs_params()

N/A

sl_rtl_service_create_cs_estimator()

N/A

sl_rtl_service_set_cs_estimator_param()

N/A

sl_rtl_service_process_cs()

N/A

sl_rtl_service_process_ras()

N/A

sl_rtl_service_get_cs_distance_estimate()

N/A

sl_rtl_service_get_cs_distance_estimate_confidence()

N/A

sl_rtl_service_get_cs_distance_estimate_extended_info()

N/A

Modified APIs#

Modified in 11.1.2#

None.

Modified in 11.1.1#

Old API

Modified

sl_rtl_cs_estimator_param_type

Added SL_RTL_LIKELINESS_THRESHOLD enum value.

sl_rtl_cs_estimator_param_value

Added likeliness_threshold union member.

sl_rtl_error_code

Added SL_RTL_ERROR_LIKELINESS_BELOW_THRESHOLD error code.

Modified in 11.1.0#

Old API

Modified

sl_rtl_util_validate_bluetooth_cs_channel_map(cs_mode, ...)

sl_rtl_util_validate_bluetooth_cs_channel_map(main_mode, sub_mode, ...): Input parameter cs_mode renamed to main_mode and new parameter sub_mode added.

Removed APIs#

Removed in 11.1.2#

None.

Removed in 11.1.1#

None.

Removed in 11.1.0#

None.

Deprecated APIs#

Deprecated in 11.1.2#

None.

Deprecated in 11.1.1#

None.

Deprecated in 11.1.0#

None.

Bug Fixes#

Fixed in 11.1.2#

None.

ID Issue Description GitHub / Salesforce Reference (if any) Affected SW or HW Variants, Modes
1569167 Maximum distance limitation of 40 m for PBR estimation in algorithm mode SL_RTL_CS_ALGO_MODE_TRACKING_ACCURACY_OPTIMIZED has been removed. None SL_RTL_CS_ALGO_MODE_TRACKING_ACCURACY_OPTIMIZED
1524912 CS API will now return error if the unsupported combinations listed below are attempted: Main mode: PBR, sub mode: RTT, algorithm mode: SL_RTL_CS_ALGO_MODE_TRACKING_LATENCY_OPTIMIZED or SL_RTL_CS_ALGO_MODE_TRACKING_ACCURACY_OPTIMIZED, Channel map preset: MEDIUM. None PBR with RTT sub mode

Chip Enablement#

None.

Known Issues and Limitations#

ID Issue or Limitation Description GitHub / Salesforce Reference (if any) Workaround (if any) Affected Software Variants, Hardware, Modes, Host Interfaces
1442293 The velocity output in RTF algorithm mode is for experimental use only in this release. The value may have large outliers, and the distance measurement may stay fixed around the same value in certain cases e.g., when the device is in back pocket. None None EFR32xG24
1449019 The RTF algorithm mode with medium channel map has weak accuracy in some NLOS cases. None None EFR32xG24
1569167 The maximum range is limited to 70 meters in STATIC_HIGH_ACCURACY mode. None None EFR32xG24

Impact of Release Changes#

Impact Statements in 11.1.2#

None.

Impact Statements and Migrations from 11.0.x to 11.1.0#

Change Migration Guide Affected Software Variants if applicable Affected Modes Affected OPNs / Boards / OPN Combinations Affected Host Interfaces
Value change of SL_RTL_CS_MODE_NONE Rebuild the application if this enum is used; otherwise no impact. All All Hardware agnostic N/A
Parameter change in sl_rtl_util_validate_bluetooth_cs_channel_map Update calls to include the new sub_mode parameter. The cs_mode parameter has been renamed to main_mode. All All Hardware agnostic N/A

Using This Release#

Compatible Software | Installation and Use | Help and Feedback

Compatible Software#

Software Compatible Version or Variant
Simplicity SDK 2026.6.0
GCC 14.2.1
LLVM 21.1.1 (provided with Simplicity Studio)

Installation and Use#

For instructions on developing with the RTL library, see Developing Bluetooth Location Services Applications and the API reference included with the documentation installed through Simplicity Studio in the Bluetooth SDK.

Development Kit customers are eligible for training and technical support. Use the Silicon Labs Bluetooth LE web page to obtain information about all Silicon Labs Bluetooth products and services, and to sign up for product support.

For information about Secure Vault Integration, see Secure Vault.

To review Security and Software Advisory notifications and manage your notification preferences:

  1. Go to https://community.silabs.com/.

  2. Log in with your account credentials.

  3. Click your profile icon in the upper-right corner of the page.

  4. Select Notifications from the dropdown menu.

  5. In the Notifications section, go to the My Product Notifications tab to review historical Security and Software Advisory notifications

  6. To manage your preferences, use the Manage Notifications tab to customize which product updates and advisories you receive.

Help and Feedback#

SDK Release and Maintenance Policy#

See our SDK Release and Maintenance Policy.