Edit

Z-Wave SDK Version 8.1.2 - Release Notes (Oct 14, 2026)#

Z-Wave and Z-Wave Long Range SDK are designed to meet the demands of the future smart home and beyond, where increasing needs for more sensors and battery-operated devices require both long range and low power. Context-aware environments are the next evolution in the smart home market, and they require technologies that have been optimized specifically for these applications.

Click here for earlier releases.

Release Summary#

Key Features | API Changes | Bug Fixes | Chip Enablement

Key Features#

Added in 8.1.2#

  • LLVM 21.1.1 compiler support for Z-Wave applications.

Added in 8.1.1#

  • This release restores proper Z-Wave Image Rejection (IR) calibration, allowing accurate detection of in-band interference and improving overall RF performance across all supported chips.

Added in 8.1.0#

  • The Silicon Labs Bootloader now supports switching multiprotocol solutions. See the Creating Z-Wave-BLE SMP solution instruction for an example how to build a switched multiprotocol (SMP) firmware which combines a Z-Wave Switch On/Off application and a Bluetooth OTA DFU application that can upgrade the Z-Wave app.

API Changes#

Changed in 8.1.2#

None.

Changed in 8.1.1#

  • The Serial API command Get Node Information Protocol Data is no longer supported on end devices (which do not store other nodes' information), and Request Node Information is now supported on both end devices and controllers.

Changed in 8.1.0#

  • (Breaking change) On Series 2, SL_SLEEPTIMER_PERIPHERAL must be SL_SLEEPTIMER_PERIPHERAL_DEFAULT (typically SYSRTC), not BURTC. The platform sleeptimer and Z-Wave deep sleep (zw_shutdown_manager) must not use the same peripheral: BURTC is reserved for EM4 wake-up and compare programming. Project generation fails if BURTC is selected. When you migrate a project from an older SDK, SL_SLEEPTIMER_PERIPHERAL is updated to DEFAULT automatically (Simplicity SDK project migration / upgrade.slcu and sleeptimer_peripheral_upgrade.lua).

Bug Fixes#

Fixed in 8.1.2#

The following table lists the key issues fixed in this release. For a complete list, see this section.

  • Serial API NVM backup and restore (FUNC_ID_NVM_BACKUP_RESTORE and FUNC_ID_NVM_EXT_BACKUP_RESTORE) could read or write outside the NVM region under certain conditions. Offsets at or past the end of the NVM region now return EOF with a data length of 0 without accessing flash, and read or write failures are reported as errors. Hosts that follow the size reported on open are unaffected.

  • Fixed SUC Node ID Command handling so that a secondary controller cannot advertise the SUC Node ID to the SUC itself, and the SUC no longer interprets self-addressed advertisements in a way that can degrade or cause the loss of its SUC role.

  • NODES_EXIST topology updates are now validated, and safeguards are added based on the SIS role, frame validity, sender identity, and Automatic Controller Update state.

  • Fixed an issue where end devices did not respond to S2 Commands Supported Get after a post-OTA reboot, which could stall the post-OTA interview.

  • Fixed the Serial API Setup Set Max LR Tx Power command on 20 dBm boards so that they can set and use the maximum Long Range transmit power.

Fixed in 8.1.1#

The following table lists the key issues fixed in this release. For a complete list, see this section.

  • Radio was not correctly calibrated at startup. Because of this bad calibration, RSSI measurements were affected by close frequencies. In addition to bad noise measurements, this could have also affected CCA, so a channel may have looked busy because of activity on a close frequency. Only EFR32ZG28 was affected.

  • Long transmission stalls observed in certain congested RF conditions have been fixed by ensuring that transmissions are only attempted when LBT conditions are met.

Fixed in 8.1.0#

The following table lists the key issues fixed in this release. For a complete list, see this section.

  • The Multilevel Sensor Command Class now correctly reports its multi-channel capabilities.

  • Network Level Security (NLS) support is no longer enabled by default. Added the optional zw_s2_nls_support component to advertise NLS support in the KEX Report during S2 inclusion. This allows alpha testing of NLS while avoiding certification issues when the feature is not certified.

  • Adjusted the dynamic Tx power algorithm margin to 6 dBm to provide additional headroom and reduce the probability of first-attempt transmission failures.

  • The ZW_DCDC_CONFIG setting (Project Configurator / zw_hardware_config.h) is now applied at startup. Previously, the device always operated in AUTO mode regardless of the configured setting. See the migration guide for information about the available modes. If sleep current remains high after transmission at very low battery voltages (approximately 2.1–2.5 V), consider using BYPASS mode.

  • NLS enabled nodes would accept protocol encrypted commands with a lower security level. This issue is now fixed and NLS enabled nodes will accept only the highest security level for encrypted protocol commands.

  • Use of SerialAPI command Set RF Receive Mode with a FL configured SerialAPI end device would result in an unresponsive device. This issue is now fixed and the node will restart on Set RF Receive Mode ON to ensure correct configuration of the radio.

  • In some cases, the first LR frame after startup was sent with an invalid noise level. Now it waits until a valid noise level is available before sending the first LR frame.

  • Fixed Transport Service handling for Long Range controllers with node IDs above 255 so fragmented responses use the correct destination node ID.

  • Fixed an issue where Serial API Controller could re-enable Long Range auto channel after reset even when Channel A or Channel B had been selected explicitly.

  • Fixed end-of-beam fragment detection so Frequently Listening nodes can acknowledge fragmented beams correctly, improving response latency.

  • Fixed transmission locking so the lock starts only after a successful transmission, avoiding incorrect lockouts after failed attempts.

  • Fixed a CCA/CSMA regression where transmissions could start while the channel was still busy, causing collisions.

  • Corrected LBT/CCA threshold handling for 2-channel and Long Range regions in zpal_radio.

  • Refactored and fixed app_session_id handling through the transmit stack: session IDs are carried from the Serial API into the transport and security layers (S0/S2) and returned in extended TX status, with separate unicast/multicast tracking to avoid overwrites during concurrent sends.

Chip Enablement#

None.

Key Features#

New Features | Enhancements | Removed Features | Deprecated Features

New Features#

Added in 8.1.2#

  • LLVM 21.1.1 compiler support for Z-Wave applications.

Added in 8.1.1#

  • Proper Z-Wave Image Rejection (IR) calibration has been restored. Previously, IR calibration was effectively inactive and the radio operated with incorrect settings on every boot. Valid calibration values are now stored in non-volatile memory, applied at startup, and refreshed on region change. Accurate image rejection prevents the receiver from misreading in-band interference as channel activity, eliminating spurious Listen Before Talk (LBT) failures in certain dual-channel scenarios. Overall RF performance has been improved across all supported chips.

  • Serial API applications now allow the host application to send non-secure protocol commands to nodes with NLS enabled for testing purposes.

Added in 8.1.0#

  • The Silicon Labs Bootloader now supports switching multiprotocol solutions. See the Creating Z-Wave-BLE SMP solution instruction for an example how to build a switched multiprotocol (SMP) firmware which combines a Z-Wave Switch On/Off application and a Bluetooth OTA DFU application that can upgrade the Z-Wave app.

  • Added an API to customize the DTPA noise margin from the application.
    Note: The noise margin is not stored in NVM. Applications must set the customized value after each initialization.

  • Added component zw_host_hibernation to support hibernating host controller.

  • Added component zw_cc_wakeoncriticalmessage to support alpha command class Wake On Critical Message.

  • Supported new variant of Pro Kit Mainboard: BRD4002B. The new SHT40 sensor and the previous sensor are supported by a unidriver component for dynamic run-time selection in the sample applications. Note that it causes a RAM usage increase. To avoid increased RAM usage in production, use a dedicated driver for the sensors.

Enhancements#

Added in 8.1.1#

  • SmartStart power consumption has been optimized. Image Rejection calibration is now scheduled by RAIL. This can cause a short, temporary increase in power consumption on significant PHY changes (such as changing the transmit region).

Added in 8.1.0#

  • BURTC is now initialized only in Z-Wave application code (zw_shutdown_manager) for never-listening EM4 entry and wake-up. The platform sl_sleeptimer uses the default peripheral (SYSRTC on Series 2). Remaining sleeptimer ticks are converted to BURTC ticks when programming the EM4 compare register. For internal measurement results from the Sensor PIR sample application, see Smart Start pre-inclusion power.

  • Smart Start pre-inclusion power: For never-listening battery end devices, Smart Start pre-inclusion power consumption is significantly lower. On the Z-Wave Sensor PIR reference application, average supply current measured 4 minutes after startup (device not yet included, Smart Start idle) decreased from about 0.75 mA to about 0.21 mA (~72% lower) in internal measurements. Previously, Smart Start kept the radio in a stay-awake state (EM1) between activity instead of allowing deep shutdown, to avoid a dependency on application code. Smart Start now uses an internal state machine that preserves its state in retention across EM4, so pre-inclusion idle periods can use deep sleep instead of holding the radio awake.

  • Increased SPAN decryption capacity on end devices to 5 values per CC:009F.01.00.12.003, reducing network congestion by recovering from lost messages without S2 re-synchronization.

  • Improved S2 SPAN synchronization handling to mitigate conflicts when the sender and the receiver transmit simultaneously.

  • Multilevel Sensor Command Class: Endpoint-aware sensor and scale querying functions are now available.

  • CLI components now only use the iostream component. The app_log component is no longer used by the CLI. This allows logs to be accessed via an interface different from the CLI (e.g., logging through RTT and CLI through UART). Note that a migration script will restore app_log in old projects for backward compatibility.

  • Improved channel lock management in the 3ch region. A channel is now locked only after a successful transmission. Previously, the channel could remain locked even if the transmission failed, especially in case of LBT failure.

  • Improved SmartStart performance when multiple devices are started at the same time, reducing contention during inclusion.

  • Refined SmartStart backoff timing so inclusion activity is spread more evenly across devices.

Removed Features#

None.

Deprecated Features#

None.

API Changes#

New APIs | Modified APIs | Removed APIs | Deprecated APIs

New APIs#

Added in 8.1.2#

None.

Added in 8.1.1#

None.

Added in 8.1.0#

New API Signature Deprecated API replaced by this (if any)
cc_multilevel_sensor_get_supported_scale_by_endpoint None
cc_multilevel_sensor_get_supported_sensors_by_endpoint None
ZW_dtpa_set_noise_margin None
ZW_dtpa_get_noise_margin None

For more details, refer to the Migration Guide.

Modified APIs#

Changed in 8.1.2#

None.

Changed in 8.1.1#

Old API Modified API
SAPI command Get Node Information Protocol Data was supporetd by all device types The command is no longer supported by end devices as these do not store the node information of other nodes
SAPI command Request Node Information was not supported by end devices The command is now supported by both end devices and controllers

Changed in 8.1.0#

Old API Modified API
SL_SLEEPTIMER_PERIPHERAL default was BURTC SL_SLEEPTIMER_PERIPHERAL default is now SYSRTC (SL_SLEEPTIMER_PERIPHERAL_DEFAULT). Project configuration (slcp) must use the new default; build validation fails if left as BURTC. Project migration from an older SDK automatically sets non-DEFAULT values to SL_SLEEPTIMER_PERIPHERAL_DEFAULT via upgrade.slcu and sleeptimer_peripheral_upgrade.lua.
zpal_radio_get_background_rssi used to unconditionally return ZPAL_STATUS_OK zpal_radio_get_background_rssi now returns ZPAL_STATUS_BUSY when the radio is busy or if the underlying RSSI measurement is not available. In this case, rssi is set to SL_RADIO_RSSI_INVALID_DBM.

Removed APIs#

Removed in 8.1.2#

None.

Removed in 8.1.1#

None.

Removed in 8.1.0#

Removed API

Was Deprecated?

Explanation

cc_configuration_set_interface

No

Unimplemented function declaration. The behavior can be changed by overriding the weakly defined default implementation.

cc_configuration_set_default_configuration

No

Default configuration parameter values can be defined via the cc_config file.

Deprecated APIs#

None.

Bug Fixes#

Fixed in 8.1.2#

ID Issue Description GitHub / Salesforce Reference (if any) Affected Software Variants, Hardware, Modes, Host Interfaces
1826914Prevented removal of SUC role from a Static Update Controller via an external SUC Node ID advertisement. A SUC no longer accepts such advertisements if they originate from a secondary controller or from the SUC itself, or if the frame's contents are invalid. Role transfer remains possible exclusively through the Set SUC command.NoneNCP Serial API Controller (Static Update Controller role)
1817992Validated NODES_EXIST topology updates. Added safeguards for NODES_EXIST processing based on SIS role, frame validity, sender identity, and Automatic Controller Update state to prevent unintended removal of nodes from the controller database.00343085NCP Serial API Controller
1817990Fixed an issue where, after a successful OTA update and reboot, the end device would acknowledge S2 Commands Supported Get but not transmit S2 Commands Supported Report or an SOS Nonce Report, stalling the post-OTA interview.NoneEnd devices
1813402Serial API NVM backup and restore (FUNC_ID_NVM_BACKUP_RESTORE and FUNC_ID_NVM_EXT_BACKUP_RESTORE) could read or write outside the NVM region under certain conditions. Offsets at or past the end of the NVM region now return EOF with data length 0 without accessing flash, and read or write failures are reported as an error. Hosts that follow the size reported on open are unaffected.00343720SerialAPI Controller and End Device, NVM backup and restore host commands
1760825Fixed Serial API Setup command Set Max LR Tx Power (0x0B 0x03) so it correctly applies the requested maximum Long Range transmit power on 20 dBm boards (previously failed and remained unchanged, capping actual TX power to 14 dBm).00343433NCP Serial API Controller and End Device on 20 dBm boards (e.g. BRD4210A, BRD4401C)
1694596Fixed an unexpected wake-up/reset on never-listening applications after attempting to send a Battery Report while communication with the controller is unavailable.NoneNever Listening end devices
1831275Fixed an issue where, after several transmission failures on a congested network, the device could no longer send frames.NoneAll devices

Fixed in 8.1.1#

ID Issue Description GitHub / Salesforce Reference (if any) Affected Software Variants, Hardware, Modes, Host Interfaces
1661022Radio was not correctly calibrated at startup. Because of this bad calibration, RSSI measurements were affected by close frequencies. In addition to bad noise measurements, this could have also affected CCA, so a channel may have looked busy because of activity on a close frequency. Only EFRZG28 was affected.EFR32ZG28 devices
1683767LBT CSMA is now handled in the Z-Wave PAL instead of RAIL's hardware CSMA, which could transmit even when LBT conditions were not met. The PAL uses RAIL for CCA only and performs CSMA retries in software, ensuring correct LBT behavior and preventing long transmission stalls in congested RF conditions.Series 2 devices
1566733Fixed occasionally missing frame after the fragmented beam following an LBT failure in the JP region.NCP Serial API Controller
1583206Fixed an issue with fragmented beam period variability that caused fragment drift and occasional out-of-spec timing.NCP Serial API Controller

Fixed in 8.1.0#

ID Issue Description GitHub / Salesforce Reference (if any) Affected Software Variants, Hardware, Modes, Host Interfaces
1556587Regardless of the endpoint specified in the query, every sensor type supported by the device was reported for every multi channel endpoint and only the supported scales of the first endpoint were reported for any single sensor type.NoneMultilevel Sensor Command Class
1596754NLS Support was advertised in KEX Report for all end node firmwares since version 7.23.0 even when the feature was not certified, which could cause certification issues. Added optional component (zw_s2_nls_support) to allow users to choose whether to enable NLS support for alpha testing.NoneS2V2, end nodes
1568087The ZW_DCDC_CONFIG setting had no effect: startup always forced AUTO. The chosen mode (AUTO, BYPASS, or DCDC low-noise) is now applied from zw_hardware_config.h / Project Configurator.NoneDevices using on-chip DC/DC
1506054With the default AUTO mode, some products on a weak supply (about 2.1–2.5 V) saw higher sleep current after transmitting. You can now change ZW_DCDC_CONFIG (for example BYPASS) instead of being stuck on AUTO.00332759Battery / low-voltage supplies, DC/DC-capable parts
1570179Use of SerialAPI command Set RF Receive Mode with a FL configured SerialAPI end device would result in an unresponsive device. This issue is now fixed and the node will restart on Set RF Receive Mode ON to ensure correct configuration of the radio.NoneSerialAPI End Device in Frequently Listening device type mode
1619678NLS enabled nodes would accept protocol encrypted commands with a lower security level. This issue is now fixed and NLS enabled nodes will accept only the highest security level for encrypted protocol commands.NoneS2V2, end nodes with NLS support enabled (alpha feature)
1630119In some cases, the first LR frame after startup was sent with an invalid noise level. Now wait until a valid noise level is available before sending the first LR frame. NoneLR & Dynamic Tx Power Algorithm
1629596Fixed Transport Service handling for Long Range controllers with node IDs above 255 so fragmented responses use the correct destination node ID.NoneLong Range devices
1625699Fixed an issue where Serial API Controller could re-enable Long Range auto channel after reset even when Channel A or Channel B had been selected explicitly.NoneNCP Serial API Controller
1568316Fixed end-of-beam fragment detection so Frequently Listening nodes can acknowledge fragmented beams correctly, improving response latency.NoneFrequently Listening device type
1557297Reduced never-listening SmartStart awake time so devices no longer stay awake significantly longer than expected during SmartStart activity.NoneNever listening device type
1639024Fixed transmission locking so the lock starts only after a successful transmission, avoiding incorrect lockouts after failed attempts.None3ch region, especially after LBT failure
1620305Updated background RSSI handling to return zpal_status_busy when the sampled RSSI value is invalid.NoneZ-Wave Platform Abstraction Layer
1594583Fixed a CCA/CSMA regression where transmissions could start while the channel was still busy, causing collisions.NoneLBT / CCA-CSMA transmit path
1590900Corrected LBT/CCA threshold handling for 2-channel and Long Range regions in zpal_radio.None2-channel regions and Long Range regions
1586442Refactored and fixed app_session_id handling through the transmit stack: session IDs are carried from the Serial API into the transport and security layers (S0/S2) and returned in extended TX status, with separate unicast/multicast tracking to avoid overwrites during concurrent sends.NoneSerial API command handling
1568859Frequently Listening device type applications originally created with an SDK version lower than 8.0.0 could become unresponsive when upgraded to a higher SDK version due to a misaligned power-management configuration. Upgrades now apply the required configuration automatically.NoneFrequently Listening device type applications
1562754Fixed an out-of-bounds access in NOP frame handling.NoneNever Listening and Frequently Listening device type applications before inclusion
1574930Corrected retry statistics tracking to use proper channel indexing for the LR dynamic channel switchNoneLong Range devices

Chip Enablement#

None.

Application Example Changes#

New Examples | Modified Examples | Removed Examples | Deprecated Examples

New Examples#

None.

Modified Examples#

None.

Removed Examples#

None.

Deprecated Examples#

None.

Known Issues and Limitations#

Workarounds

ID Issue or Limitation Description GitHub / Salesforce Reference (if any) Workaround (if any) Affected Software Variants, Hardware, Modes, Host Interfaces
1399709Reported S2 command class version remains 1 until certification covers S2v2.Currently not available.All Z-Wave applications
369430All S2 multicast frames are sent using verified delivery S2_TXOPTION_VERIFY_DELIVERY whether or not a response is expected. Change source code depending on the frame sent.ZAF
1067228Zniffer on BRD4204D does not detect LR wakeup beams.Use different board for sniffing LR wakeup beams.zwave_ncp_zniffer
1574455S2v2 alpha implementation allows for disabling NLS via NLS State Set command for experimenting with the alpha implementation. This is not allowed according to the Z-Wave specification and will be removed in the future GA implementation.S2v2 alpha feature
1619029When a fragmented beam is transmitted in a 3ch region, the channel hopping is not frequent enough to comply with local regulation.Currently not available.Frequently Listening device type
1666189Frequently Listening (FLiRS) battery applications, such as the door lock example, may experience watchdog resets when the IDLE task does not run often enough to feed the watchdog. The hardware watchdog counts only during EM0 (active) execution. In FLiRS mode, the device wakes briefly for beam reception and other interrupt-driven work; if application changes prevent the IDLE task from feeding the watchdog, EM0 active time from many short wakeups can accumulate until the watchdog timeout is exceeded. Unmodified SDK sample applications are not expected to hit this issue, but customized firmware has no guarantee.Use FreeRTOS YIELD regularly if no task are scheduled to properly enter IDLE Hook in order to feed properly the watchdog and prevent watchdog resets.Frequently Listening (FLiRS) end devices: zwave_soc_door_lock_keypad battery-powered end nodes with watchdog enabled
1641161Zniffer truncates destination node IDs to 8 bits in WakeUp Beam Start frames when connected via USB.https://github.com/Z-Wave-Alliance/z-wave-tools-core/issues/76Connect to the Zniffer device via Ethernet.zwave_ncp_zniffer
1682748After being included without security, a FLiRS device will stay awake for 7 to 8 seconds instead of the expected 2 seconds.Currently not available.FLiRS end devices
1793517Custom Dynamic Transmit Power Algorithm (DTPA) noise margin configured via ZWAVE_DTPA_NOISE_MARGIN_DBM in zw_dtpa_config.h is not applied at startup; the default 6 dB margin is used instead.See DTPA noise margin.Long Range / Dynamic Tx Power Algorithm
1733594Frames destined for a FLiRS node are sometimes aborted before beaming finishes. This can cause neighbor updates to miss neighbors (NOP Power frames not sent to every neighbor) and can also abort routed frames requested by the host application to a FLiRS end node.Currently not available.End devices
The DCDC configuration value is not applied by the application. Instead, the default value of the macro is used.Call sl_dcdc_vmon_init(ZW_DCDC_CONFIG); from the application code.All Z-Wave applications
1840450Under high channel occupancy, LBT failures can delay or prevent SmartStart Prime and Include Request transmissions at their scheduled time.Retry failed inclusions.FL nodes running on ZG28 with Z-Wave mesh

Workarounds#

DTPA noise margin#

Declare the DTPA noise margin setter and call it from application code after other initialization steps (for example, at the end of ApplicationTask in app.c, before the infinite loop):

extern void ZW_dtpa_set_noise_margin(uint8_t margin);

...

ApplicationTask(...) {
  ...

  ZW_dtpa_set_noise_margin(ZWAVE_DTPA_NOISE_MARGIN_DBM * 10);

  for (;;) {

Impact of Release Changes#

Impact Statements | Migration Guide

Impact Statements#

  • Toolchains: Z-Wave SDK 8.1.2 is built and validated with GCC 14.2.rel1, and LLVM 21.1.1. Rebuild existing projects after upgrading the SDK or toolchain.

Migration Guide#

Click here for the migration guide for deprecated, removed, and modified items.

Documentation Changes#

The 'Important Changes' document is now removed. All information relevant to the current release is provided in both the Release Notes and the Migration Guide.

Using This Release#

Installation and Use | Help and Feedback

Installation and Use#

To upgrade your existing software with this release, see instructions in the Migration Guide.

To run your first demo, see our Z-Wave Getting Started for End Devices.

To learn more about the software in this release, dive into our Z-Wave online documentation.

For information about Secure Vault Integration, see Secure Vault.

To review Security and Software Advisory notifications and manage your notification preferences:

  1. Go to https://community.silabs.com/.

  2. Log in with your account credentials.

  3. Click your profile icon in the upper-right corner of the page.

  4. Select Notifications from the dropdown menu.

  5. In the Notifications section, go to the My Product Notifications tab to review historical Security and Software Advisory notifications

  6. To manage your preferences, use the Manage Notifications tab to customize which product updates and advisories you receive.

Help and Feedback#

SDK Release and Maintenance Policy#

See our SDK Release and Maintenance Policy.