Edit

Silicon Labs AI/ML Version 3.0.2 - Release Notes (Oct 14, 2026)#

Simplicity SDK Version 2026.6.2

The Silicon Labs AI/ML SDK enables machine learning development on Series 2 (EFR and SiWG917) devices using the Tensorflow Lite for Microcontrollers (TFLM) framework.

Release Summary#

Release Item Version Release Date Release Notes Key Features API Changes Bug Fixes Chip Enablement

AI/ML SDK

3.0.2

Oct 14, 2026

Release Notes

  • Added BRD2605B board compatibility to SiWG917 AI/ML applications.
  • Added BRD2608B support to EFR32 AI/ML applications.
  • Improved Model Profiler firmware memory handling and configuration.
  • Added support for the LLVM compiler for the SiW917 AI/ML applications.
  • Restored Tensorflow Lite Micro as a prebuilt static library.
  • Limited ML model code generation to model-specific header files.

None

Fixed application, Model Profiler firmware, and tool integration issues.

None

MVP Math Library

6.0.2

Oct 14, 2026

Release Notes

  • Fixed MVP Math Demo for IAR and SiWG917.

None

None

None

Impact of Release Changes#

Impact Statements | Migration Guide

Impact Statements#

Change Impact Affected Software Variants if applicable Affected Modes Affected OPNs / Boards / OPN Combinations Affected Host Interfaces

Inference optimizations enabled on EFR32 devices.

  • Inference time reduction by up to 50% to 80%.
  • Amortized energy usage reduction due to faster transition back to EM2.

Standard

SoC

  • EFR32
  • EFM32

None

Tensorflow Lite Micro is again provided as a prebuilt static library (AI/ML SDK 3.0.2).

  • If your project still compiles TFLM sources (for example, copied sources or custom build settings from AI/ML SDK 3.0.0 or 3.0.1), remove those overrides and use the tensorflow_lite_micro component static library so the runtime is not duplicated or mismatched with the SDK.
  • See Migration Guide.

Standard

SoC

  • EFR32
  • EFM32
  • SiWG917

None

ML model code generation is limited to model-specific header files (AI/ML SDK 3.0.2).

  • Remove autogenerated model implementation sources (.c files) from the project tree, project configuration, and source control; include the generated headers instead.
  • Regenerate models after upgrade so stale sources are not built.
  • See Migration Guide.

Standard

SoC

  • EFR32
  • EFM32
  • SiWG917

None

Migration Guide#

When upgrading from AI/ML SDK 3.0.0 or 3.0.1 to 3.0.2, review the impact statements for Tensorflow Lite Micro static library delivery and header-only model code generation.

Click here for the migration guide for deprecated, removed, and modified items introduced in AI/ML SDK 3.0.0.

Using This Release#

What's in the Release? | Compatible Software | Installation and Use | Help and Feedback

What's in the Release?#

This release includes:

  • AI/ML SDK 3.0.2: Board compatibility updates, Model Profiler improvements, application fixes, LLVM compiler support, external sml-compile integration, TFLM delivered again as a static library, and ML model code generation limited to model-specific header files.

  • MVP Math Library 6.0.2: MVP Math Demo fixes for IAR and SiWG917.

Compatible Software#

Software Compatible Version or Variant

Software Development Kit (SDK)

  • Simplicity SDK: 2026.6.2
  • WiSeConnect SDK: 4.1.2

Installation and Use#

To upgrade your existing software with the latest features included in this release, update Simplicity Studio to the latest version, Simplicity SDK to v2026.6.2, WiSeConnect SDK to v4.1.2, and AI/ML SDK to v3.0.2 using Studio installation manager. Alternatively, download the SDKs from the links listed in the Compatible Software section.

To run your first demo, see our Getting Started

To kick start your development, see our Developer's Guide.

For information about Secure Vault Integration, see Secure Vault.

To review Security and Software Advisory notifications and manage your notification preferences:

  1. Go to https://community.silabs.com/.

  2. Log in with your account credentials.

  3. Select your profile icon in the upper-right corner of the page.

  4. Select Notifications from the dropdown menu.

  5. In the Notifications section, go to the My Product Notifications tab to review historical Security and Software Advisory notifications.

  6. To manage your preferences, use the Manage Notifications tab to customize which product updates and advisories you receive.

To learn more about the software in this release, dive into our online documentation

Help and Feedback#

Feature Matrix#

Supported Features | Unsupported Features

See the detailed feature matrix in each component release notes page:

Supported Features#

None

Unsupported Features#

  • IAR 9.70.3 is supported only on EFR32 devices. Support for SiWG917 is not yet available.

SDK Release and Maintenance Policy#

See our SDK Release and Maintenance Policy.