Edit

Silicon Labs MVP Math Library Version 6.0.1 - Release Notes (Oct 14, 2026)#

Silicon Labs AI/ML Version 3.0.1

Simplicity SDK Version 2026.6.1

MVP Math Library includes Real and Complex Matrix and Vector operations using the Matrix Vector Processor available on EFR32xG24/6/8 and SiWG917. The library is an alternative to CMSIS-DSP for Matrix and Vector math operations.

Release Summary#

Key Features | API Changes | Bug Fixes | Chip Enablement

Key Features#

Added in 6.0.2#

None

Added in 6.0.1#

  • Enabled MVP Math Demo sample application on SiWG917.

Added in 6.0.0#

  • MVP Math Library release notes moved from Platform to AI/ML.

  • NN kernels moved from MVP Math Library to AI/ML SDK.

  • Renamed "MVP Math Demo" sample application to "Compute - SoC Math MVP EFR32".

API Changes#

Changed in 6.0.2#

None

Bug Fixes#

Fixed in 6.0.2#

None

Chip Enablement#

Added in 6.0.2#

None

Key Features#

New Features | Enhancements | Removed Features | Deprecated Features

Note: See Feature Matrix for a list of any applicable APIs, examples, software variants, modes, hardware, and host interfaces for each feature.

New Features#

Added in 6.0.2#

None

Enhancements#

Added in 6.0.2#

None

Added in 6.0.1#

None

Added in 6.0.0#

  • Package relocation: MVP Math Library is now delivered as part of the AI/ML SDK extension instead of the Platform SDK. Release notes are published under AI/ML instead of Platform.

  • Sample application rename: Renamed "MVP Math Demo" to "Compute - SoC Math MVP EFR32" in Simplicity Studio.

Removed Features#

Removed in 6.0.2#

None

Removed in 6.0.1#

None

Removed in 6.0.0#

Removed Feature

Was Deprecated?

NN kernels (moved to AI/ML SDK)

No

Neural network kernels previously provided by the MVP Math Library are now part of the AI/ML SDK. Applications that used NN kernels from the MVP Math Library should use the AI/ML SDK components instead.

Deprecated Features#

Deprecated in 6.0.2#

None

API Changes#

New APIs | Modified APIs | Removed APIs | Deprecated APIs

New APIs#

Added in 6.0.2#

None

Modified APIs#

Modified in 6.0.2#

None

Removed APIs#

Removed in 6.0.2#

None

Removed in 6.0.1#

None

Removed in 6.0.0#

Removed API / Feature

Was Deprecated?

NN kernels in MVP Math Library

No

Deprecated APIs#

Deprecated in 6.0.2#

None

Bug Fixes#

Fixed in 6.0.2#

None

Chip Enablements#

Added in 6.0.2#

None

Application Example Changes#

New Examples | Modified Examples | Removed Examples | Deprecated Examples

New Examples#

Added in 6.0.2#

None

Modified Examples#

Modified in 6.0.2#

None

Modified in 6.0.1#

Example Name

Changes

Compute - SoC Math MVP

Renamed from "Compute - SoC Math MVP EFR32".

Modified in 6.0.0#

Example Name

Changes

Compute - SoC Math MVP EFR32

Renamed from "MVP Math Demo".

Removed Examples#

Removed in 6.0.2#

None

Deprecated Examples#

Deprecated in 6.0.2#

None

Known Issues and Limitations#

None