Simplicity Connect Mobile App Version 3.3.2 - Release Notes (Oct 14, 2026)#

These release notes cover Simplicity Connect for Android and iOS.

Click here for earlier releases.

The Simplicity Connect app includes sample demos to help you get started with Simplicity Connect and Silicon Labs development tools.

Release Summary#

Key Features | API Changes | Bug Fixes | Chip Enablement

Key Features#

Added in 3.3.2#

  • None.

Added in 3.3.1#

  • None.

Added in 3.3.0#

  • Added Simplicity Connect rebranding.

  • Added Matter demos for Oven and Range Hood.

  • Added example app titles to the app and user guide.

  • Added a proximity lock demo via channel sounding on Android.

API Changes#

None.

Bug Fixes#

Fixed in 3.3.2#

  • None.

Fixed in 3.3.1#

  • Fixed an issue where the peripheral device disconnected when selecting a file during the Over-the-Air (OTA) Non-Ack interoperability (IOP) test.

  • Fixed an issue where the informational popup for FreeRTOS system-on-chip (SoC) devices was not displayed during IOP testing.

Fixed in 3.3.0#

  • Fixed BLE disconnection (0x4E13 timeout expired) occurring during repeated Wi-Fi AP switching.

Chip Enablement#

None.

Key Features#

New Features | Enhancements | Removed Features | Deprecated Features

Note: See Feature Matrix for APIs, examples, software variants, modes, hardware, and host interfaces that apply to each feature.

New Features#

Added in 3.3.2#

  • None.

Added in 3.3.1#

  • None.

Added in 3.3.0#

  • Added Simplicity Connect rebranding.

  • Added Matter demos for Oven and Range Hood.

  • Added example app titles to the app and user guide.

  • Added a proximity lock demo via channel sounding on Android.

Enhancements#

Added in 3.3.2#

  • None.

Added in 3.3.1#

  • Added Expert Mode to the IOP Test.

  • Added a Generic Attribute Profile (GATT) Table to the IOP Test.

  • Added Throughput Status to the IOP Test.

  • Updated the test result with the message "Test Case 7.5 is not applicable for Android".

  • Improved the documentation for the Channel Sounding Demo.

Added in 3.3.0#

  • Updated the Channel Sounding Phase 1 demo for Android.

Removed Features#

None.

Deprecated Features#

None.

API Changes#

New APIs#

None.

Modified APIs#

None.

Removed APIs#

None.

Deprecated APIs#

None.

Bug Fixes#

Fixed in 3.3.2#

  • None.

Fixed in 3.3.1#

ID Issue Description GitHub / Salesforce Reference Affected Software Variants, Hardware, Modes, Host Interfaces
1685574 Fixed an issue where the peripheral device disconnected when selecting a file during the Over-the-Air (OTA) Non-Ack interoperability (IOP) test. None.
    IOP Test
1686308 Fixed an issue where the informational popup for FreeRTOS system-on-chip (SoC) devices was not displayed during IOP testing. None.
    IOP Test

Fixed in 3.3.0#

ID Issue Description GitHub / Salesforce Reference Affected Software Variants, Hardware, Modes, Host Interfaces
1650052 Fixed BLE disconnection (0x4E13 timeout expired) occurring during repeated Wi-Fi AP switching. None.
  • Wi-Fi Commissioning

Chip Enablement#

None.

Application Example Changes#

New Examples | Modified Examples | Removed Examples | Deprecated Examples

New Examples#

Added in 3.3.2#

  • None.

Added in 3.3.1#

None.

Added in 3.3.0#

  • Added Simplicity Connect rebranding.

  • Added Matter demos for Oven and Range Hood.

  • Added example app titles to the app and user guide.

  • Added a proximity lock demo via channel sounding on Android.

Modified Examples#

Added in 3.3.2#

  • None.

Modified in 3.3.1#

  • Enhanced the IOP test case demo with robust testing coverage and validations.

  • Updated the Channel Sounding demo for Android.

Modified in 3.3.0#

  • Updated the Channel Sounding demo for Android.

Removed Examples#

None.

Deprecated Examples#

None.

Known Issues and Limitations#

None.

Impact of Release Changes#

None.

Using This Release#

What's in the Release?#

Added in 3.3.2#

  • None.

Added in 3.3.1#

  • None.

Added in 3.3.0#

  • Added Simplicity Connect rebranding.

  • Added Matter demos for Oven and Range Hood.

  • Added example app titles to the app and user guide.

  • Added a proximity lock demo via channel sounding on Android.

Compatible Software#

Software

Compatible version or variant

Simplicity Connect App

3.3.2

WiSeConnect

4.1.2

Silicon Labs Matter

2.9.2 - 1.6

Installation and Use#

To upgrade your application with this release, download from Google Play Store or Apple App Store.

Find the source code on GitHub for iOS and Android.

To run your first demo, see the Getting Started Guides.

To start your development, see the Developer's Guide.

For information about Secure Vault integration, see Secure Vault.

To review Security and Software Advisory notifications and manage your notification preferences:

  1. Go to https://community.silabs.com/.

  2. Log in with your account credentials.

  3. Click your profile icon in the upper-right corner of the page.

  4. Select Notifications from the dropdown menu.

  5. In the Notifications section, go to the My Product Notifications tab to review historical Security and Software Advisory notifications.

  6. To manage your preferences, use the Manage Notifications tab to customize which product updates and advisories you receive.

To learn more about the software in this release, see the online documentation.

Help and Feedback#

Feature Matrix#

Supported Features#

Feature Name Description Quality Related API Name(s) Supported Software Variant(s) Supported Mode(s) Supported OPN(s) / Board(s) / OPN Combination(s) Supported Host Interface(s) Application Examples
Health Thermometer Read data from the Health Thermometer Service Sample Demo N/A Secure connectivity firmware for BLE SoC EFR32xG24 N/A Bluetooth - SoC Thermometer example from Simplicity Studio
Connected Device Control connected lights and switches Sample Demo N/A Secure connectivity firmware for BLE SoC EFR32xG24 N/A rail_soc_light & rail_soc_switch example from Simplicity Studio
Blinky Control the LED and receive button presses Sample Demo N/A Secure connectivity firmware for BLE SoC EFR32xG24 N/A Bluetooth - SoC Blinky example from Simplicity Studio
Range Test Evaluate the link budget and range of EFR32 devices Sample Demo N/A Secure connectivity firmware for BLE SoC EFR32xG24 N/A RAIL - SoC Range Test example from Simplicity Studio
BLE Throughput Measure throughput between a mobile device and an EFR32 device Sample Demo N/A Secure connectivity firmware for BLE SoC EFR32xG24 N/A Bluetooth - SoC Throughput example from Simplicity Studio
Motion Control a 3D rendering of the dev kit Sample Demo N/A Secure connectivity firmware for BLE SoC EFR32xG24 N/A bt_soc_thunderboard example from Simplicity Studio
Environment Read and display data from the dev kit Sample Demo N/A Secure connectivity firmware for BLE SoC EFR32xG24 N/A bt_soc_thunderboard example from Simplicity Studio
Wi-Fi Commissioning Wi-Fi Commissioning over BLE Sample Demo N/A Standard connectivity firmware for Wi-Fi SoC SiWx917 N/A Out-of-box demo (SoC) example from Simplicity Studio
ESL Add and commission ESL tags by scanning a QR code Sample Demo N/A Secure connectivity firmware for BLE SoC and NCP EFR32xG22 (SoC), EFR32BG22 (NCP) UART Bluetooth - NCP ESL Access Point and Bluetooth ESL tag example from Simplicity Studio
Matter Add and commission Matter devices by scanning QR codes Sample Demo N/A Secure connectivity firmware for BLE and Standard connectivity firmware for Wi-Fi SoC EFR32xG24 (Thread), SiWx917 (Wi-Fi) UART Matter - SoC Lighting over Wi-Fi/Thread from Simplicity Studio
Wi-Fi OTA Control over-the-air (OTA) firmware updates over Wi-Fi Sample Demo N/A Standard connectivity firmware for Wi-Fi SoC SiWx917 UART Wi-Fi - M4 Firmware Update via TCP example from Simplicity Studio
Wi-Fi Sensor Read and display sensor data from the dev kit Sample Demo N/A Standard connectivity firmware for Wi-Fi SoC SiWx917 UART Wi-Fi - SiWx917 Dev Kit (BRD2605A) example from Simplicity Studio
Wi-Fi Throughput Measure Wi-Fi throughput between a mobile device and a SiWx917 device Sample Demo N/A Standard connectivity firmware for Wi-Fi SoC SiWx917 UART Wi-Fi - Throughput (SoC) example from Simplicity Studio
Wi-Fi Provisioning Wi-Fi Provisioning over Wi-Fi Sample Demo N/A Standard connectivity firmware for Wi-Fi SoC SiWx917 UART Wi-Fi - Provisioning via Access Point (SoC) example from Simplicity Studio
Amazon AWS IoT Cloud Add, commission, and read data from devices over AWS IoT Cloud Sample Demo N/A Standard connectivity firmware for Wi-Fi SoC SiWx917 UART Wi-Fi Coex - Wi-Fi Client BLE Provisioning with AWS (SoC) example from Simplicity Studio
Smart Lock Add and commission smart locks and read and control them over Bluetooth and AWS IoT Cloud. Sample Demo N/A Standard connectivity firmware for Wi-Fi SoC SiWx917 UART Smart Lock example from Simplicity Studio
Battery-less Asset Tagging Demonstrates energy harvesting from devices Sample Demo N/A Standard connectivity firmware for Wi-Fi SoC BRD2710A and BRD8201A UART Bluetooth - SoC Energy Harvesting Sensor example from Simplicity Studio
Channel Sounding Demo (Android) Demonstrates a proximity lock demo via channel sounding. Sample Demo N/A Standard connectivity firmware for BLE SoC BRD2606A UART Bluetooth - SoC CS Initiator and Bluetooth - SoC CS Reflector example from Simplicity Studio

Unsupported Features#

None.

SDK Release and Maintenance Policy#

See here for SDK release and maintenance policy.