Bluetooth LE Version 11.1.2 - Release Notes (Oct 14, 2026)#
Silicon Labs is a leading vendor in Bluetooth hardware and software technologies, used in products such as sports and fitness, consumer electronics, beacons, and smart home applications. The core SDK is an advanced Bluetooth 6.1-compliant stack that provides all of the core functionality along with multiple API to simplify development. The core functionality offers both standalone mode, allowing a developer to create and run their application directly on the SoC, or NCP mode, allowing for the use of an external host MCU.
Click here for earlier releases.
Release Summary#
| Release Item | Version | Release Date | Release Notes | Key Features | API Changes | Bug Fixes | Chip Enablement |
|---|---|---|---|---|---|---|---|
| Example and Middleware | 11.1.2 | Oct 14, 2026 | Release Notes |
|
None | Fixed the host UART interface to avoid wrong-handle use after select() by migrating to poll(). |
None |
| Host Stack | 11.1.2 | Oct 14, 2026 | Release Notes | None | None |
|
None |
| Controller | 11.1.2 | Oct 14, 2026 | Release Notes | None | Updated periodic advertising synchronization behavior so changes to the skip value in sl_bt_sync_update_sync_parameters() take effect sooner for both PA and PAwR. |
|
None |
| 802.15.4 Mesh + BLE Multiprotocol | 11.1.2 | Oct 14, 2026 | None |
None |
Targeted quality improvements and bug fixes. |
None |
Impact of Release Changes#
Impact Statements | Migration Guide
Impact Statements#
None.
Using This Release#
What's in the Release? | Compatible Software | Installation and Use | Help and Feedback
What's in the Release?#
Compatible Software#
| Software | Compatible Version or Variant |
|---|---|
| Simplicity SDK | 2025.12.3 |
| Simplicity Studio | Any version that is compatible to Simplicity SDK 2025.12 |
| Simplicity Commander | provided with Simplicity Studio |
| GCC (The GNU Compiler Collection) | 12.2.1 (provided with Simplicity Studio) |
| IAR Embedded Workbench for ARM (IAR-EWARM) | 9.40.1 |
| LLVM | 21.1.1 (provided with Simplicity Studio) |
Installation and Use#
To run your first demo, see our Getting Started Guides.
To kick start your development, see our Developer's Guide.
For information about Secure Vault Integration, see Secure Vault.
To review Security and Software Advisory notifications and manage your notification preferences:
Log in with your account credentials.
Click your profile icon in the upper-right corner of the page.
Select Notifications from the dropdown menu.
In the Notifications section, go to the My Product Notifications tab to review historical Security and Software Advisory notifications
To manage your preferences, use the Manage Notifications tab to customize which product updates and advisories you receive.
To learn more about the software in this release, dive into our online documentation.
Help and Feedback#
Contact Silicon Labs Support.
To use our Ask AI tool to get answers, see the search field at the top of this page.
Note: Ask AI is experimental.
Get help from our developer community.
SDK Release and Maintenance Policy#
See our SDK Release and Maintenance Policy.