Edit

Zigbee Version 9.1.2 - Release Notes (Oct 14, 2026)#

Silicon Labs is the vendor of choice for OEMs developing Zigbee networking into their products. The Silicon Labs Zigbee platform is the most integrated, complete, and feature-rich Zigbee solution available.

Silicon Labs EmberZNet SDK contains Silicon Labs’ implementation of the Zigbee stack specification.

Click here for earlier releases.

Release Summary#

Release Item Version Release Date Release Notes Key Features API Changes Bug Fixes Chip Enablement

SDK

9.1.2

Oct 14, 2026

Release Notes

None None

Targeted quality improvements and bug fixes.

None

802.15.4 Mesh + BLE Multiprotocol

9.1.2

Oct 14, 2026

Release Notes

None None

Targeted quality improvements and bug fixes.

None

Impact of Release Changes#

Impact Statements | Migration Guide

Impact Statements#

  • Toolchains: Zigbee SDK 9.1.2 is built and validated with GCC 14.2.rel1, IAR 9.70.4, and LLVM 21.1.1. Rebuild existing projects after upgrading the SDK or toolchain.

  • Example labels and project names: Standardized display labels and project names for certain Zigbee example applications in Simplicity Studio. Example apps now use a consistent title format that identifies the stack (Zigbee, Zigbee SE, Zigbee GP, or Zigbee BLE DMP), the target role (SoC, Host, or NCP), and the application name with readable spacing (for example, "Zigbee - SoC Z3 Light" instead of "Zigbee - Z3Light"). The NCP SPI example was renamed from ncp-spi to zigbee_ncp_spi (project folder, .slcp file, and project_name field). NCP example labels were normalized (for example, UartHw to UART HW, Multi-PAN naming). GPD single-button/LED variant examples use distinct project names and labels so each variant is uniquely identified in Studio. This affects how example applications appear when browsing or creating projects in Simplicity Studio only; application functionality is unchanged. See Changes in the Zigbee SDK release notes.

  • This release includes new features, API changes, bug fixes, and chip enablement updates. See the Zigbee SDK release notes for details.

Migration Guide#

Using This Release#

What's in the Release? | Compatible Software | Installation and Use | Help and Feedback

What's in the Release?#

This release contains the following:

  • Zigbee Stack

  • Zigbee Application Framework

  • Zigbee Sample Applications

For more information about Zigbee and the EmberZNet SDK see Zigbee Fundamentals.

If you are a first-time user, see Zigbee EmberZNet Quick-Start Guide for SDK 7.0 and Higher, for instructions on configuring your development environment, building and flashing a sample application, and documentation references pointing to next steps.

Compatible Software#

Compatibility and Use Notices: For information about security updates and notices, see the Security chapter of the Platform Release Notes installed with this SDK or on the TECH DOCS tab on https://www.silabs.com/developers/zigbee-emberznet. Silicon Labs also strongly recommends that you subscribe to Security Advisories for up-to-date information.

For instructions, or if you are new to the Zigbee EmberZNet SDK, see Using This Release.

Software Compatible Version or Variant

IAR Embedded Workbench for ARM (IAR-EWARM)

Using wine to build with the IarBuild.exe command line utility or IAR Embedded Workbench GUI on macOS or Linux could result in incorrect files being used due to collisions in wine’s hashing algorithm for generating short file names.

Customers on macOS or Linux are advised not to build with IAR outside of Simplicity Studio. Customers who do should carefully verify that the correct files are being used.

Version 9.70.4
GCC (The GNU Compiler Collection) Version 14.2.rel1
LLVM Version 21.1.1
EZSP Protocol Version 0x13

Installation and Use#

To run your first demo, see our Getting Started Guide.

To kick start your development, see our Developer's Guide.

For information about Secure Vault Integration, see Secure Vault.

To review Security and Software Advisory notifications and manage your notification preferences:

  1. Go to https://community.silabs.com/.

  2. Log in with your account credentials.

  3. Click your profile icon in the upper-right corner of the page.

  4. Select Notifications from the dropdown menu.

  5. In the Notifications section, go to the My Product Notifications tab to review historical Security and Software Advisory notifications

  6. To manage your preferences, use the Manage Notifications tab to customize which product updates and advisories you receive.

To learn more about the software in this release, dive into our online documentation.

Additional Information#

Zigbee Certification

The EmberZNet 9.0 release is qualified as a Zigbee Compliant Platform for SoC, NCP and RCP architectures. For ZCP certification ID tied to this release, please check the CSA website here: https://csa-iot.org/csa-iot_products/.

Note that the ZCP certification is filed post-release and takes a few weeks before getting reflected on the CSA website. For any further queries, please contact Silicon Laboratories support at http://www.silabs.com/support.

Help and Feedback#

Feature Matrix#

Supported Features | Unsupported Features

Supported Features#

Feature Name Description Quality Related API Names Supported Software Variants, Hardware, Modes, Host Interfaces Related Example Names
GPD configurable next RX channel Green Power Device applications can set the next RX channel and second next RX channel at runtime before bi-directional commissioning Channel Request GPDFs. Configure via node set-next-channel or sl_zigbee_gpd_af_plugin_set_next_channel(). Production sl_zigbee_gpd_af_plugin_set_next_channel
GPD (SoC) GPD sample applications with Zigbee GPD CLI
Secure inter-PAN fragmentation The Inter-PAN plugin supports large, APS link-encrypted inter-PAN messages with Inter-PAN Message Fragmentation after Certificate-Based Key Establishment (CBKE). Production Inter-PAN plugin APIs and callbacks
SoC
Host-NCP
Zigbee Smart Energy and inter-PAN sample applications
Packet handoff link quality Post-incoming packet filter callback reports RSSI, LQI, and receive channel for packets intercepted through packet handoff. Implement sl_zigbee_post_incoming_packet_filter_with_lqi_and_rssi_cb() with sl_zigbee_packet_link_quality_t. Production sl_zigbee_post_incoming_packet_filter_with_lqi_and_rssi_cb
sl_zigbee_packet_link_quality_t
SoC
Host-NCP
Applications with Packet Handoff component
Zigbee 4.0 gateway sample Host gateway sample for Zigbee 4.0 joining with Z4 light and switch sample applications. Production Host-NCP
Zigbee 4.0 gateway
GCC and IAR toolchain upgrade Zigbee SDK 9.1.0 is validated with GCC 14.2.rel1 and IAR Embedded Workbench 9.70.4. IAR 9.70.4 supports Zigbee SoC and NCP applications on Series 3, in addition to Series 2 targets. Rebuild existing projects after upgrading the SDK or toolchain. Production All variants
All Zigbee sample applications
Configurable route table size Route table size is configurable through the Zigbee Pro Stack Config component (SL_ZIGBEE_ROUTE_TABLE_SIZE). Production SL_ZIGBEE_ROUTE_TABLE_SIZE
SoC, Host-NCP (Pro stack)
Router and coordinator applications

Unsupported Features#

None.

SDK Release and Maintenance Policy#

See our SDK Release and Maintenance Policy.